<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 Re: IMX6 Solo LPDDR2 Calibration Failure</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/IMX6-Solo-LPDDR2-Calibration-Failure/m-p/741998#M115500</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Awesome!&amp;nbsp; Thanks for verifying Yuri!&amp;nbsp; So I guess we will fix DQ[0:7] and clean up our layout and then hopefully everything will work after that, since the rest of the schematics and configuration look good.&amp;nbsp; I will update this post after we get new boards.&amp;nbsp; Thanks for the the help Yuri!!!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-Jarrod&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 16 Feb 2018 14:11:51 GMT</pubDate>
    <dc:creator>jcc273</dc:creator>
    <dc:date>2018-02-16T14:11:51Z</dc:date>
    <item>
      <title>IMX6 Solo LPDDR2 Calibration Failure</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX6-Solo-LPDDR2-Calibration-Failure/m-p/741994#M115496</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;We have created a custom board using an IMX6 Solo and a combination NAND/LPDDR2 chip (MT29RZ4B2DZZHHWD-18I).&amp;nbsp; We have just finished producing some prototypes and I have used the Register programming aid (V1.3) to setup a script for the DDR Stress Tester Tool (I have tried both V2.80 and V1.0.3).&amp;nbsp; I am connecting via the USB port and I am able to download into the part and I can even read and write individual registers using the DDR tool; however, I am unable to run either the Calibration or the Stress test successfully.&amp;nbsp; I am thinking this likely indicates some sort of layout issue, but wondered if someone could verify the following are correct:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;OL&gt;&lt;LI&gt;Init Script - It was generated using the script aid tool and I think i got all the values in there correct but i don't have a working Solo/Dual Lite board with LPDDR2 to test it with.&amp;nbsp; Script is attached.&lt;/LI&gt;&lt;LI&gt;Circuit - There was this confusing table in the hardware document of how to map pins on the Solo for LPDDR3 instead of DDR3 and I am nervous that one of the non-data lines is incorrectly connected.&lt;/LI&gt;&lt;/OL&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I just want to verify the above uncertainties aren't a problem before i head down the route of layout modifications and ordering new boards.&amp;nbsp; Thanks!&amp;nbsp; Oh here is the output from the DDR Test Tool:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;============================================&lt;BR /&gt; DDR Stress Test (2.6.0) &lt;BR /&gt; Build: Jan 24 2018, 14:20:57&lt;BR /&gt; NXP Semiconductors.&lt;BR /&gt;============================================&lt;/P&gt;&lt;P&gt;============================================&lt;BR /&gt; Chip ID&lt;BR /&gt;CHIP ID = i.MX6 Solo/DualLite (0x61)&lt;BR /&gt;Internal Revision = TO1.3&lt;BR /&gt;============================================&lt;/P&gt;&lt;P&gt;============================================&lt;BR /&gt; Boot Configuration&lt;BR /&gt;SRC_SBMR1(0x020d8004) = 0x00000000&lt;BR /&gt;SRC_SBMR2(0x020d801c) = 0x32000001&lt;BR /&gt;============================================&lt;/P&gt;&lt;P&gt;ARM Clock set to 800MHz&lt;/P&gt;&lt;P&gt;============================================&lt;BR /&gt; DDR configuration&lt;BR /&gt;BOOT_CFG3[5-4]: 0x00, Single DDR channel.&lt;BR /&gt;DDR type is LPDDR2 in 1-channel mode.&lt;BR /&gt;Data width: 32, bank num: 8&lt;BR /&gt;Row size: 13, col size: 10&lt;BR /&gt;Chip select CSD0 is used &lt;BR /&gt;Density per chip select: 256MB &lt;BR /&gt;Density per channel: 256MB &lt;BR /&gt;============================================&lt;/P&gt;&lt;P&gt;&lt;BR /&gt; 0x0 0x4 0x8 0xC&lt;BR /&gt; ----------------------------------------------------------------------------------------------------------------&lt;BR /&gt;0x10000000: 0xFFFFFFFF 0xFFFFFFFF 0xFFFFFFFF 0xFFFFFFFF &lt;BR /&gt;memory read is done&lt;BR /&gt;addr=0x10000000,data=0xDEADBEEF&lt;/P&gt;&lt;P&gt;Success to write address 0x10000000&lt;/P&gt;&lt;P&gt;0x0 0x4 0x8 0xC&lt;BR /&gt; ----------------------------------------------------------------------------------------------------------------&lt;BR /&gt;0x10000000: 0xDEADBEEF 0xFFFFFFFF 0xFFFFFFFF 0xFFFFFFFF &lt;BR /&gt;memory read is done&lt;BR /&gt;Current Temperature: 71&lt;BR /&gt;============================================&lt;/P&gt;&lt;P&gt;DDR Freq: 396 MHz&lt;/P&gt;&lt;P&gt;Note: Array result[] holds the DRAM test result of each byte. &lt;BR /&gt; 0: test pass. 1: test fail &lt;BR /&gt; 4 bits respresent the result of 1 byte. &lt;BR /&gt; result 0001:byte 0 fail. &lt;BR /&gt; result 0011:byte 0, 1 fail.&lt;/P&gt;&lt;P&gt;Starting Read calibration...&lt;/P&gt;&lt;P&gt;ABS_OFFSET=0x00000000 result[00]=0x1111&lt;BR /&gt;ABS_OFFSET=0x04040404 result[01]=0x1111&lt;BR /&gt;ABS_OFFSET=0x08080808 result[02]=0x1111&lt;BR /&gt;ABS_OFFSET=0x0C0C0C0C result[03]=0x1111&lt;BR /&gt;ABS_OFFSET=0x10101010 result[04]=0x1111&lt;BR /&gt;ABS_OFFSET=0x14141414 result[05]=0x1111&lt;BR /&gt;ABS_OFFSET=0x18181818 result[06]=0x1111&lt;BR /&gt;ABS_OFFSET=0x1C1C1C1C result[07]=0x1111&lt;BR /&gt;ABS_OFFSET=0x20202020 result[08]=0x1111&lt;BR /&gt;ABS_OFFSET=0x24242424 result[09]=0x1111&lt;BR /&gt;ABS_OFFSET=0x28282828 result[0A]=0x1111&lt;BR /&gt;ABS_OFFSET=0x2C2C2C2C result[0B]=0x1111&lt;BR /&gt;ABS_OFFSET=0x30303030 result[0C]=0x1111&lt;BR /&gt;ABS_OFFSET=0x34343434 result[0D]=0x1111&lt;BR /&gt;ABS_OFFSET=0x38383838 result[0E]=0x1111&lt;BR /&gt;ABS_OFFSET=0x3C3C3C3C result[0F]=0x1111&lt;BR /&gt;ABS_OFFSET=0x40404040 result[10]=0x1111&lt;BR /&gt;ABS_OFFSET=0x44444444 result[11]=0x1111&lt;BR /&gt;ABS_OFFSET=0x48484848 result[12]=0x1111&lt;BR /&gt;ABS_OFFSET=0x4C4C4C4C result[13]=0x1111&lt;BR /&gt;ABS_OFFSET=0x50505050 result[14]=0x1111&lt;BR /&gt;ABS_OFFSET=0x54545454 result[15]=0x1111&lt;BR /&gt;ABS_OFFSET=0x58585858 result[16]=0x1111&lt;BR /&gt;ABS_OFFSET=0x5C5C5C5C result[17]=0x1111&lt;BR /&gt;ABS_OFFSET=0x60606060 result[18]=0x1111&lt;BR /&gt;ABS_OFFSET=0x64646464 result[19]=0x1111&lt;BR /&gt;ABS_OFFSET=0x68686868 result[1A]=0x1111&lt;BR /&gt;ABS_OFFSET=0x6C6C6C6C result[1B]=0x1111&lt;BR /&gt;ABS_OFFSET=0x70707070 result[1C]=0x1111&lt;BR /&gt;ABS_OFFSET=0x74747474 result[1D]=0x1111&lt;BR /&gt;ABS_OFFSET=0x78787878 result[1E]=0x1111&lt;BR /&gt;ABS_OFFSET=0x7C7C7C7C result[1F]=0x1111&lt;/P&gt;&lt;P&gt;ERROR FOUND, we can't get suitable value !!!!&lt;BR /&gt;dram test fails for all values.&lt;/P&gt;&lt;P&gt;Error: failed during ddr calibration&lt;/P&gt;&lt;P&gt;DDR Stress Test Iteration 1&lt;BR /&gt;Current Temperature: 71&lt;BR /&gt;============================================&lt;/P&gt;&lt;P&gt;DDR Freq: 297 MHz&lt;BR /&gt;t0.1: data is addr test&lt;BR /&gt;Address of failure(step2): 0x10000140&lt;BR /&gt;Data was: 0x00000000&lt;BR /&gt;But pattern should match address &lt;BR /&gt;Error: failed to run stress test!!!&lt;/P&gt;&lt;P&gt;DDR Stress Test Iteration 1&lt;BR /&gt;Current Temperature: 70&lt;BR /&gt;============================================&lt;/P&gt;&lt;P&gt;DDR Freq: 297 MHz&lt;BR /&gt;t0.1: data is addr test&lt;BR /&gt;Address of failure(step2): 0x10000220&lt;BR /&gt;Data was: 0x00000000&lt;BR /&gt;But pattern should match address &lt;BR /&gt;Error: failed to run stress test!!!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 14 Feb 2018 00:15:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX6-Solo-LPDDR2-Calibration-Failure/m-p/741994#M115496</guid>
      <dc:creator>jcc273</dc:creator>
      <dc:date>2018-02-14T00:15:49Z</dc:date>
    </item>
    <item>
      <title>Re: IMX6 Solo LPDDR2 Calibration Failure</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX6-Solo-LPDDR2-Calibration-Failure/m-p/741995#M115497</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;Hello,&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;&amp;nbsp; Please look at my comments below.&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;1.&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; For Your configuration only MMDC0 should be init-ed.&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;(&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;BOOT_CFG3[5-4]: 0x00, Single DDR channel.&lt;BR /&gt;DDR type is LPDDR2 in 1-channel mode.&lt;BR /&gt;)&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;2.&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;&amp;nbsp;Scheme in general is correct, but strictly speaking, data bit swapping for LPDDR2&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;is not allowed.&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;&lt;A href="https://community.nxp.com/message/571460"&gt;https://community.nxp.com/message/571460&lt;/A&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;Have a great day,&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;Yuri&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;------------------------------------------------------------------------------&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;Note: If this post answers your question, please click the Correct Answer &lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;button. Thank you!&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 15 Feb 2018 06:41:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX6-Solo-LPDDR2-Calibration-Failure/m-p/741995#M115497</guid>
      <dc:creator>Yuri</dc:creator>
      <dc:date>2018-02-15T06:41:46Z</dc:date>
    </item>
    <item>
      <title>Re: IMX6 Solo LPDDR2 Calibration Failure</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX6-Solo-LPDDR2-Calibration-Failure/m-p/741996#M115498</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Yuri,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks for the reply!&amp;nbsp; I greatly appreciate it!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;1.&amp;nbsp; Alright so basically just remove anything from the script that sets up MMDC1, like the new attached version?&amp;nbsp; I still had to enable CS0 on MMDC1(0x021b4000) even though I'm only using MMDC0 otherwise things don't work at all.&amp;nbsp; (Still failed after the changes, assuming layout problems at this point).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;2.&amp;nbsp; Okay as we redo the layout we will try to route them unswapped as best we can.&amp;nbsp; We are very tight on area and can only come out 1 side of the CPU, but we only have 1 LPDDR2 Chip and from what I am reading it seems that the restrictions are due only to the ability to read the mode register out of DQ0-7 and for driving MRR bursts on the least significant bit of each byte.&amp;nbsp; So does this mean as long as I don't bit or byte swap DQ[0:7] and i leave the least significant bit of each byte (0,8,16,24)&amp;nbsp;in the correct spot i should be okay?&amp;nbsp; Meaning i could byte swap DQ[8:15],DQ[16:23],DQ[24:31] and i could bit swap bits 1-7 in within each byte group?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks again!&lt;/P&gt;&lt;P&gt;-Jarrod&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 15 Feb 2018 16:02:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX6-Solo-LPDDR2-Calibration-Failure/m-p/741996#M115498</guid>
      <dc:creator>jcc273</dc:creator>
      <dc:date>2018-02-15T16:02:04Z</dc:date>
    </item>
    <item>
      <title>Re: IMX6 Solo LPDDR2 Calibration Failure</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX6-Solo-LPDDR2-Calibration-Failure/m-p/741997#M115499</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;According to the discussion from the link below:&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;&amp;nbsp; Byte Group:&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;1. Byte Group 0 should not be swapped (for Mode Reg Read).&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;2. Byte Groups 1, 2 and 3 can be swapped in any order. &lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;&amp;nbsp; As for Bits within Byte Groups &lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;3. Byte Group 0 should not have bits rearranged (for Mode Reg Read data)&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;4. Byte Groups 1, 2 and 3 can have bits rearranged within them &lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;&amp;nbsp; if manufacturer allows it (Micron drives DQ Calibration to all bits). &lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;5. It would be technically more correct to keep bits 8, 16, and 24 as the &lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;&amp;nbsp; LSB in each byte group.&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;&lt;A class="link-titled" href="https://forums.xilinx.com/t5/Embedded-Processor-System-Design/Zynq-LPDDR2-DQ-Swap-Question/td-p/396867" title="https://forums.xilinx.com/t5/Embedded-Processor-System-Design/Zynq-LPDDR2-DQ-Swap-Question/td-p/396867"&gt;Zynq LPDDR2 DQ Swap Question - Community Forums&lt;/A&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;So, You are right: "&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;this mean as long as I don't bit or byte swap DQ[0:7] and I leave the &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;least significant bit of each byte (0,8,16,24)&amp;nbsp;in the correct spot it should be okay".&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Yuri.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 16 Feb 2018 04:11:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX6-Solo-LPDDR2-Calibration-Failure/m-p/741997#M115499</guid>
      <dc:creator>Yuri</dc:creator>
      <dc:date>2018-02-16T04:11:03Z</dc:date>
    </item>
    <item>
      <title>Re: IMX6 Solo LPDDR2 Calibration Failure</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX6-Solo-LPDDR2-Calibration-Failure/m-p/741998#M115500</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Awesome!&amp;nbsp; Thanks for verifying Yuri!&amp;nbsp; So I guess we will fix DQ[0:7] and clean up our layout and then hopefully everything will work after that, since the rest of the schematics and configuration look good.&amp;nbsp; I will update this post after we get new boards.&amp;nbsp; Thanks for the the help Yuri!!!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-Jarrod&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 16 Feb 2018 14:11:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX6-Solo-LPDDR2-Calibration-Failure/m-p/741998#M115500</guid>
      <dc:creator>jcc273</dc:creator>
      <dc:date>2018-02-16T14:11:51Z</dc:date>
    </item>
    <item>
      <title>Re: IMX6 Solo LPDDR2 Calibration Failure</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX6-Solo-LPDDR2-Calibration-Failure/m-p/741999#M115501</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Another quick note we also had the positive and negative clocks reversed.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 04 May 2018 21:16:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX6-Solo-LPDDR2-Calibration-Failure/m-p/741999#M115501</guid>
      <dc:creator>jcc273</dc:creator>
      <dc:date>2018-05-04T21:16:20Z</dc:date>
    </item>
  </channel>
</rss>