<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Temperature sensor connectivity in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Temperature-sensor-connectivity/m-p/741516#M115398</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;SPAN style="font-size: 12.0pt;"&gt;Hi,&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 12.0pt;"&gt;We are using IMXD7 application processor (MCIMX7D3EVK10SD ) for our wearable design. &amp;nbsp;When exploring the options for connecting external temperature sensors with the processor, we found from the datasheet that &amp;nbsp;we have a pin named TEMPSENSOR_REXT. This pin is recommended to connect to a 100k resistor to ground. Our query is that can we use this pin for external thermistor connection. Can the internal temperature sensor monitor module use this pin for temperature sensing. If yes please provide required inputs for the same.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 12.0pt;"&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 12.0pt;"&gt;Is there any other recommended way to connect external thermistors to IMX7D processor.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 12.0pt;"&gt;Thanks.&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 22 Dec 2017 13:30:28 GMT</pubDate>
    <dc:creator>logeshs</dc:creator>
    <dc:date>2017-12-22T13:30:28Z</dc:date>
    <item>
      <title>Temperature sensor connectivity</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Temperature-sensor-connectivity/m-p/741516#M115398</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;SPAN style="font-size: 12.0pt;"&gt;Hi,&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 12.0pt;"&gt;We are using IMXD7 application processor (MCIMX7D3EVK10SD ) for our wearable design. &amp;nbsp;When exploring the options for connecting external temperature sensors with the processor, we found from the datasheet that &amp;nbsp;we have a pin named TEMPSENSOR_REXT. This pin is recommended to connect to a 100k resistor to ground. Our query is that can we use this pin for external thermistor connection. Can the internal temperature sensor monitor module use this pin for temperature sensing. If yes please provide required inputs for the same.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 12.0pt;"&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 12.0pt;"&gt;Is there any other recommended way to connect external thermistors to IMX7D processor.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 12.0pt;"&gt;Thanks.&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 22 Dec 2017 13:30:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Temperature-sensor-connectivity/m-p/741516#M115398</guid>
      <dc:creator>logeshs</dc:creator>
      <dc:date>2017-12-22T13:30:28Z</dc:date>
    </item>
    <item>
      <title>Re: Temperature sensor connectivity</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Temperature-sensor-connectivity/m-p/741517#M115399</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Logesh&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 12.0pt;"&gt;EMPSENSOR_REXT&lt;/SPAN&gt; is used for biasing internal temperature sensor,&lt;/P&gt;&lt;P&gt;it can not be used for &lt;SPAN style="font-size: 12.0pt;"&gt;external thermistors&lt;/SPAN&gt;. E&lt;SPAN style="font-size: 12.0pt;"&gt;xternal thermistors can be &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 12.0pt;"&gt;connected to adc (with additional precision resistor connected to stable &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 12.0pt;"&gt;reference voltage source).&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 12.0pt;"&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 22 Dec 2017 23:40:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Temperature-sensor-connectivity/m-p/741517#M115399</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2017-12-22T23:40:51Z</dc:date>
    </item>
  </channel>
</rss>