<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 Linux imx6</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Linux-imx6/m-p/741514#M115396</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&amp;nbsp;&lt;/P&gt;&lt;P&gt;Id like to ask if there's a way to have a linux bin that doesn't require the .dtb file.&amp;nbsp;&lt;BR /&gt;Basically i want to include the linux .bin file on my code using .incbin and then jump to the linux image after executing my program.&amp;nbsp;&lt;/P&gt;&lt;P&gt;The flow i want its like this&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Startup code ----&amp;gt; main of my program ------&amp;gt; linux&amp;nbsp;&lt;/P&gt;&lt;P&gt;im using the imx6quad sd&lt;/P&gt;&lt;P&gt;kind regards,&amp;nbsp;&lt;/P&gt;&lt;P&gt;Ailton Lopes&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 17 Apr 2018 17:58:35 GMT</pubDate>
    <dc:creator>ailtonlopes</dc:creator>
    <dc:date>2018-04-17T17:58:35Z</dc:date>
    <item>
      <title>Linux imx6</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Linux-imx6/m-p/741514#M115396</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&amp;nbsp;&lt;/P&gt;&lt;P&gt;Id like to ask if there's a way to have a linux bin that doesn't require the .dtb file.&amp;nbsp;&lt;BR /&gt;Basically i want to include the linux .bin file on my code using .incbin and then jump to the linux image after executing my program.&amp;nbsp;&lt;/P&gt;&lt;P&gt;The flow i want its like this&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Startup code ----&amp;gt; main of my program ------&amp;gt; linux&amp;nbsp;&lt;/P&gt;&lt;P&gt;im using the imx6quad sd&lt;/P&gt;&lt;P&gt;kind regards,&amp;nbsp;&lt;/P&gt;&lt;P&gt;Ailton Lopes&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 17 Apr 2018 17:58:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Linux-imx6/m-p/741514#M115396</guid>
      <dc:creator>ailtonlopes</dc:creator>
      <dc:date>2018-04-17T17:58:35Z</dc:date>
    </item>
    <item>
      <title>Re: Linux imx6</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Linux-imx6/m-p/741515#M115397</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Ailton Lopes,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The current linux kernels require the .dtb file for hardware information so the information has to be loaded by the kernel, either from a separate .dtb file or as an append to the kernel.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The ROM code looks for the bootloader, you could run a script from the bootloader and then load the kernel; or alternatively you could run a plugin image and later run the booloader.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I hope this information helps!&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 18 Apr 2018 17:34:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Linux-imx6/m-p/741515#M115397</guid>
      <dc:creator>gusarambula</dc:creator>
      <dc:date>2018-04-18T17:34:39Z</dc:date>
    </item>
  </channel>
</rss>