<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: DDR Config tool gave invalid value</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/DDR-Config-tool-gave-invalid-value/m-p/741321#M115366</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi David&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;seems there is misprint when editing imximage.cfg :&lt;/P&gt;&lt;P&gt;ddr tool log&amp;nbsp; suggested value : MPDGCTRL0 = 0x01300124&lt;BR /&gt;while in imximage_new.cfg.zip :&lt;BR /&gt;/*&amp;nbsp;&amp;nbsp; Read DQS Gating calibration*/&lt;BR /&gt;DATA 4 0x021b083c 0x13000124&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 29 Nov 2017 07:56:08 GMT</pubDate>
    <dc:creator>igorpadykov</dc:creator>
    <dc:date>2017-11-29T07:56:08Z</dc:date>
    <item>
      <title>DDR Config tool gave invalid value</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/DDR-Config-tool-gave-invalid-value/m-p/741320#M115365</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;This is in relation to a custom board, patterned after the Sabre board, with an iMX6SX; I used the DDR stress test tool v2.7, to get the config values for my DDR; I then ran the stress test and it passed, I assume it used the config values it gave during the config. However, if I modify imximage.cfg in u-boot with these values, the board will not boot. So I went through the values and the registers in the reference manual and determined that the value for&amp;nbsp;&lt;SPAN style="font-size: 11.0pt;"&gt;MMDC_MPDGCTRL0 (0x021B083C) is the problem. So I set that one value back to the default and now the board boots. This gives me little confidence in the other values given; they work, but are they optimal? Is there something we did incorrectly in the setup?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 11.0pt;"&gt;I am attaching several things:&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 11.0pt;"&gt;ddr_calibration_20171113-10'54'40.log: this is the output of the DDR calibration in the Stress Test Tool&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 11.0pt;"&gt;MX6SX_SDB_DDR3_256MB_16bit_x2_Rev1.inc: this is the setup script used by the DDR Stress Test tool, derived from the setup aid&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 11.0pt;"&gt;imximage_old.cfg: this is the cfg file with the default values that will boot the board&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 11.0pt;"&gt;imximage_new.cfg: this is the cfg file with all of the changes from the DDR Stress Test tool script and the output of the config; this will not allow the target to boot, unless I change&amp;nbsp;&lt;SPAN&gt;MMDC_MPDGCTRL0 (0x021B083C) back to the default value, then it will boot&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 11.0pt;"&gt;&lt;SPAN&gt;I.MX6SX_DDR3_Script_Aid_V0.01.xlsx: this is the setup aid I downloaded from NXP and filled in the values&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 11.0pt;"&gt;Can anyone please help steer me to the correct path? Why did I get a value that will not allow the board to boot? Thanks...&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 28 Nov 2017 21:38:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/DDR-Config-tool-gave-invalid-value/m-p/741320#M115365</guid>
      <dc:creator>davidpatton</dc:creator>
      <dc:date>2017-11-28T21:38:18Z</dc:date>
    </item>
    <item>
      <title>Re: DDR Config tool gave invalid value</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/DDR-Config-tool-gave-invalid-value/m-p/741321#M115366</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi David&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;seems there is misprint when editing imximage.cfg :&lt;/P&gt;&lt;P&gt;ddr tool log&amp;nbsp; suggested value : MPDGCTRL0 = 0x01300124&lt;BR /&gt;while in imximage_new.cfg.zip :&lt;BR /&gt;/*&amp;nbsp;&amp;nbsp; Read DQS Gating calibration*/&lt;BR /&gt;DATA 4 0x021b083c 0x13000124&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 29 Nov 2017 07:56:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/DDR-Config-tool-gave-invalid-value/m-p/741321#M115366</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2017-11-29T07:56:08Z</dc:date>
    </item>
    <item>
      <title>Re: DDR Config tool gave invalid value</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/DDR-Config-tool-gave-invalid-value/m-p/741322#M115367</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Wow! Much thanks!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 29 Nov 2017 19:59:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/DDR-Config-tool-gave-invalid-value/m-p/741322#M115367</guid>
      <dc:creator>davidpatton</dc:creator>
      <dc:date>2017-11-29T19:59:14Z</dc:date>
    </item>
  </channel>
</rss>