<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic USB Hub Support using iMX7 Dual Sabre Board in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/USB-Hub-Support-using-iMX7-Dual-Sabre-Board/m-p/740681#M115266</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi everyone,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am using the imx7d sabre board for development. I trying to have multiple usb mass storage devices mounted to the system via a usb hub. But debug messages give read error and there is no sdx device shown using the lsblk command.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The mass storage devices can be mounted well to the system by direction i.e. without usb hub. The USB hub is FE2.1&amp;nbsp;USB 2.0 HIGH SPEED 7-PORT HUB CONTROLLER. And I am using the Buildroot 2018.02 for my development.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Any advice? Thanks.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Chris Tsang&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 17 Apr 2018 09:14:47 GMT</pubDate>
    <dc:creator>christsang</dc:creator>
    <dc:date>2018-04-17T09:14:47Z</dc:date>
    <item>
      <title>USB Hub Support using iMX7 Dual Sabre Board</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/USB-Hub-Support-using-iMX7-Dual-Sabre-Board/m-p/740681#M115266</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi everyone,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am using the imx7d sabre board for development. I trying to have multiple usb mass storage devices mounted to the system via a usb hub. But debug messages give read error and there is no sdx device shown using the lsblk command.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The mass storage devices can be mounted well to the system by direction i.e. without usb hub. The USB hub is FE2.1&amp;nbsp;USB 2.0 HIGH SPEED 7-PORT HUB CONTROLLER. And I am using the Buildroot 2018.02 for my development.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Any advice? Thanks.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Chris Tsang&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 17 Apr 2018 09:14:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/USB-Hub-Support-using-iMX7-Dual-Sabre-Board/m-p/740681#M115266</guid>
      <dc:creator>christsang</dc:creator>
      <dc:date>2018-04-17T09:14:47Z</dc:date>
    </item>
    <item>
      <title>Re: USB Hub Support using iMX7 Dual Sabre Board</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/USB-Hub-Support-using-iMX7-Dual-Sabre-Board/m-p/740682#M115267</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Here is the log:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;root@imx7dsabresd:~# random: nonblocking pool is initialized&lt;BR /&gt;usb 1-1: new high-speed USB device number 7 using ci_hdrc&lt;BR /&gt;usb 1-1: device not accepting address 7, error -71&lt;BR /&gt;usb 1-1: new high-speed USB device number 9 using ci_hdrc&lt;BR /&gt;hub 1-1:1.0: USB hub found&lt;BR /&gt;hub 1-1:1.0: 7 ports detected&lt;BR /&gt;usb 1-1: USB disconnect, device number 9&lt;BR /&gt;usb usb1-port1: cannot reset (err = -32)&lt;BR /&gt;usb usb1-port1: cannot reset (err = -32)&lt;BR /&gt;usb usb1-port1: cannot reset (err = -32)&lt;BR /&gt;usb usb1-port1: cannot reset (err = -32)&lt;BR /&gt;usb usb1-port1: cannot reset (err = -32)&lt;BR /&gt;usb usb1-port1: Cannot enable. Maybe the USB cable is bad?&lt;BR /&gt;usb usb1-port1: cannot reset (err = -32)&lt;BR /&gt;usb usb1-port1: cannot reset (err = -32)&lt;BR /&gt;usb usb1-port1: cannot reset (err = -32)&lt;BR /&gt;usb usb1-port1: cannot reset (err = -32)&lt;BR /&gt;usb usb1-port1: cannot reset (err = -32)&lt;BR /&gt;usb usb1-port1: Cannot enable. Maybe the USB cable is bad?&lt;BR /&gt;usb usb1-port1: cannot reset (err = -32)&lt;BR /&gt;usb usb1-port1: cannot reset (err = -32)&lt;BR /&gt;usb usb1-port1: cannot reset (err = -32)&lt;BR /&gt;usb usb1-port1: cannot reset (err = -32)&lt;BR /&gt;usb usb1-port1: cannot reset (err = -32)&lt;BR /&gt;usb usb1-port1: Cannot enable. Maybe the USB cable is bad?&lt;BR /&gt;usb usb1-port1: cannot reset (err = -32)&lt;BR /&gt;usb usb1-port1: cannot reset (err = -32)&lt;BR /&gt;usb usb1-port1: cannot reset (err = -32)&lt;BR /&gt;usb usb1-port1: cannot reset (err = -32)&lt;BR /&gt;usb usb1-port1: cannot reset (err = -32)&lt;BR /&gt;usb usb1-port1: Cannot enable. Maybe the USB cable is bad?&lt;BR /&gt;usb usb1-port1: unable to enumerate USB device&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 18 Apr 2018 02:20:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/USB-Hub-Support-using-iMX7-Dual-Sabre-Board/m-p/740682#M115267</guid>
      <dc:creator>christsang</dc:creator>
      <dc:date>2018-04-18T02:20:11Z</dc:date>
    </item>
    <item>
      <title>Re: USB Hub Support using iMX7 Dual Sabre Board</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/USB-Hub-Support-using-iMX7-Dual-Sabre-Board/m-p/740683#M115268</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Chris,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Check if this issue is not due to PMIC, I saw before but for i.mx6q:&lt;/P&gt;&lt;PRE&gt;ARM: imx6qdl-sabresd: set swbst_reg as vbus's parent reg&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; USB vbus 5V is from PMIC SWBST, so set swbst_reg as vbus's&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; parent reg, it fixed a bug that the voltage of vbus is incorrect&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; due to swbst_reg is disabled after boots up.&lt;/PRE&gt;&lt;PRE&gt;&lt;/PRE&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 18 Apr 2018 14:11:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/USB-Hub-Support-using-iMX7-Dual-Sabre-Board/m-p/740683#M115268</guid>
      <dc:creator>Bio_TICFSL</dc:creator>
      <dc:date>2018-04-18T14:11:58Z</dc:date>
    </item>
    <item>
      <title>Re: USB Hub Support using iMX7 Dual Sabre Board</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/USB-Hub-Support-using-iMX7-Dual-Sabre-Board/m-p/740684#M115269</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Bio, so you mean that may be a hardware issue due to the incorrect voltage at the vbus? Or you mean swbst_reg should be set to other voltage?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 30 Apr 2018 08:09:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/USB-Hub-Support-using-iMX7-Dual-Sabre-Board/m-p/740684#M115269</guid>
      <dc:creator>christsang</dc:creator>
      <dc:date>2018-04-30T08:09:37Z</dc:date>
    </item>
    <item>
      <title>Re: USB Hub Support using iMX7 Dual Sabre Board</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/USB-Hub-Support-using-iMX7-Dual-Sabre-Board/m-p/740685#M115270</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi everyone, I have found the root cause for this problem. I just add dc power to the usb hub and it works properly on the imx7 sabre board now.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 04 May 2018 09:24:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/USB-Hub-Support-using-iMX7-Dual-Sabre-Board/m-p/740685#M115270</guid>
      <dc:creator>christsang</dc:creator>
      <dc:date>2018-05-04T09:24:30Z</dc:date>
    </item>
  </channel>
</rss>