<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processorsのトピックbootstrap mx 233</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/bootstrap-mx-233/m-p/738706#M114968</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;1) Question #1: Is there a way to bootstrap the i.MX233 from serial jtag?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We'd like to automatically program our hardware, which uses an i.MX233 as it's main MCU. The examples I see use USB or SD, but in the volumes we do it, we prefer to use a more automated approach, such as JTAG.&lt;/P&gt;&lt;P&gt;We need SD as well as JTAG and they are sharing pins.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;2) Question #2: I read about HW_DIGCTL_CTRL_USE_SERIAL_JTAG, but I cannot work out if that is enabled or disabled by "factory defaults". Is this set or not set when shipped?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;3) Question #3: jtag feature flash ram&lt;/P&gt;&lt;P&gt;I also assume - based from experience with different cpus - that I can use the JTAG to write to the built-in flash memory and reset the mcu and tell it to boot from built-in flash?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Conrad&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 21 Dec 2017 11:54:11 GMT</pubDate>
    <dc:creator>conradwood</dc:creator>
    <dc:date>2017-12-21T11:54:11Z</dc:date>
    <item>
      <title>bootstrap mx 233</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/bootstrap-mx-233/m-p/738706#M114968</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;1) Question #1: Is there a way to bootstrap the i.MX233 from serial jtag?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We'd like to automatically program our hardware, which uses an i.MX233 as it's main MCU. The examples I see use USB or SD, but in the volumes we do it, we prefer to use a more automated approach, such as JTAG.&lt;/P&gt;&lt;P&gt;We need SD as well as JTAG and they are sharing pins.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;2) Question #2: I read about HW_DIGCTL_CTRL_USE_SERIAL_JTAG, but I cannot work out if that is enabled or disabled by "factory defaults". Is this set or not set when shipped?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;3) Question #3: jtag feature flash ram&lt;/P&gt;&lt;P&gt;I also assume - based from experience with different cpus - that I can use the JTAG to write to the built-in flash memory and reset the mcu and tell it to boot from built-in flash?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Conrad&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 21 Dec 2017 11:54:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/bootstrap-mx-233/m-p/738706#M114968</guid>
      <dc:creator>conradwood</dc:creator>
      <dc:date>2017-12-21T11:54:11Z</dc:date>
    </item>
    <item>
      <title>Re: bootstrap mx 233</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/bootstrap-mx-233/m-p/738707#M114969</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Conrad&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;1. no&lt;/P&gt;&lt;P&gt;2. "factory defaults" to serial jtag enabled&lt;/P&gt;&lt;P&gt;3. i.MX23 has not built-in flash memory, except fuses (OTP).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;for programming images one can look on mfg tool:&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="https://www.nxp.com/support/developer-resources/software-development-tools/i.mx-developer-resources/i.mx23-evaluation-kit:IMX23EVK?tab=Design_Tools_Tab" title="https://www.nxp.com/support/developer-resources/software-development-tools/i.mx-developer-resources/i.mx23-evaluation-kit:IMX23EVK?tab=Design_Tools_Tab"&gt;i.MX23 Evaluation Kit|NXP&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;or reuse i.MX28 OBDS baremetal examples (folder /drivers/fuse)&lt;/P&gt;&lt;P&gt;Lab and Test Software (3)&lt;BR /&gt;On-Board Diagnostic Suit for the i.MX28(REV 1)&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="https://www.nxp.com/products/processors-and-microcontrollers/applications-processors/i.mx-applications-processors/i.mx28-processors/multimedia-applications-processors-dual-ethernet-dual-can-lcd-touch-screen-arm9-core:i.MX287?tab=Design_Tools_Tab" title="https://www.nxp.com/products/processors-and-microcontrollers/applications-processors/i.mx-applications-processors/i.mx28-processors/multimedia-applications-processors-dual-ethernet-dual-can-lcd-touch-screen-arm9-core:i.MX287?tab=Design_Tools_Tab"&gt;i.MX287 Processors|Dual Ethernet|NXP&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 04 Jan 2018 02:14:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/bootstrap-mx-233/m-p/738707#M114969</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2018-01-04T02:14:17Z</dc:date>
    </item>
  </channel>
</rss>