<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: IMX6 Overlay resolution set in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/IMX6-Overlay-resolution-set/m-p/738124#M114865</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;one can try to use the FBIOPUET_VSCREENINFO, for more detailed information, pls refer to the link as below:&lt;/P&gt;&lt;P style="margin-bottom: .0001pt;"&gt;&lt;SPAN style="font-size: 10.0pt;"&gt;&lt;A class="jive-link-wiki-small" data-containerid="2004" data-containertype="14" data-objectid="328548" data-objecttype="102" href="https://community.nxp.com/docs/DOC-328548"&gt;https://community.nxp.com/docs/DOC-328548&lt;/A&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P style="margin-bottom: .0001pt;"&gt;&lt;SPAN style="font-size: 10.0pt;"&gt;focus on the &lt;/SPAN&gt;&lt;SPAN style="font-size: 10.0pt; color: black;"&gt;mxc_v4l2_tvin test source code.&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 08 Nov 2017 09:07:38 GMT</pubDate>
    <dc:creator>joanxie</dc:creator>
    <dc:date>2017-11-08T09:07:38Z</dc:date>
    <item>
      <title>IMX6 Overlay resolution set</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX6-Overlay-resolution-set/m-p/738123#M114864</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi all,&lt;/P&gt;&lt;P&gt;how to set the overlay resolution /dev/fb1 to a default value. Currently it is showing as 320x240. saw the dummy values set in&amp;nbsp;&lt;A class="link-titled" href="https://github.com/boundarydevices/linux-imx6/blob/boundary-imx_3.14.28_1.0.0_ga/drivers/video/mxc/mxc_ipuv3_fb.c#L2708" title="https://github.com/boundarydevices/linux-imx6/blob/boundary-imx_3.14.28_1.0.0_ga/drivers/video/mxc/mxc_ipuv3_fb.c#L2708"&gt;linux-imx6/mxc_ipuv3_fb.c at boundary-imx_3.14.28_1.0.0_ga · boundarydevices/linux-imx6 · GitHub&lt;/A&gt;&amp;nbsp;. Changed this to 1600x900 , but its coming as 1280x720. I tested with "fbset -xres 1600 -yres 900 -fb /dev/fb1" and is working. But fbset does'n make any change if i call this from init-script. Is there a way to hard-code the resolution, or any IOCTL call toset the overlay resolution&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 31 Oct 2017 16:47:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX6-Overlay-resolution-set/m-p/738123#M114864</guid>
      <dc:creator>anjojohn</dc:creator>
      <dc:date>2017-10-31T16:47:43Z</dc:date>
    </item>
    <item>
      <title>Re: IMX6 Overlay resolution set</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX6-Overlay-resolution-set/m-p/738124#M114865</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;one can try to use the FBIOPUET_VSCREENINFO, for more detailed information, pls refer to the link as below:&lt;/P&gt;&lt;P style="margin-bottom: .0001pt;"&gt;&lt;SPAN style="font-size: 10.0pt;"&gt;&lt;A class="jive-link-wiki-small" data-containerid="2004" data-containertype="14" data-objectid="328548" data-objecttype="102" href="https://community.nxp.com/docs/DOC-328548"&gt;https://community.nxp.com/docs/DOC-328548&lt;/A&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P style="margin-bottom: .0001pt;"&gt;&lt;SPAN style="font-size: 10.0pt;"&gt;focus on the &lt;/SPAN&gt;&lt;SPAN style="font-size: 10.0pt; color: black;"&gt;mxc_v4l2_tvin test source code.&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 08 Nov 2017 09:07:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX6-Overlay-resolution-set/m-p/738124#M114865</guid>
      <dc:creator>joanxie</dc:creator>
      <dc:date>2017-11-08T09:07:38Z</dc:date>
    </item>
  </channel>
</rss>