<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: Does u-boot run in RAM or in the boot device ?</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Does-u-boot-run-in-RAM-or-in-the-boot-device/m-p/738122#M114863</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Ran&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;early initialization is done in ROM using Device Configuration Data (DCD),&lt;/P&gt;&lt;P&gt;described in Boot Chapter of Reference Manual.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 06 Mar 2018 23:57:06 GMT</pubDate>
    <dc:creator>igorpadykov</dc:creator>
    <dc:date>2018-03-06T23:57:06Z</dc:date>
    <item>
      <title>Does u-boot run in RAM or in the boot device ?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Does-u-boot-run-in-RAM-or-in-the-boot-device/m-p/738119#M114860</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I try to get better understanding of u-boot initialization.&lt;/P&gt;&lt;P&gt;From my reading, it seems that there are 2 methods of boot:&lt;/P&gt;&lt;P&gt;1. boot the u-boot.imx from the device boot&lt;/P&gt;&lt;P&gt;2. boot spl which initialize ddr, and then load u-boot from the boot device (into DDR?) ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;As to (1) option above, is it that u-boot runs in the boot device or in RAM ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Another question:&lt;/P&gt;&lt;P&gt;what's the purpose of pmic and rtc initalization (with i2c) ?&lt;/P&gt;&lt;P&gt;Why can't kernel do that ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you,&lt;/P&gt;&lt;P&gt;Ran&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 19 Jan 2018 15:33:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Does-u-boot-run-in-RAM-or-in-the-boot-device/m-p/738119#M114860</guid>
      <dc:creator>rans</dc:creator>
      <dc:date>2018-01-19T15:33:51Z</dc:date>
    </item>
    <item>
      <title>Re: Does u-boot run in RAM or in the boot device ?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Does-u-boot-run-in-RAM-or-in-the-boot-device/m-p/738120#M114861</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Ran&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;you are right, there are two uboot versions: directly run uboot and two steps process,&lt;BR /&gt;first "spl" small loader then it initializes chip peripherals and run remaining uboot.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Purpose of uboot pmic and rtc initalization (with i2c) is to prepare necessary pmic&lt;BR /&gt;voltages for running linux. It is convenient to do this in uboot, not kernel, so any kernel image&lt;BR /&gt;could be portable and be able to run on different uboot versions/boards,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 19 Jan 2018 23:25:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Does-u-boot-run-in-RAM-or-in-the-boot-device/m-p/738120#M114861</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2018-01-19T23:25:24Z</dc:date>
    </item>
    <item>
      <title>Re: Does u-boot run in RAM or in the boot device ?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Does-u-boot-run-in-RAM-or-in-the-boot-device/m-p/738121#M114862</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Igor,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;So, in imx6 there is no "early u-boot", but only one u-boot , Right ?&lt;/P&gt;&lt;P&gt;Does it run from RAM ? If so, who initialized RAM before u-boot was loaded to RAM ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;ranran&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 06 Mar 2018 20:54:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Does-u-boot-run-in-RAM-or-in-the-boot-device/m-p/738121#M114862</guid>
      <dc:creator>rans</dc:creator>
      <dc:date>2018-03-06T20:54:09Z</dc:date>
    </item>
    <item>
      <title>Re: Does u-boot run in RAM or in the boot device ?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Does-u-boot-run-in-RAM-or-in-the-boot-device/m-p/738122#M114863</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Ran&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;early initialization is done in ROM using Device Configuration Data (DCD),&lt;/P&gt;&lt;P&gt;described in Boot Chapter of Reference Manual.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 06 Mar 2018 23:57:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Does-u-boot-run-in-RAM-or-in-the-boot-device/m-p/738122#M114863</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2018-03-06T23:57:06Z</dc:date>
    </item>
  </channel>
</rss>