<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: spi4-slave register in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/spi4-slave-register/m-p/738097#M114854</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;thank you,so i can only use mosi miso pclk,is that right?&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 28 Mar 2018 06:46:12 GMT</pubDate>
    <dc:creator>leihe</dc:creator>
    <dc:date>2018-03-28T06:46:12Z</dc:date>
    <item>
      <title>spi4-slave register</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/spi4-slave-register/m-p/738095#M114852</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;I have a problem in spi driver ,platform is imx6D6AVT&amp;amp;&amp;amp;linux3.0.35,I can't get rx Interrupt when using&amp;nbsp; spi4 as salve mode,the hardware connection is EIM_A25,EIM_D21,&lt;SPAN&gt;EIM_D22,,EIM_D28,so i mustchose SS1 as chip select?&amp;nbsp; ECSPI4_CONREG:0x00f0e101;&amp;nbsp; &amp;nbsp;ECSPI4_CONFIGREG:0x00f00000; ECSPIx_INTREG=0xf8,is this config avalible?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/19124iDD0971452310D4A4/image-size/large?v=v2&amp;amp;px=999" title="08dd1a3f677f3149a01f406b79db84af.png" alt="08dd1a3f677f3149a01f406b79db84af.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/20712iE5B16F811E453385/image-size/large?v=v2&amp;amp;px=999" title="webwxgetmsgimg.jpg" alt="webwxgetmsgimg.jpg" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;I can only get&amp;nbsp;TXFIFO Empty Interrupt,when ECSPIx_INTREG=0xff,so I write 0x1 to ECSPI4_TXDATA&amp;nbsp; to stop it,if&amp;nbsp;&lt;SPAN&gt;TXDATA buffer is not NULL,how can i start read bytes from master,by&amp;nbsp;setting ECSPIx_CONREG xch bit with 1?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;thank you!!!&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 27 Mar 2018 08:05:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/spi4-slave-register/m-p/738095#M114852</guid>
      <dc:creator>leihe</dc:creator>
      <dc:date>2018-03-27T08:05:22Z</dc:date>
    </item>
    <item>
      <title>Re: spi4-slave register</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/spi4-slave-register/m-p/738096#M114853</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi lei&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;one can check ERR009535 eCSPI: Burst completion by SS signal in slave mode is not functional&lt;/P&gt;&lt;P&gt;i.MX6DQ Errata &lt;/P&gt;&lt;P&gt;&lt;A href="https://www.nxp.com/docs/en/errata/IMX6DQCE.pdf"&gt;https://www.nxp.com/docs/en/errata/IMX6DQCE.pdf&lt;/A&gt;&lt;/P&gt;&lt;P&gt;mainline slave support&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="http://lists.infradead.org/pipermail/linux-arm-kernel/2017-April/501267.html" title="http://lists.infradead.org/pipermail/linux-arm-kernel/2017-April/501267.html"&gt;[PATCH RFC 5/5] spi: imx: Add support for SPI Slave mode for imx53 and imx6 chips&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 28 Mar 2018 06:09:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/spi4-slave-register/m-p/738096#M114853</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2018-03-28T06:09:48Z</dc:date>
    </item>
    <item>
      <title>Re: spi4-slave register</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/spi4-slave-register/m-p/738097#M114854</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;thank you,so i can only use mosi miso pclk,is that right?&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 28 Mar 2018 06:46:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/spi4-slave-register/m-p/738097#M114854</guid>
      <dc:creator>leihe</dc:creator>
      <dc:date>2018-03-28T06:46:12Z</dc:date>
    </item>
  </channel>
</rss>