<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 Adding Python-twisted in yocto build</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Adding-Python-twisted-in-yocto-build/m-p/736483#M114614</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I have added python-twisted in local.conf&lt;/P&gt;&lt;P&gt;IMAGE_INSTALL_append = " python-twisted"&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;now when i run following command on build os on my board&lt;/P&gt;&lt;P&gt;pip list&lt;/P&gt;&lt;P&gt;I get that twisted v17.9.0 is present&lt;/P&gt;&lt;P&gt;but when i try to run an application which requires python twisted ,twisted asks for dependencies (hyperlink,six,autobahn,automat etc.)&lt;/P&gt;&lt;P&gt;so i have to download packages on my board and install them or by connecting board to internet and install twisted using pip.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;How to install and ensure that all the dependencies required by python-twisted is build during yocto build itself ??&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;regards&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 31 May 2018 03:54:39 GMT</pubDate>
    <dc:creator>sameerarvikar</dc:creator>
    <dc:date>2018-05-31T03:54:39Z</dc:date>
    <item>
      <title>Adding Python-twisted in yocto build</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Adding-Python-twisted-in-yocto-build/m-p/736483#M114614</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I have added python-twisted in local.conf&lt;/P&gt;&lt;P&gt;IMAGE_INSTALL_append = " python-twisted"&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;now when i run following command on build os on my board&lt;/P&gt;&lt;P&gt;pip list&lt;/P&gt;&lt;P&gt;I get that twisted v17.9.0 is present&lt;/P&gt;&lt;P&gt;but when i try to run an application which requires python twisted ,twisted asks for dependencies (hyperlink,six,autobahn,automat etc.)&lt;/P&gt;&lt;P&gt;so i have to download packages on my board and install them or by connecting board to internet and install twisted using pip.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;How to install and ensure that all the dependencies required by python-twisted is build during yocto build itself ??&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;regards&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 31 May 2018 03:54:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Adding-Python-twisted-in-yocto-build/m-p/736483#M114614</guid>
      <dc:creator>sameerarvikar</dc:creator>
      <dc:date>2018-05-31T03:54:39Z</dc:date>
    </item>
    <item>
      <title>Re: Adding Python-twisted in yocto build</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Adding-Python-twisted-in-yocto-build/m-p/736484#M114615</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Sameerarvikar,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Since the dependencies do not have a yocto recipe there is no straightforward way to accomplish this. You could write a recipe that installs them but it’s not implemented on the BSP.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 25 Jun 2018 16:27:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Adding-Python-twisted-in-yocto-build/m-p/736484#M114615</guid>
      <dc:creator>gusarambula</dc:creator>
      <dc:date>2018-06-25T16:27:43Z</dc:date>
    </item>
  </channel>
</rss>