<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 Re: Hardware Codec Resets often when 720P streaming is done using WebRTC on iMX6 Android Marshmallow</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Hardware-Codec-Resets-often-when-720P-streaming-is-done-using/m-p/736309#M114587</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Unfortunately, we cannot provide you that kind of support. For that I recommend you to go with the developer of the application. I apologize for the inconvenience.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Diego.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 16 Feb 2018 00:11:26 GMT</pubDate>
    <dc:creator>diegoadrian</dc:creator>
    <dc:date>2018-02-16T00:11:26Z</dc:date>
    <item>
      <title>Hardware Codec Resets often when 720P streaming is done using WebRTC on iMX6 Android Marshmallow</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Hardware-Codec-Resets-often-when-720P-streaming-is-done-using/m-p/736308#M114586</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&amp;nbsp;&lt;/P&gt;&lt;P&gt;I am trying to develop a video chat system on a custom baseboard which uses iMX6 Quad processor. I use Android Marshmallow as OS. And I use Apprtc a webRTC based application on the android side.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;When I try to stream 640x480, I was able to send and receive video without any glitch. But when I opt to stream 720P streaming, I am able to encode the data and send it to the receiver from iMX6 but decoding is very poor.&lt;/P&gt;&lt;P&gt;The proble is the Hardware codec resets often saying&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;01-22 12:44:13.001 2775 15602 I MediaCodec: [OMX.Freescale.std.video_decoder.avc.v3.hw-based] setting surface generation to 2841646&lt;BR /&gt;01-22 12:44:13.003 2775 15700 I ACodec : Send reorder config(0) to VPU&lt;BR /&gt;01-22 12:44:13.004 15518 15518 W OMXNodeInstance: [2f:Freescale.std._decoder.avc.v3.hw-based] component does not support metadata mode; using fallback&lt;BR /&gt;01-22 12:44:13.005 2775 15700 E ACodec : [OMX.Freescale.std.video_decoder.avc.v3.hw-based] storeMetaDataInBuffers failed w/ err -1010&lt;BR /&gt;01-22 12:44:13.009 15518 15518 E OMXNodeInstance: getConfig(2f:Freescale.std._decoder.avc.v3.hw-based, ConfigCommonOutputCrop(0x700000f)) ERROR: IncorrectStateTransition(0x80001017)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;It happens often that I finally receive only 1 fps.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have verified the capability of the device, that it can encode and decode 720P 30 fps simultaneously, by using a app which records h264 camera streaming and play the h264 encoded video simultaneously.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 12 Feb 2018 05:32:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Hardware-Codec-Resets-often-when-720P-streaming-is-done-using/m-p/736308#M114586</guid>
      <dc:creator>hariprasathgopa</dc:creator>
      <dc:date>2018-02-12T05:32:30Z</dc:date>
    </item>
    <item>
      <title>Re: Hardware Codec Resets often when 720P streaming is done using WebRTC on iMX6 Android Marshmallow</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Hardware-Codec-Resets-often-when-720P-streaming-is-done-using/m-p/736309#M114587</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Unfortunately, we cannot provide you that kind of support. For that I recommend you to go with the developer of the application. I apologize for the inconvenience.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Diego.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 16 Feb 2018 00:11:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Hardware-Codec-Resets-often-when-720P-streaming-is-done-using/m-p/736309#M114587</guid>
      <dc:creator>diegoadrian</dc:creator>
      <dc:date>2018-02-16T00:11:26Z</dc:date>
    </item>
  </channel>
</rss>