<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 frequency lower at high temperature - imx6</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/frequency-lower-at-high-temperature-imx6/m-p/736265#M114577</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;hi all,&lt;/P&gt;&lt;P&gt;i add some work with&amp;nbsp;&amp;nbsp;imx6 and&amp;nbsp; ddr stress test,&lt;/P&gt;&lt;P&gt;the test failed in high temperature above 80 c and i think it's because of the change in the cpu frequency.&lt;/P&gt;&lt;P&gt;i nodes that there is 2 threshold:&lt;/P&gt;&lt;P&gt;passive &amp;amp; critical, and i'm sure i worked above the passive threshold - 80.&amp;nbsp;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;i would like to know what is the specific value of the frequency cpu in this mode?&lt;/P&gt;&lt;P&gt;(when the cpu decided to change the frq)&lt;/P&gt;&lt;P&gt;i like to get some table that show frq VS temp&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;best regards&lt;/P&gt;&lt;P&gt;GG&amp;nbsp; &amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 16 Apr 2018 12:37:00 GMT</pubDate>
    <dc:creator>barakbarak</dc:creator>
    <dc:date>2018-04-16T12:37:00Z</dc:date>
    <item>
      <title>frequency lower at high temperature - imx6</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/frequency-lower-at-high-temperature-imx6/m-p/736265#M114577</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;hi all,&lt;/P&gt;&lt;P&gt;i add some work with&amp;nbsp;&amp;nbsp;imx6 and&amp;nbsp; ddr stress test,&lt;/P&gt;&lt;P&gt;the test failed in high temperature above 80 c and i think it's because of the change in the cpu frequency.&lt;/P&gt;&lt;P&gt;i nodes that there is 2 threshold:&lt;/P&gt;&lt;P&gt;passive &amp;amp; critical, and i'm sure i worked above the passive threshold - 80.&amp;nbsp;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;i would like to know what is the specific value of the frequency cpu in this mode?&lt;/P&gt;&lt;P&gt;(when the cpu decided to change the frq)&lt;/P&gt;&lt;P&gt;i like to get some table that show frq VS temp&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;best regards&lt;/P&gt;&lt;P&gt;GG&amp;nbsp; &amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 16 Apr 2018 12:37:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/frequency-lower-at-high-temperature-imx6/m-p/736265#M114577</guid>
      <dc:creator>barakbarak</dc:creator>
      <dc:date>2018-04-16T12:37:00Z</dc:date>
    </item>
    <item>
      <title>Re: frequency lower at high temperature - imx6</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/frequency-lower-at-high-temperature-imx6/m-p/736266#M114578</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Barak&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;cpu frequency changing behaviour is described in&lt;/P&gt;&lt;P&gt;AN4579 i.MX 6 Series Thermal Management Guidelines&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="https://www.nxp.com/docs/en/application-note/AN4579.pdf" title="https://www.nxp.com/docs/en/application-note/AN4579.pdf"&gt;https://www.nxp.com/docs/en/application-note/AN4579.pdf&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Failures at higher temperatures may mean that the drive strength is too low &lt;BR /&gt;and the signals may not rise/fall fast enough.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 17 Apr 2018 07:35:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/frequency-lower-at-high-temperature-imx6/m-p/736266#M114578</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2018-04-17T07:35:35Z</dc:date>
    </item>
  </channel>
</rss>