<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: adding cups into LTIB</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/adding-cups-into-LTIB/m-p/203525#M11457</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Boundary Devices Sabre Lite!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 22 Oct 2012 13:53:02 GMT</pubDate>
    <dc:creator>TomMorrison</dc:creator>
    <dc:date>2012-10-22T13:53:02Z</dc:date>
    <item>
      <title>adding cups into LTIB</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/adding-cups-into-LTIB/m-p/203520#M11452</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am trying to add the package CUPS into LTIB.&lt;/P&gt;&lt;P&gt;However, I get this error when running scbuild.&lt;/P&gt;&lt;P&gt;I looked into the source file but nothing can be altered to redirect the&amp;nbsp;/lib/ld-linux.so.3 which is in my target filesystem.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;ERROR&lt;/P&gt;&lt;P&gt;Compressing cupsd.man... 56.0%&lt;BR /&gt; 53.4%&lt;BR /&gt; 51.6%&lt;BR /&gt;Converting man pages to HTML...&lt;BR /&gt; cancel.1.gz...&lt;BR /&gt;/lib/ld-linux.so.3: No such file or directory&lt;BR /&gt; cups-config.1.gz...&lt;BR /&gt;/lib/ld-linux.so.3: No such file or directory&lt;BR /&gt; cupstestdsc.1.gz...&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 19 Jan 2012 02:23:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/adding-cups-into-LTIB/m-p/203520#M11452</guid>
      <dc:creator>LeeHong</dc:creator>
      <dc:date>2012-01-19T02:23:59Z</dc:date>
    </item>
    <item>
      <title>Re: adding cups into LTIB</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/adding-cups-into-LTIB/m-p/203521#M11453</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Has anyone solved this problem - I REALLY would like to print captured / encoded images wireless to ad-hoc printer!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 17 Oct 2012 21:18:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/adding-cups-into-LTIB/m-p/203521#M11453</guid>
      <dc:creator>TomMorrison</dc:creator>
      <dc:date>2012-10-17T21:18:17Z</dc:date>
    </item>
    <item>
      <title>Re: adding cups into LTIB</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/adding-cups-into-LTIB/m-p/203522#M11454</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;what is the BSP are you using?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 18 Oct 2012 02:35:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/adding-cups-into-LTIB/m-p/203522#M11454</guid>
      <dc:creator>jimmychan</dc:creator>
      <dc:date>2012-10-18T02:35:55Z</dc:date>
    </item>
    <item>
      <title>Re: adding cups into LTIB</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/adding-cups-into-LTIB/m-p/203523#M11455</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am using the Freescale ER6-1209 release (that looks like came out last week).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I tried incorporating 1.3.11 (1.4.8 had MANY more issues than 1.3.11 did).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;But, even then, there were multiple issues in the cross-compile (e.g.:do not create&lt;/P&gt;&lt;P&gt;the HTML output (because the compiled mantohtml doesn't run on host system)).&lt;/P&gt;&lt;P&gt;And, the final problem that I couldn't seem to get around was install script that&lt;/P&gt;&lt;P&gt;was having dependency issues for lib files (couldn't find them - due to NOT pointing&lt;/P&gt;&lt;P&gt;to the appropriate rootfs).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I gave up after that...for the moment.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;got any suggestions?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;tom&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 18 Oct 2012 13:29:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/adding-cups-into-LTIB/m-p/203523#M11455</guid>
      <dc:creator>TomMorrison</dc:creator>
      <dc:date>2012-10-18T13:29:23Z</dc:date>
    </item>
    <item>
      <title>Re: adding cups into LTIB</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/adding-cups-into-LTIB/m-p/203524#M11456</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;which board are you using?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 22 Oct 2012 06:58:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/adding-cups-into-LTIB/m-p/203524#M11456</guid>
      <dc:creator>jimmychan</dc:creator>
      <dc:date>2012-10-22T06:58:01Z</dc:date>
    </item>
    <item>
      <title>Re: adding cups into LTIB</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/adding-cups-into-LTIB/m-p/203525#M11457</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Boundary Devices Sabre Lite!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 22 Oct 2012 13:53:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/adding-cups-into-LTIB/m-p/203525#M11457</guid>
      <dc:creator>TomMorrison</dc:creator>
      <dc:date>2012-10-22T13:53:02Z</dc:date>
    </item>
    <item>
      <title>Re: adding cups into LTIB</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/adding-cups-into-LTIB/m-p/203526#M11458</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;A class="jx-jive-macro-user" href="https://community.nxp.com/people/pejmankalkhoran"&gt;pejmankalkhoran&lt;/A&gt;, can you help?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 22 Oct 2012 16:34:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/adding-cups-into-LTIB/m-p/203526#M11458</guid>
      <dc:creator>admin</dc:creator>
      <dc:date>2012-10-22T16:34:12Z</dc:date>
    </item>
  </channel>
</rss>