<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックCan iMX6 act as USB Audio Class 2.0 device?</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Can-iMX6-act-as-USB-Audio-Class-2-0-device/m-p/736030#M114551</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I want iMX6 act as a USB audio&amp;nbsp;interface device (Not usb host), but I can't find any information about USB Audio Class in IMX6DQCEC.pdf or IMX6DQRM.pdf. Can iMX6 be configured as&amp;nbsp;USB Audio Class 2.0 device?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;thanks, &lt;BR /&gt;Steven&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 16 Apr 2018 09:52:32 GMT</pubDate>
    <dc:creator>stevenlin001</dc:creator>
    <dc:date>2018-04-16T09:52:32Z</dc:date>
    <item>
      <title>Can iMX6 act as USB Audio Class 2.0 device?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Can-iMX6-act-as-USB-Audio-Class-2-0-device/m-p/736030#M114551</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I want iMX6 act as a USB audio&amp;nbsp;interface device (Not usb host), but I can't find any information about USB Audio Class in IMX6DQCEC.pdf or IMX6DQRM.pdf. Can iMX6 be configured as&amp;nbsp;USB Audio Class 2.0 device?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;thanks, &lt;BR /&gt;Steven&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 16 Apr 2018 09:52:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Can-iMX6-act-as-USB-Audio-Class-2-0-device/m-p/736030#M114551</guid>
      <dc:creator>stevenlin001</dc:creator>
      <dc:date>2018-04-16T09:52:32Z</dc:date>
    </item>
    <item>
      <title>Re: Can iMX6 act as USB Audio Class 2.0 device?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Can-iMX6-act-as-USB-Audio-Class-2-0-device/m-p/736031#M114552</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Both (Linux and Android) BSPs for i.MX6 does support USB Audio.&lt;BR /&gt;And also i.MX6 can be configured as USB Audio device. Please look at g_audio module.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a great day,&lt;BR /&gt;Victor&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 19 Apr 2018 06:03:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Can-iMX6-act-as-USB-Audio-Class-2-0-device/m-p/736031#M114552</guid>
      <dc:creator>b36401</dc:creator>
      <dc:date>2018-04-19T06:03:30Z</dc:date>
    </item>
  </channel>
</rss>