<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: Unbelievable errors when compiling udev-90 to realize automatic mounting</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Unbelievable-errors-when-compiling-udev-90-to-realize-automatic/m-p/735926#M114528</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Yang Lv,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;This error looks a bit like the one described on the following thread:&lt;/P&gt;&lt;P&gt;&lt;A _jive_internal="true" href="https://community.nxp.com/thread/329263"&gt;https://community.nxp.com/thread/329263&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;However, in this case you seem to be using a the right path for the sysroots and the cross compiler but I would recommend making sure that a simple Hello World can be compiled. Are you using the toolchain from the L4.1.15_2.0.1_ga BSP?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 16 Apr 2018 17:33:17 GMT</pubDate>
    <dc:creator>gusarambula</dc:creator>
    <dc:date>2018-04-16T17:33:17Z</dc:date>
    <item>
      <title>Unbelievable errors when compiling udev-90 to realize automatic mounting</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Unbelievable-errors-when-compiling-udev-90-to-realize-automatic/m-p/735925#M114527</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;STRONG&gt;Hi,&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;I have downloaded and built Freescale release L4.1.15_2.0.1_ga yocto project&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Now,i want to&amp;nbsp;compile udev-90 to realize automatic mounting.&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;I try to modify the original Makefile in udev-90(dir),but some unbelievable following errors stoped me ruthlessly.&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;I need your help, my dear friend.&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Error:&lt;/STRONG&gt;&lt;BR /&gt;&lt;EM&gt;/opt/fuyanSourceCode/fuyanSDK/sysroot/x86_64-pokysdk-linux/usr/libexec/arm-poky-linux-gnueabi/gcc/arm-poky-linux-gnueabi/5.3.0/real-ld:cannot find crt1.o:No such file or directory&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;/opt/fuyanSourceCode/fuyanSDK/sysroot/x86_64-pokysdk-linux/usr/libexec/arm-poky-linux-gnueabi/gcc/arm-poky-linux-gnueabi/5.3.0/real-ld:cannot find crti.o:No such file or directory&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;/opt/fuyanSourceCode/fuyanSDK/sysroot/x86_64-pokysdk-linux/usr/libexec/arm-poky-linux-gnueabi/gcc/arm-poky-linux-gnueabi/5.3.0/real-ld:cannot find crtbegin.o:No such file or directory&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;/opt/fuyanSourceCode/fuyanSDK/sysroot/x86_64-pokysdk-linux/usr/libexec/arm-poky-linux-gnueabi/gcc/arm-poky-linux-gnueabi/5.3.0/real-ld:cannot find -lgcc&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;/opt/fuyanSourceCode/fuyanSDK/sysroot/x86_64-pokysdk-linux/usr/libexec/arm-poky-linux-gnueabi/gcc/arm-poky-linux-gnueabi/5.3.0/real-ld:cannot find -lgcc_s&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;/opt/fuyanSourceCode/fuyanSDK/sysroot/x86_64-pokysdk-linux/usr/libexec/arm-poky-linux-gnueabi/gcc/arm-poky-linux-gnueabi/5.3.0/real-ld:cannot find -lc&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;/opt/fuyanSourceCode/fuyanSDK/sysroot/x86_64-pokysdk-linux/usr/libexec/arm-poky-linux-gnueabi/gcc/arm-poky-linux-gnueabi/5.3.0/real-ld:cannot find -lgcc&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;/opt/fuyanSourceCode/fuyanSDK/sysroot/x86_64-pokysdk-linux/usr/libexec/arm-poky-linux-gnueabi/gcc/arm-poky-linux-gnueabi/5.3.0/real-ld:cannot find -lgcc_s&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;/opt/fuyanSourceCode/fuyanSDK/sysroot/x86_64-pokysdk-linux/usr/libexec/arm-poky-linux-gnueabi/gcc/arm-poky-linux-gnueabi/5.3.0/real-ld:cannot find crtn.o:No such file or directory&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;/opt/fuyanSourceCode/fuyanSDK/sysroot/x86_64-pokysdk-linux/usr/libexec/arm-poky-linux-gnueabi/gcc/arm-poky-linux-gnueabi/5.3.0/real-ld:cannot find crtend.o:No such file or directory&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Makefile (red line part is added by me)&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/9857i17BFC7EEC0A7A803/image-size/large?v=v2&amp;amp;px=999" title="捕获.JPG" alt="捕获.JPG" /&gt;&lt;/span&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/9864i09B9142593AB1E03/image-size/large?v=v2&amp;amp;px=999" title="捕获.JPG" alt="捕获.JPG" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 16 Apr 2018 06:53:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Unbelievable-errors-when-compiling-udev-90-to-realize-automatic/m-p/735925#M114527</guid>
      <dc:creator>yanglv</dc:creator>
      <dc:date>2018-04-16T06:53:39Z</dc:date>
    </item>
    <item>
      <title>Re: Unbelievable errors when compiling udev-90 to realize automatic mounting</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Unbelievable-errors-when-compiling-udev-90-to-realize-automatic/m-p/735926#M114528</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Yang Lv,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;This error looks a bit like the one described on the following thread:&lt;/P&gt;&lt;P&gt;&lt;A _jive_internal="true" href="https://community.nxp.com/thread/329263"&gt;https://community.nxp.com/thread/329263&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;However, in this case you seem to be using a the right path for the sysroots and the cross compiler but I would recommend making sure that a simple Hello World can be compiled. Are you using the toolchain from the L4.1.15_2.0.1_ga BSP?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 16 Apr 2018 17:33:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Unbelievable-errors-when-compiling-udev-90-to-realize-automatic/m-p/735926#M114528</guid>
      <dc:creator>gusarambula</dc:creator>
      <dc:date>2018-04-16T17:33:17Z</dc:date>
    </item>
  </channel>
</rss>