<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: U-boot loading fails on LS2088 in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/U-boot-loading-fails-on-LS2088/m-p/734203#M114259</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I tried to remove the RAM from slot, cleaned it up and tried again. It worked. Dont know what the issue is but it works again now.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 02 Nov 2017 13:14:45 GMT</pubDate>
    <dc:creator>vijaykumardesai</dc:creator>
    <dc:date>2017-11-02T13:14:45Z</dc:date>
    <item>
      <title>U-boot loading fails on LS2088</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/U-boot-loading-fails-on-LS2088/m-p/734201#M114257</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;When I powerup the LS2088 board, I get an error from the U-boot as described below.&lt;/P&gt;&lt;P&gt;I use the default u-boot available in the board.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Can someone help me understand what the issue is?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;U-Boot 2016.01LS2088A-SDK+g1179f5b (Dec 21 2016 - 21:23:49 +0800)&lt;/P&gt;&lt;P&gt;SoC: LS2088E Version:1.0 (0x87090010)&lt;BR /&gt;Clock Configuration:&lt;BR /&gt; CPU0(A72):1800 MHz CPU1(A72):1800 MHz CPU2(A72):1800 MHz&lt;BR /&gt; CPU3(A72):1800 MHz CPU4(A72):1800 MHz CPU5(A72):1800 MHz&lt;BR /&gt; CPU6(A72):1800 MHz CPU7(A72):1800 MHz&lt;BR /&gt; Bus: 700 MHz DDR: 1866.667 MT/s DP-DDR: 1600 MT/s&lt;BR /&gt;Reset Configuration Word (RCW):&lt;BR /&gt; 00000000: 483038b8 48480048 00000000 00000000&lt;BR /&gt; 00000010: 00000000 00000000 00a00000 00000000&lt;BR /&gt; 00000020: 01001180 00002581 00000000 00000000&lt;BR /&gt; 00000030: 00000c0b 00000000 00000000 00000000&lt;BR /&gt; 00000040: 00000000 00000000 00000000 00000000&lt;BR /&gt; 00000050: 00000000 00000000 00000000 00000000&lt;BR /&gt; 00000060: 00000000 00000000 00027000 00000000&lt;BR /&gt; 00000070: 412a0000 00000000 00000000 00000000&lt;BR /&gt;I2C: ready&lt;BR /&gt;Model: Freescale Layerscape 2085a RDB Board&lt;BR /&gt;Board: LS2085A/LS2088A-RDB, Board Arch: V1, Board version: F, boot from vBank: 0&lt;BR /&gt;FPGA: v1.22&lt;BR /&gt;SERDES1 Reference : Clock1 = 156.25MHz Clock2 = 156.25MHz&lt;BR /&gt;SERDES2 Reference : Clock1 = 100MHz Clock2 = 100MHz&lt;BR /&gt;DRAM: Initializing DDR....using SPD&lt;BR /&gt;wait_for_sr_state: Arbitration lost sr=92 cr=0 state=2020&lt;BR /&gt;i2c_init_transfer: failed for chip 0x36 retry=0&lt;BR /&gt;wait_for_sr_state: Arbitration lost sr=92 cr=0 state=2020&lt;BR /&gt;i2c_init_transfer: failed for chip 0x36 retry=1&lt;BR /&gt;wait_for_sr_state: Arbitration lost sr=92 cr=0 state=2020&lt;BR /&gt;i2c_init_transfer: failed for chip 0x36 retry=2&lt;BR /&gt;i2c_init_transfer: give up i2c_regs=0x2000000&lt;BR /&gt;wait_for_sr_state: Arbitration lost sr=92 cr=0 state=2020&lt;BR /&gt;i2c_init_transfer: failed for chip 0x51 retry=0&lt;BR /&gt;wait_for_sr_state: Arbitration lost sr=92 cr=0 state=2020&lt;BR /&gt;i2c_init_transfer: failed for chip 0x51 retry=1&lt;BR /&gt;wait_for_sr_state: Arbitration lost sr=92 cr=0 state=2020&lt;BR /&gt;i2c_init_transfer: failed for chip 0x51 retry=2&lt;BR /&gt;i2c_init_transfer: give up i2c_regs=0x2000000&lt;BR /&gt;DDR: failed to read SPD from address 81&lt;BR /&gt;wait_for_sr_state: failed sr=a0 cr=0 state=2000&lt;BR /&gt;wait_for_sr_state: failed sr=a0 cr=0 state=2000&lt;BR /&gt;i2c_imx_stop:trigger stop failed&lt;BR /&gt;i2c_init_transfer: failed for chip 0x36 retry=0&lt;BR /&gt;wait_for_sr_state: failed sr=a0 cr=0 state=2000&lt;BR /&gt;wait_for_sr_state: failed sr=a0 cr=0 state=2000&lt;BR /&gt;i2c_imx_stop:trigger stop failed&lt;BR /&gt;i2c_init_transfer: failed for chip 0x36 retry=1&lt;BR /&gt;wait_for_sr_state: failed sr=a0 cr=0 state=2000&lt;BR /&gt;wait_for_sr_state: failed sr=a0 cr=0 state=2000&lt;BR /&gt;i2c_imx_stop:trigger stop failed&lt;BR /&gt;i2c_init_transfer: failed for chip 0x36 retry=2&lt;BR /&gt;i2c_init_transfer: give up i2c_regs=0x2000000&lt;BR /&gt;wait_for_sr_state: failed sr=a0 cr=0 state=2000&lt;BR /&gt;wait_for_sr_state: failed sr=a0 cr=0 state=2000&lt;BR /&gt;i2c_imx_stop:trigger stop failed&lt;BR /&gt;i2c_init_transfer: failed for chip 0x52 retry=0&lt;BR /&gt;wait_for_sr_state: failed sr=a0 cr=0 state=2000&lt;BR /&gt;wait_for_sr_state: failed sr=a0 cr=0 state=2000&lt;BR /&gt;i2c_imx_stop:trigger stop failed&lt;BR /&gt;i2c_init_transfer: failed for chip 0x52 retry=1&lt;BR /&gt;wait_for_sr_state: failed sr=a0 cr=0 state=2000&lt;BR /&gt;wait_for_sr_state: failed sr=a0 cr=0 state=2000&lt;BR /&gt;i2c_imx_stop:trigger stop failed&lt;BR /&gt;i2c_init_transfer: failed for chip 0x52 retry=2&lt;BR /&gt;i2c_init_transfer: give up i2c_regs=0x2000000&lt;BR /&gt;wait_for_sr_state: failed sr=a0 cr=0 state=2000&lt;BR /&gt;wait_for_sr_state: failed sr=a0 cr=0 state=2000&lt;BR /&gt;i2c_imx_stop:trigger stop failed&lt;BR /&gt;i2c_init_transfer: failed for chip 0x36 retry=0&lt;BR /&gt;wait_for_sr_state: failed sr=a0 cr=0 state=2000&lt;BR /&gt;wait_for_sr_state: failed sr=a0 cr=0 state=2000&lt;BR /&gt;i2c_imx_stop:trigger stop failed&lt;BR /&gt;i2c_init_transfer: failed for chip 0x36 retry=1&lt;BR /&gt;wait_for_sr_state: failed sr=a0 cr=0 state=2000&lt;BR /&gt;wait_for_sr_state: failed sr=a0 cr=0 state=2000&lt;BR /&gt;i2c_imx_stop:trigger stop failed&lt;BR /&gt;i2c_init_transfer: failed for chip 0x36 retry=2&lt;BR /&gt;i2c_init_transfer: give up i2c_regs=0x2000000&lt;BR /&gt;wait_for_sr_state: failed sr=a0 cr=0 state=2000&lt;BR /&gt;wait_for_sr_state: failed sr=a0 cr=0 state=2000&lt;BR /&gt;i2c_imx_stop:trigger stop failed&lt;BR /&gt;i2c_init_transfer: failed for chip 0x53 retry=0&lt;BR /&gt;wait_for_sr_state: failed sr=a0 cr=0 state=2000&lt;BR /&gt;wait_for_sr_state: failed sr=a0 cr=0 state=2000&lt;BR /&gt;i2c_imx_stop:trigger stop failed&lt;BR /&gt;i2c_init_transfer: failed for chip 0x53 retry=1&lt;BR /&gt;wait_for_sr_state: failed sr=a0 cr=0 state=2000&lt;BR /&gt;wait_for_sr_state: failed sr=a0 cr=0 state=2000&lt;BR /&gt;i2c_imx_stop:trigger stop failed&lt;BR /&gt;i2c_init_transfer: failed for chip 0x53 retry=2&lt;BR /&gt;i2c_init_transfer: give up i2c_regs=0x2000000&lt;BR /&gt;wait_for_sr_state: failed sr=a0 cr=0 state=2000&lt;BR /&gt;wait_for_sr_state: failed sr=a0 cr=0 state=2000&lt;BR /&gt;i2c_imx_stop:trigger stop failed&lt;BR /&gt;i2c_init_transfer: failed for chip 0x36 retry=0&lt;BR /&gt;wait_for_sr_state: failed sr=a0 cr=0 state=2000&lt;BR /&gt;wait_for_sr_state: failed sr=a0 cr=0 state=2000&lt;BR /&gt;i2c_imx_stop:trigger stop failed&lt;BR /&gt;i2c_init_transfer: failed for chip 0x36 retry=1&lt;BR /&gt;wait_for_sr_state: failed sr=a0 cr=0 state=2000&lt;BR /&gt;wait_for_sr_state: failed sr=a0 cr=0 state=2000&lt;BR /&gt;i2c_imx_stop:trigger stop failed&lt;BR /&gt;i2c_init_transfer: failed for chip 0x36 retry=2&lt;BR /&gt;i2c_init_transfer: give up i2c_regs=0x2000000&lt;BR /&gt;wait_for_sr_state: failed sr=a0 cr=0 state=2000&lt;BR /&gt;wait_for_sr_state: failed sr=a0 cr=0 state=2000&lt;BR /&gt;i2c_imx_stop:trigger stop failed&lt;BR /&gt;i2c_init_transfer: failed for chip 0x54 retry=0&lt;BR /&gt;wait_for_sr_state: failed sr=a0 cr=0 state=2000&lt;BR /&gt;wait_for_sr_state: failed sr=a0 cr=0 state=2000&lt;BR /&gt;i2c_imx_stop:trigger stop failed&lt;BR /&gt;i2c_init_transfer: failed for chip 0x54 retry=1&lt;BR /&gt;wait_for_sr_state: failed sr=a0 cr=0 state=2000&lt;BR /&gt;wait_for_sr_state: failed sr=a0 cr=0 state=2000&lt;BR /&gt;i2c_imx_stop:trigger stop failed&lt;BR /&gt;i2c_init_transfer: failed for chip 0x54 retry=2&lt;BR /&gt;i2c_init_transfer: give up i2c_regs=0x2000000&lt;BR /&gt;Error: No valid SPD detected.&lt;BR /&gt;DP-DDR: wait_for_sr_state: failed sr=a0 cr=0 state=2000&lt;BR /&gt;wait_for_sr_state: failed sr=a0 cr=0 state=2000&lt;BR /&gt;i2c_imx_stop:trigger stop failed&lt;BR /&gt;i2c_init_transfer: failed for chip 0x36 retry=0&lt;BR /&gt;wait_for_sr_state: failed sr=a0 cr=0 state=2000&lt;BR /&gt;wait_for_sr_state: failed sr=a0 cr=0 state=2000&lt;BR /&gt;i2c_imx_stop:trigger stop failed&lt;BR /&gt;i2c_init_transfer: failed for chip 0x36 retry=1&lt;BR /&gt;wait_for_sr_state: failed sr=a0 cr=0 state=2000&lt;BR /&gt;wait_for_sr_state: failed sr=a0 cr=0 state=2000&lt;BR /&gt;i2c_imx_stop:trigger stop failed&lt;BR /&gt;i2c_init_transfer: failed for chip 0x36 retry=2&lt;BR /&gt;i2c_init_transfer: give up i2c_regs=0x2000000&lt;BR /&gt;wait_for_sr_state: failed sr=a0 cr=0 state=2000&lt;BR /&gt;wait_for_sr_state: failed sr=a0 cr=0 state=2000&lt;BR /&gt;i2c_imx_stop:trigger stop failed&lt;BR /&gt;i2c_init_transfer: failed for chip 0x55 retry=0&lt;BR /&gt;wait_for_sr_state: failed sr=a0 cr=0 state=2000&lt;BR /&gt;wait_for_sr_state: failed sr=a0 cr=0 state=2000&lt;BR /&gt;i2c_imx_stop:trigger stop failed&lt;BR /&gt;i2c_init_transfer: failed for chip 0x55 retry=1&lt;BR /&gt;wait_for_sr_state: failed sr=a0 cr=0 state=2000&lt;BR /&gt;wait_for_sr_state: failed sr=a0 cr=0 state=2000&lt;BR /&gt;i2c_imx_stop:trigger stop failed&lt;BR /&gt;i2c_init_transfer: failed for chip 0x55 retry=2&lt;BR /&gt;i2c_init_transfer: give up i2c_regs=0x2000000&lt;BR /&gt;Not detected16 EiB&lt;BR /&gt;DDR 16 EiB (DDR not enabled)&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 30 Oct 2017 12:56:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/U-boot-loading-fails-on-LS2088/m-p/734201#M114257</guid>
      <dc:creator>vijaykumardesai</dc:creator>
      <dc:date>2017-10-30T12:56:00Z</dc:date>
    </item>
    <item>
      <title>Re: U-boot loading fails on LS2088</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/U-boot-loading-fails-on-LS2088/m-p/734202#M114258</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Please create a Technical Case referring the following thread:&lt;/P&gt;&lt;P&gt;&lt;A class="jive-link-external-small" href="https://community.nxp.com/external-link.jspa?url=https%3A%2F%2Fcommunity.freescale.com%2Fthread%2F381898" rel="nofollow" target="_blank"&gt;https://community.freescale.com/thread/381898&lt;/A&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 31 Oct 2017 03:03:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/U-boot-loading-fails-on-LS2088/m-p/734202#M114258</guid>
      <dc:creator>ufedor</dc:creator>
      <dc:date>2017-10-31T03:03:24Z</dc:date>
    </item>
    <item>
      <title>Re: U-boot loading fails on LS2088</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/U-boot-loading-fails-on-LS2088/m-p/734203#M114259</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I tried to remove the RAM from slot, cleaned it up and tried again. It worked. Dont know what the issue is but it works again now.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 02 Nov 2017 13:14:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/U-boot-loading-fails-on-LS2088/m-p/734203#M114259</guid>
      <dc:creator>vijaykumardesai</dc:creator>
      <dc:date>2017-11-02T13:14:45Z</dc:date>
    </item>
  </channel>
</rss>