<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: Modify Linux Kernel source code</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Modify-Linux-Kernel-source-code/m-p/733846#M114216</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Alfio,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;if you want to customize kernel you need to have your own build and add a new layer to your yocto image. Please take a look to the following training. &lt;A href="https://community.nxp.com/docs/DOC-94849"&gt;Yocto Training - HOME&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Regards,&lt;BR /&gt;Carlos&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 31 Oct 2017 15:02:11 GMT</pubDate>
    <dc:creator>Carlos_Musich</dc:creator>
    <dc:date>2017-10-31T15:02:11Z</dc:date>
    <item>
      <title>Modify Linux Kernel source code</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Modify-Linux-Kernel-source-code/m-p/733845#M114215</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Good afternoon,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have some question about Linux development for imx6/7 boards inside the Yocto framework.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;What are the steps I need to follow to:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;1. Build and deploy to an sdcard an Image with different configurations (with respect to the pre-built ones provided by nxp which I already tested)&lt;/P&gt;&lt;P&gt;2. Modify Linux kernel sources or add custom modules and, build and deploy the custom Image to the sdcard&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Sorry in advance for the very basic questions but I am not so familiar with Linux on embedded platforms (I would appreciate a lot any pointer to doc material)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks in advance&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 30 Oct 2017 13:49:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Modify-Linux-Kernel-source-code/m-p/733845#M114215</guid>
      <dc:creator>adimauro</dc:creator>
      <dc:date>2017-10-30T13:49:01Z</dc:date>
    </item>
    <item>
      <title>Re: Modify Linux Kernel source code</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Modify-Linux-Kernel-source-code/m-p/733846#M114216</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Alfio,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;if you want to customize kernel you need to have your own build and add a new layer to your yocto image. Please take a look to the following training. &lt;A href="https://community.nxp.com/docs/DOC-94849"&gt;Yocto Training - HOME&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Regards,&lt;BR /&gt;Carlos&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 31 Oct 2017 15:02:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Modify-Linux-Kernel-source-code/m-p/733846#M114216</guid>
      <dc:creator>Carlos_Musich</dc:creator>
      <dc:date>2017-10-31T15:02:11Z</dc:date>
    </item>
  </channel>
</rss>