<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: MIPI DBI support on i.MX6 Solo</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/MIPI-DBI-support-on-i-MX6-Solo/m-p/733639#M114159</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Daniel&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;one can look at linux drivers/video/fbdev/mxc/mipi_dsi.c for&lt;/P&gt;&lt;P&gt;"MIPI_DSI_CMD_MODE_CFG". DBI-2 interface is used for smart display&lt;/P&gt;&lt;P&gt;and command and data should be sent from IPU ASYNC port. Unfortunately&lt;/P&gt;&lt;P&gt;in i.MX6DQ/SDL IPU there is no support for IPU Asynchronous Interface (i.MX53 IPU&lt;/P&gt;&lt;P&gt;has such interface).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 01 Nov 2017 09:26:40 GMT</pubDate>
    <dc:creator>igorpadykov</dc:creator>
    <dc:date>2017-11-01T09:26:40Z</dc:date>
    <item>
      <title>MIPI DBI support on i.MX6 Solo</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/MIPI-DBI-support-on-i-MX6-Solo/m-p/733638#M114158</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;On the i.mx6Solo part, the MIPI_DSI section specifically calls out both generic read/writes and DBI read/writes for DCS commands.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The System Overview section of the reference manual (42.2.1) makes it look like the DBI FIFOs which would be used for a DCS read/write are not accessible via the MIPI DSI registers defined in section 42.6.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;At the moment I am trying to interlace DCS commands (reads and writes) between video packets as called out in the MIPI standards.&amp;nbsp;When I send the commands with video mode enabled (MIPI_DSI_VID_MODE_CFG&amp;nbsp;with en_video_mode&amp;nbsp;set to 1, and vid_mode_type set to 3), I can see that the DBI read FIFO (MIPI_DSI_CMD_PKT_STATUS: dbi_pld_r_empty ) now reports not empty when I do reads, but how do I get the actual data from the FIFO?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is there a memory area somewhere that is the DBI DCS command read and write FIFOs that is accessible?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Or is there a reason that the DCS read/writes using the generic FIFO does not work when video is enabled?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 30 Oct 2017 18:52:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/MIPI-DBI-support-on-i-MX6-Solo/m-p/733638#M114158</guid>
      <dc:creator>danielherring</dc:creator>
      <dc:date>2017-10-30T18:52:11Z</dc:date>
    </item>
    <item>
      <title>Re: MIPI DBI support on i.MX6 Solo</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/MIPI-DBI-support-on-i-MX6-Solo/m-p/733639#M114159</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Daniel&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;one can look at linux drivers/video/fbdev/mxc/mipi_dsi.c for&lt;/P&gt;&lt;P&gt;"MIPI_DSI_CMD_MODE_CFG". DBI-2 interface is used for smart display&lt;/P&gt;&lt;P&gt;and command and data should be sent from IPU ASYNC port. Unfortunately&lt;/P&gt;&lt;P&gt;in i.MX6DQ/SDL IPU there is no support for IPU Asynchronous Interface (i.MX53 IPU&lt;/P&gt;&lt;P&gt;has such interface).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 01 Nov 2017 09:26:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/MIPI-DBI-support-on-i-MX6-Solo/m-p/733639#M114159</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2017-11-01T09:26:40Z</dc:date>
    </item>
  </channel>
</rss>