<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Timing for Boot mode configuration pins in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Timing-for-Boot-mode-configuration-pins/m-p/733536#M114147</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Boris&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;yes true, also it will take some time for locking plls, prepare system clocks are read fuses.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;from sect.6.5.6.1.2.2 COLD RESET:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Once the reset source deasserts, system_early_rst_b reset is deasserted after at least 2&lt;BR /&gt;XTALI clocks. The system_early_rst_b is used for the CCM and PLL-IPs to start&lt;BR /&gt;generating PLL clock outputs and the system root clocks.&lt;BR /&gt;Once the system root clocks are ready, the CCM will assert system_clk_ready signal.&lt;BR /&gt;This signal is generated during the start sequence in the CCM and it involves the&lt;BR /&gt;preparation of the PLLs to generate clock roots for functional operation.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;from sect.6.5.6.3.1 BOOT_MODE Pin Latching:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The value of the BOOT_MODE pins will be latched after the OCOTP_CTRL asserts the&lt;BR /&gt;fuse read completion flag. After latching, the values of the BOOT_MODE pins are used&lt;BR /&gt;to determine the booting options of the core as described in the SRC_SBMRx registers.&lt;BR /&gt;The boot mode general purpose bits can be provided to the SRC from either e-fuses or&lt;BR /&gt;GPIO signals. The gpio_bt_sel e-fuse defines the source to be used to derive the boot&lt;BR /&gt;information. When gpio_bt_sel is set, e-fuses are used. When cleared, GPIO signals are&lt;BR /&gt;used.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 10 May 2018 06:33:44 GMT</pubDate>
    <dc:creator>igorpadykov</dc:creator>
    <dc:date>2018-05-10T06:33:44Z</dc:date>
    <item>
      <title>Timing for Boot mode configuration pins</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Timing-for-Boot-mode-configuration-pins/m-p/733533#M114144</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;In our new project with iMX8, part of the boot mode configuration pins (BOOT_MODE0/1, SAI1_TXD1, SAI1_TXD4, and SAI1_TXD5) will be changed during active reset (I mean when POR_B input us low), but before rising edge of the POR_B it's will get the necessary value.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;According to reference manual of iMX8 for BOOT_MODE0 and BOOT_MODE1, it's OK&lt;/P&gt;&lt;P&gt;Paragraph "6.1.2.1 Boot mode pin settings": The BOOT_MODE is initialized by sampling the BOOT_MODE0 and BOOT_MODE1 inputs on the rising edge of the POR_B.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is this rule valid for other boot configuration pins also?&lt;/P&gt;&lt;P&gt;Thank You,&lt;/P&gt;&lt;P&gt;Boris&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 08 May 2018 14:13:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Timing-for-Boot-mode-configuration-pins/m-p/733533#M114144</guid>
      <dc:creator>borisberman</dc:creator>
      <dc:date>2018-05-08T14:13:43Z</dc:date>
    </item>
    <item>
      <title>Re: Timing for Boot mode configuration pins</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Timing-for-Boot-mode-configuration-pins/m-p/733534#M114145</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Boris&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;for other pins it is not the same, sect.6.5.6.1.2.1 POR (SRC_POR_B)&lt;/P&gt;&lt;P&gt;i.MX8MDQ Reference Manual describes timings which enables OCOTP_CTRL and fusebox,&lt;/P&gt;&lt;P&gt;they later are used for sampling boot configuration and reading from fuses.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;&lt;A class="jive-link-external-small" href="https://community.nxp.com/external-link.jspa?url=https%3A%2F%2Fwww.nxp.com%2Fdocs%2Fen%2Freference-manual%2FIMX8MDQLQRM.pdf" rel="nofollow" target="_blank"&gt;https://www.nxp.com/docs/en/reference-manual/IMX8MDQLQRM.pdf&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 08 May 2018 23:20:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Timing-for-Boot-mode-configuration-pins/m-p/733534#M114145</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2018-05-08T23:20:22Z</dc:date>
    </item>
    <item>
      <title>Re: Timing for Boot mode configuration pins</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Timing-for-Boot-mode-configuration-pins/m-p/733535#M114146</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Igor,&lt;/P&gt;&lt;P&gt;Thank You for your fast answer!&lt;/P&gt;&lt;P&gt;From sect.6.5.6.1.2. of i.MX8MDQ Reference Manual i understood that OCOTP_CTRL and fusebox clocks will be enabled after more than 2 XTALI clocks since reset signal (In my case POR_B pin) de-assertion.&lt;/P&gt;&lt;P&gt;Is this true conclusion?&lt;/P&gt;&lt;P&gt;Thank you&lt;/P&gt;&lt;P&gt;Boris&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 09 May 2018 11:51:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Timing-for-Boot-mode-configuration-pins/m-p/733535#M114146</guid>
      <dc:creator>borisberman</dc:creator>
      <dc:date>2018-05-09T11:51:54Z</dc:date>
    </item>
    <item>
      <title>Re: Timing for Boot mode configuration pins</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Timing-for-Boot-mode-configuration-pins/m-p/733536#M114147</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Boris&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;yes true, also it will take some time for locking plls, prepare system clocks are read fuses.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;from sect.6.5.6.1.2.2 COLD RESET:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Once the reset source deasserts, system_early_rst_b reset is deasserted after at least 2&lt;BR /&gt;XTALI clocks. The system_early_rst_b is used for the CCM and PLL-IPs to start&lt;BR /&gt;generating PLL clock outputs and the system root clocks.&lt;BR /&gt;Once the system root clocks are ready, the CCM will assert system_clk_ready signal.&lt;BR /&gt;This signal is generated during the start sequence in the CCM and it involves the&lt;BR /&gt;preparation of the PLLs to generate clock roots for functional operation.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;from sect.6.5.6.3.1 BOOT_MODE Pin Latching:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The value of the BOOT_MODE pins will be latched after the OCOTP_CTRL asserts the&lt;BR /&gt;fuse read completion flag. After latching, the values of the BOOT_MODE pins are used&lt;BR /&gt;to determine the booting options of the core as described in the SRC_SBMRx registers.&lt;BR /&gt;The boot mode general purpose bits can be provided to the SRC from either e-fuses or&lt;BR /&gt;GPIO signals. The gpio_bt_sel e-fuse defines the source to be used to derive the boot&lt;BR /&gt;information. When gpio_bt_sel is set, e-fuses are used. When cleared, GPIO signals are&lt;BR /&gt;used.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 10 May 2018 06:33:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Timing-for-Boot-mode-configuration-pins/m-p/733536#M114147</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2018-05-10T06:33:44Z</dc:date>
    </item>
  </channel>
</rss>