<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: MII Connection problem</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/MII-Connection-problem/m-p/732919#M114078</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi &amp;nbsp;Alessandro&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;one can recheck enet power supplies connections using&lt;/P&gt;&lt;P&gt;i.MX6SX Datasheet Table 110. 19x19 mm Functional Contact Assignments&lt;/P&gt;&lt;P&gt;"Power Group" column&lt;BR /&gt;&lt;A href="https://www.nxp.com/docs/en/data-sheet/IMX6SXCEC.pdf"&gt;https://www.nxp.com/docs/en/data-sheet/IMX6SXCEC.pdf&lt;/A&gt;&lt;/P&gt;&lt;P&gt;Also one can look for layout errors and short circuit between traces.&lt;/P&gt;&lt;P&gt;3.3V is allowable value according to Table 10. Operating Ranges i.MX6SX Datasheet.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 17 Jan 2018 23:42:36 GMT</pubDate>
    <dc:creator>igorpadykov</dc:creator>
    <dc:date>2018-01-17T23:42:36Z</dc:date>
    <item>
      <title>MII Connection problem</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/MII-Connection-problem/m-p/732918#M114077</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I have a custom board(designed by us) based on IMX6 SoloX. This board has (among other) two optical ports 100-FX, realized connecting a micrel KSZ8873FLLI via MII to the SoloX.&lt;/P&gt;&lt;P&gt;The problem is that I found an unexpected electrical level on the MII interface in TX direction. I would like the high level to be 3.3V, but on the oscilloscope I quite often can see a stable level around 2 volts.&lt;/P&gt;&lt;P&gt;So on the TX line I can see 3 different voltage level: 3.3V (expected igh level), 2V (unexpected and unwanted high level), and 0V (low level).&lt;/P&gt;&lt;P&gt;Of course with this condition the port is not working.&lt;/P&gt;&lt;P&gt;My question are:&lt;/P&gt;&lt;P&gt;1) Is it possibile for the SoloX to work with an MII interface with 3.3V as high level ? The reference manual is not very clear on this topic.&lt;/P&gt;&lt;P&gt;2) If yes, how the&amp;nbsp;NVCC_SGMII should be connected ?&lt;/P&gt;&lt;P&gt;3) What can cause this strange 3 level signal ?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 17 Jan 2018 12:48:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/MII-Connection-problem/m-p/732918#M114077</guid>
      <dc:creator>alessandromaggi</dc:creator>
      <dc:date>2018-01-17T12:48:43Z</dc:date>
    </item>
    <item>
      <title>Re: MII Connection problem</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/MII-Connection-problem/m-p/732919#M114078</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi &amp;nbsp;Alessandro&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;one can recheck enet power supplies connections using&lt;/P&gt;&lt;P&gt;i.MX6SX Datasheet Table 110. 19x19 mm Functional Contact Assignments&lt;/P&gt;&lt;P&gt;"Power Group" column&lt;BR /&gt;&lt;A href="https://www.nxp.com/docs/en/data-sheet/IMX6SXCEC.pdf"&gt;https://www.nxp.com/docs/en/data-sheet/IMX6SXCEC.pdf&lt;/A&gt;&lt;/P&gt;&lt;P&gt;Also one can look for layout errors and short circuit between traces.&lt;/P&gt;&lt;P&gt;3.3V is allowable value according to Table 10. Operating Ranges i.MX6SX Datasheet.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 17 Jan 2018 23:42:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/MII-Connection-problem/m-p/732919#M114078</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2018-01-17T23:42:36Z</dc:date>
    </item>
  </channel>
</rss>