<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: imx28 custom board does not boot in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/imx28-custom-board-does-not-boot/m-p/732601#M114005</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Jill&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;one can test board with obds and jtag, it has simple usb tests.&lt;/P&gt;&lt;P&gt;Also may be useful to check:&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/docs/DOC-95515"&gt;Application note sharing: Issues often met in i.MX28 application&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 14 Feb 2018 23:27:26 GMT</pubDate>
    <dc:creator>igorpadykov</dc:creator>
    <dc:date>2018-02-14T23:27:26Z</dc:date>
    <item>
      <title>imx28 custom board does not boot</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx28-custom-board-does-not-boot/m-p/732597#M114001</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;the board is based imx28evk schematics. voltages look good. the board seems behave correctly when it is read from JTAG (but cannot be written). It does not response to USB connection (mfgtool shows not being able to place the processor to a special mode). there is no output from the debug UART.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Will there be any output if the board is configured to boot from NAND but the NAND is empty? Or any thing I can check to see if the processor is running or not?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 09 Feb 2018 02:55:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx28-custom-board-does-not-boot/m-p/732597#M114001</guid>
      <dc:creator>jlu</dc:creator>
      <dc:date>2018-02-09T02:55:33Z</dc:date>
    </item>
    <item>
      <title>Re: imx28 custom board does not boot</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx28-custom-board-does-not-boot/m-p/732598#M114002</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;no. nothing from the debug UART&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 09 Feb 2018 22:23:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx28-custom-board-does-not-boot/m-p/732598#M114002</guid>
      <dc:creator>jlu</dc:creator>
      <dc:date>2018-02-09T22:23:08Z</dc:date>
    </item>
    <item>
      <title>Re: imx28 custom board does not boot</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx28-custom-board-does-not-boot/m-p/732599#M114003</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi jlu&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;first recommended to test memory&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/docs/DOC-1455"&gt;Board Bring-up and DDR Initialization Tools&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/thread/385077"&gt;DDR2 Calibration and Stress Test for i.MX28&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;and test other peripherals with obds&lt;/P&gt;&lt;P&gt;Lab and Test Software (1)&lt;BR /&gt;On-Board Diagnostic Suit for the i.MX28&lt;BR /&gt;&lt;A href="https://www.nxp.com/support/developer-resources/software-development-tools/i.mx-developer-resources/i.mx28-evaluation-kit:MCIMX28EVKJ?tab=Design_Tools_Tab"&gt;https://www.nxp.com/support/developer-resources/software-development-tools/i.mx-developer-resources/i.mx28-evaluation-kit:MCIMX28EVKJ?tab=Design_Tools_Tab&lt;/A&gt;&lt;/P&gt;&lt;P&gt;Program nand image with mfg tools found on above link&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 09 Feb 2018 23:08:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx28-custom-board-does-not-boot/m-p/732599#M114003</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2018-02-09T23:08:17Z</dc:date>
    </item>
    <item>
      <title>Re: imx28 custom board does not boot</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx28-custom-board-does-not-boot/m-p/732600#M114004</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Igor,&lt;/P&gt;&lt;P&gt;thank you for reply.&lt;/P&gt;&lt;P&gt;we have followed each step to bring up the voltages, and we don't see apparent wrong, but we are not able to get the board running as we expect.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;there are some limitations on this board:&lt;/P&gt;&lt;P&gt;1) it only runs on battery (4.2V). there is no 5V connection;&amp;nbsp;&lt;/P&gt;&lt;P&gt;2) it does not have SD card. it is designed to run on NAND, with USB port to download the firmware&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Now when we connect the board with USB port, mfgtool shows there is no device connected. So we can't download firmware into the NAND. As the consequence, we can't do any further test.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Why MFGTOOL cannot see the USB when on battery only? How mfgtool detects the device?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;thank you,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Jill&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 14 Feb 2018 21:13:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx28-custom-board-does-not-boot/m-p/732600#M114004</guid>
      <dc:creator>jlu</dc:creator>
      <dc:date>2018-02-14T21:13:10Z</dc:date>
    </item>
    <item>
      <title>Re: imx28 custom board does not boot</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx28-custom-board-does-not-boot/m-p/732601#M114005</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Jill&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;one can test board with obds and jtag, it has simple usb tests.&lt;/P&gt;&lt;P&gt;Also may be useful to check:&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/docs/DOC-95515"&gt;Application note sharing: Issues often met in i.MX28 application&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 14 Feb 2018 23:27:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx28-custom-board-does-not-boot/m-p/732601#M114005</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2018-02-14T23:27:26Z</dc:date>
    </item>
  </channel>
</rss>