<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: MCIMX7SABRE  cross compiler</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/MCIMX7SABRE-cross-compiler/m-p/732163#M113931</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Raghavendra,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am not an expert in C#,&amp;nbsp; but in order to have the DLL file to be used in an application under the Target, the library need to be crosscompile for the i.MX7&amp;nbsp; using the ARM tool Chain,&amp;nbsp; available in the Linux BSP.&amp;nbsp; I do not have the details on how to do the cross compile for a DLL in C#, but this is what you need to do.&amp;nbsp; I apologize .&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;TIC&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 05 Dec 2017 14:56:38 GMT</pubDate>
    <dc:creator>jamesbone</dc:creator>
    <dc:date>2017-12-05T14:56:38Z</dc:date>
    <item>
      <title>MCIMX7SABRE  cross compiler</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/MCIMX7SABRE-cross-compiler/m-p/732162#M113930</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, I'm running c# application with Mono in linux and i need to provide one linux system call DLL for that application&amp;gt; I'm using NXP MCIMX7SABRE board to deploy with Linux. So i need to know the extra library which i want to link with which compiler i should produce. Cross compiler is Necessary ? if yes please provide details which i can use.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks in Advance&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 24 Nov 2017 06:30:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/MCIMX7SABRE-cross-compiler/m-p/732162#M113930</guid>
      <dc:creator>raghavendrapati</dc:creator>
      <dc:date>2017-11-24T06:30:00Z</dc:date>
    </item>
    <item>
      <title>Re: MCIMX7SABRE  cross compiler</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/MCIMX7SABRE-cross-compiler/m-p/732163#M113931</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Raghavendra,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am not an expert in C#,&amp;nbsp; but in order to have the DLL file to be used in an application under the Target, the library need to be crosscompile for the i.MX7&amp;nbsp; using the ARM tool Chain,&amp;nbsp; available in the Linux BSP.&amp;nbsp; I do not have the details on how to do the cross compile for a DLL in C#, but this is what you need to do.&amp;nbsp; I apologize .&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;TIC&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 05 Dec 2017 14:56:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/MCIMX7SABRE-cross-compiler/m-p/732163#M113931</guid>
      <dc:creator>jamesbone</dc:creator>
      <dc:date>2017-12-05T14:56:38Z</dc:date>
    </item>
  </channel>
</rss>