<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: How to use V4l2 capture interface for two cameras</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/How-to-use-V4l2-capture-interface-for-two-cameras/m-p/732098#M113912</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;for pcie, pls refer to the document as below:&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/docs/DOC-94541"&gt;https://community.nxp.com/docs/DOC-94541&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 19 Jan 2018 10:12:00 GMT</pubDate>
    <dc:creator>joanxie</dc:creator>
    <dc:date>2018-01-19T10:12:00Z</dc:date>
    <item>
      <title>How to use V4l2 capture interface for two cameras</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/How-to-use-V4l2-capture-interface-for-two-cameras/m-p/732097#M113911</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi All,&lt;/P&gt;&lt;P&gt;For our application we use two video streams from two different camera interfaces like below.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;1. ADV7610 -&amp;gt; parallel CSI -&amp;gt; IPU&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;2. tw6869 -&amp;gt; pcie -&amp;gt; IPU&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;To support zero copying, both video streams are captured through &lt;STRONG&gt;imxv4l2videosrc&lt;/STRONG&gt;&amp;nbsp;of gstreamer. However I have only one v4l2cap node in dts file which is being utilized for parallel csi bus :&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;v4l2_cap_0 {&lt;BR /&gt; &amp;nbsp;&amp;nbsp;&amp;nbsp;compatible = "fsl,imx6q-v4l2-capture";&lt;BR /&gt; &amp;nbsp;&amp;nbsp;&amp;nbsp;ipu_id = &amp;lt;0&amp;gt;;&lt;BR /&gt; &amp;nbsp;&amp;nbsp;&amp;nbsp;csi_id = &amp;lt;0&amp;gt;;&lt;BR /&gt; &amp;nbsp;&amp;nbsp;&amp;nbsp;mclk_source = &amp;lt;0&amp;gt;;&lt;BR /&gt; &amp;nbsp;&amp;nbsp;&amp;nbsp;mipi_camera = &amp;lt;0&amp;gt;;&lt;BR /&gt; &amp;nbsp;&amp;nbsp;&amp;nbsp;default_input = &amp;lt;1&amp;gt;;&lt;BR /&gt; &amp;nbsp;&amp;nbsp;&amp;nbsp;status = "okay";&lt;BR /&gt; };&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;should I need two nodes to achieve simultaneous video streams ?&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;P&gt;Anuradha&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 17 Jan 2018 07:18:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/How-to-use-V4l2-capture-interface-for-two-cameras/m-p/732097#M113911</guid>
      <dc:creator>tengri</dc:creator>
      <dc:date>2018-01-17T07:18:44Z</dc:date>
    </item>
    <item>
      <title>Re: How to use V4l2 capture interface for two cameras</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/How-to-use-V4l2-capture-interface-for-two-cameras/m-p/732098#M113912</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;for pcie, pls refer to the document as below:&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/docs/DOC-94541"&gt;https://community.nxp.com/docs/DOC-94541&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 19 Jan 2018 10:12:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/How-to-use-V4l2-capture-interface-for-two-cameras/m-p/732098#M113912</guid>
      <dc:creator>joanxie</dc:creator>
      <dc:date>2018-01-19T10:12:00Z</dc:date>
    </item>
  </channel>
</rss>