<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: inflexion ui plugin</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/inflexion-ui-plugin/m-p/203061#M11388</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;This query is currently being dealt with in the InflexionUI Community.&lt;/P&gt;&lt;P&gt;&lt;A href="http://communities.mentor.com/mgcx/message/27682#27682" target="_blank"&gt;http://communities.mentor.com/mgcx/message/27682#27682&lt;/A&gt;&lt;/P&gt;&lt;P&gt;Phil.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 19 Jan 2012 11:55:28 GMT</pubDate>
    <dc:creator>PhilBrumby</dc:creator>
    <dc:date>2012-01-19T11:55:28Z</dc:date>
    <item>
      <title>inflexion ui plugin</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/inflexion-ui-plugin/m-p/203060#M11387</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello all&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I try to load the plugin from the demo into my own inflexion ui appliciaton. I add a plugin to my root.template. I refer through Resource-&amp;gt;event handler = "demoPluginElement://" to my &amp;nbsp;ifxui_plugin.plugin file. In the editor the sinewave.png is visible (so I think the reference is good). However when i start up my application on the imx53 QSB, nothing appears. I just the exact same module code from the example and I made the integration layer with my UIintegrator.exe.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I think it has something to do with the startup of the element itself. (Since I checked which functions works with printf()). So I added a touchregion which tried to start the element. which got the&amp;nbsp;IFX_RETURN_STATUS&amp;nbsp;IFXM_ifxuiplugin_ExecuteLink_ButtonLink() function working but still nothing to see on the screen.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Anyone has an idea?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;thanks in advance&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;kind regards&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Lieven&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 17 Jan 2012 15:26:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/inflexion-ui-plugin/m-p/203060#M11387</guid>
      <dc:creator>Lyven</dc:creator>
      <dc:date>2012-01-17T15:26:58Z</dc:date>
    </item>
    <item>
      <title>Re: inflexion ui plugin</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/inflexion-ui-plugin/m-p/203061#M11388</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;This query is currently being dealt with in the InflexionUI Community.&lt;/P&gt;&lt;P&gt;&lt;A href="http://communities.mentor.com/mgcx/message/27682#27682" target="_blank"&gt;http://communities.mentor.com/mgcx/message/27682#27682&lt;/A&gt;&lt;/P&gt;&lt;P&gt;Phil.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 19 Jan 2012 11:55:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/inflexion-ui-plugin/m-p/203061#M11388</guid>
      <dc:creator>PhilBrumby</dc:creator>
      <dc:date>2012-01-19T11:55:28Z</dc:date>
    </item>
  </channel>
</rss>