<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: how to add spi flash driver? in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/how-to-add-spi-flash-driver/m-p/731247#M113754</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;How do I know if this drive is successful? For example, there are specific flags in the “/dev” directory.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 17 Jan 2018 09:40:42 GMT</pubDate>
    <dc:creator>youyong</dc:creator>
    <dc:date>2018-01-17T09:40:42Z</dc:date>
    <item>
      <title>how to add spi flash driver?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/how-to-add-spi-flash-driver/m-p/731245#M113752</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;the cpu is imx6dl,and we need add a driver of AT45DB021E spi flash.but it is not succeed.because it is also nor flash,so i add it like m25p80.c.but the result is as follows images.I can not see it in the "/dev".why?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 17 Jan 2018 06:27:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/how-to-add-spi-flash-driver/m-p/731245#M113752</guid>
      <dc:creator>youyong</dc:creator>
      <dc:date>2018-01-17T06:27:01Z</dc:date>
    </item>
    <item>
      <title>Re: how to add spi flash driver?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/how-to-add-spi-flash-driver/m-p/731246#M113753</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi youyong&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;please check struct spi_device_id spi_nor_ids in linux/drivers/mtd/devices/spi-nor/spi-nor.c&lt;/P&gt;&lt;P&gt;and add necessary model parameters. More details can be found in Chapter 31&lt;BR /&gt;SPI NOR Flash Memory Technology Device (MTD) Driver attached Linux Manual.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 17 Jan 2018 08:06:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/how-to-add-spi-flash-driver/m-p/731246#M113753</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2018-01-17T08:06:28Z</dc:date>
    </item>
    <item>
      <title>Re: how to add spi flash driver?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/how-to-add-spi-flash-driver/m-p/731247#M113754</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;How do I know if this drive is successful? For example, there are specific flags in the “/dev” directory.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 17 Jan 2018 09:40:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/how-to-add-spi-flash-driver/m-p/731247#M113754</guid>
      <dc:creator>youyong</dc:creator>
      <dc:date>2018-01-17T09:40:42Z</dc:date>
    </item>
    <item>
      <title>Re: how to add spi flash driver?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/how-to-add-spi-flash-driver/m-p/731248#M113755</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;having sources, one can debug it using AN4553 Using Open Source Debugging&lt;/P&gt;&lt;P&gt;Tools for Linux on i.MX Processors&lt;BR /&gt;&lt;A class="jive-link-external-small" href="https://community.nxp.com/external-link.jspa?url=https%3A%2F%2Fwww.nxp.com%2Fdocs%2Fen%2Fapplication-note%2FAN4553.pdf" rel="nofollow" target="_blank"&gt;https://www.nxp.com/docs/en/application-note/AN4553.pdf&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;~igor&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 17 Jan 2018 11:12:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/how-to-add-spi-flash-driver/m-p/731248#M113755</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2018-01-17T11:12:23Z</dc:date>
    </item>
  </channel>
</rss>