<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processorsのトピックi.MX6UL Battery Backup</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/i-MX6UL-Battery-Backup/m-p/731096#M113726</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I'm doing a design with the i.MX6UL processor with a coin cell backup for RTC and am needing to draw as little current as possible when there is no system power.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Using the eval board for this processor, I'm seeing the current draw at 300 uA when powered from&amp;nbsp;VDD_COIN_3V.&amp;nbsp; I'm assuming this large current draw is coming from various leakage currents on the design:&lt;/P&gt;&lt;P&gt;&amp;nbsp;- POR_B leakage current on the reset circuitry&lt;/P&gt;&lt;P&gt;&amp;nbsp;- PMIC_ON_REQ leakage current&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm assuming if I use MOSFET's to help isolate these lines during a coin cell only power I can get my coin cell current draw significantly lower?&amp;nbsp; Are there other areas of leakage current I should be concerned about?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 12 Apr 2018 22:23:10 GMT</pubDate>
    <dc:creator>danielfield</dc:creator>
    <dc:date>2018-04-12T22:23:10Z</dc:date>
    <item>
      <title>i.MX6UL Battery Backup</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX6UL-Battery-Backup/m-p/731096#M113726</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I'm doing a design with the i.MX6UL processor with a coin cell backup for RTC and am needing to draw as little current as possible when there is no system power.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Using the eval board for this processor, I'm seeing the current draw at 300 uA when powered from&amp;nbsp;VDD_COIN_3V.&amp;nbsp; I'm assuming this large current draw is coming from various leakage currents on the design:&lt;/P&gt;&lt;P&gt;&amp;nbsp;- POR_B leakage current on the reset circuitry&lt;/P&gt;&lt;P&gt;&amp;nbsp;- PMIC_ON_REQ leakage current&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm assuming if I use MOSFET's to help isolate these lines during a coin cell only power I can get my coin cell current draw significantly lower?&amp;nbsp; Are there other areas of leakage current I should be concerned about?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 12 Apr 2018 22:23:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX6UL-Battery-Backup/m-p/731096#M113726</guid>
      <dc:creator>danielfield</dc:creator>
      <dc:date>2018-04-12T22:23:10Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX6UL Battery Backup</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX6UL-Battery-Backup/m-p/731097#M113727</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Daniel&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;leakage may be caused by some pads which are powered by VSNVS,&lt;/P&gt;&lt;P&gt;this is&amp;nbsp; described in Table 10. Power and decoupling recommendations&lt;/P&gt;&lt;P&gt;Hardware Development Guide for the i.MX 6UltraLite Applications Processor &lt;BR /&gt;&lt;A class="jive-link-external-small" href="https://community.nxp.com/external-link.jspa?url=http%3A%2F%2Fwww.nxp.com%2Fdocs%2Fen%2Fuser-guide%2FIMX6ULHDG.pdf" rel="nofollow" target="_blank"&gt;http://www.nxp.com/docs/en/user-guide/IMX6ULHDG.pdf&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 12 Apr 2018 23:52:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX6UL-Battery-Backup/m-p/731097#M113727</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2018-04-12T23:52:03Z</dc:date>
    </item>
  </channel>
</rss>