<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックHDMI Audio Hotplug detection Issue on IMX6</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/HDMI-Audio-Hotplug-detection-Issue-on-IMX6/m-p/730723#M113659</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I've tried to test HDMI Audio hot plug detection on imx6 board. I'm using mainline-4.14 kernel version &amp;amp; DRM subsystem (drivers/gpu/drm/bridge/synopsys/dw-hdmi-ahb-audio.c)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I've verified following two cases&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;case a:&lt;/STRONG&gt;&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;boot target&lt;/LI&gt;&lt;LI&gt;connect cable&lt;/LI&gt;&lt;LI&gt;play back (No Sound)&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;case b:&lt;/STRONG&gt;&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;boot target&lt;/LI&gt;&lt;LI&gt;play back&lt;/LI&gt;&lt;LI&gt;connect cable (No sound )&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Both, case a &amp;amp; case b are failing only working case is case c,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;case c:&amp;nbsp;&amp;nbsp;&lt;/STRONG&gt; &lt;/P&gt;&lt;UL&gt;&lt;LI&gt;connect cable&lt;/LI&gt;&lt;/UL&gt;&lt;UL&gt;&lt;LI&gt;boot target&lt;/LI&gt;&lt;LI&gt;play back (Can Hear sound)&lt;/LI&gt;&lt;LI&gt;disconnect cable&lt;/LI&gt;&lt;LI&gt;connect it back (Can hear sound)&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is this known issue?&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 06 Mar 2018 09:30:45 GMT</pubDate>
    <dc:creator>vm18553</dc:creator>
    <dc:date>2018-03-06T09:30:45Z</dc:date>
    <item>
      <title>HDMI Audio Hotplug detection Issue on IMX6</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/HDMI-Audio-Hotplug-detection-Issue-on-IMX6/m-p/730723#M113659</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I've tried to test HDMI Audio hot plug detection on imx6 board. I'm using mainline-4.14 kernel version &amp;amp; DRM subsystem (drivers/gpu/drm/bridge/synopsys/dw-hdmi-ahb-audio.c)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I've verified following two cases&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;case a:&lt;/STRONG&gt;&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;boot target&lt;/LI&gt;&lt;LI&gt;connect cable&lt;/LI&gt;&lt;LI&gt;play back (No Sound)&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;case b:&lt;/STRONG&gt;&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;boot target&lt;/LI&gt;&lt;LI&gt;play back&lt;/LI&gt;&lt;LI&gt;connect cable (No sound )&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Both, case a &amp;amp; case b are failing only working case is case c,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;case c:&amp;nbsp;&amp;nbsp;&lt;/STRONG&gt; &lt;/P&gt;&lt;UL&gt;&lt;LI&gt;connect cable&lt;/LI&gt;&lt;/UL&gt;&lt;UL&gt;&lt;LI&gt;boot target&lt;/LI&gt;&lt;LI&gt;play back (Can Hear sound)&lt;/LI&gt;&lt;LI&gt;disconnect cable&lt;/LI&gt;&lt;LI&gt;connect it back (Can hear sound)&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is this known issue?&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 06 Mar 2018 09:30:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/HDMI-Audio-Hotplug-detection-Issue-on-IMX6/m-p/730723#M113659</guid>
      <dc:creator>vm18553</dc:creator>
      <dc:date>2018-03-06T09:30:45Z</dc:date>
    </item>
    <item>
      <title>Re: HDMI Audio Hotplug detection Issue on IMX6</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/HDMI-Audio-Hotplug-detection-Issue-on-IMX6/m-p/730724#M113660</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;pls refer to the link as below, hope helpful for you&lt;/P&gt;&lt;P&gt;&lt;A _jive_internal="true" href="https://community.nxp.com/thread/373572"&gt;https://community.nxp.com/thread/373572&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;A _jive_internal="true" href="https://community.nxp.com/thread/358454#comment-531371"&gt;https://community.nxp.com/thread/358454#comment-531371&lt;/A&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 12 Mar 2018 03:19:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/HDMI-Audio-Hotplug-detection-Issue-on-IMX6/m-p/730724#M113660</guid>
      <dc:creator>joanxie</dc:creator>
      <dc:date>2018-03-12T03:19:16Z</dc:date>
    </item>
  </channel>
</rss>