<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 Using MX8 DDR tool generated code with GA U-Boot</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Using-MX8-DDR-tool-generated-code-with-GA-U-Boot/m-p/728948#M113345</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I used the current MX8 DDR tool to generate DDR training code for U-Boot (ddr_init.c and ddrphy_train.c). The code runs successfully on my custom i.MX8 board with U-Boot from the imx_v2017.03_4.9.51_imx8m_beta branch.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I now updated U-Boot to the NXP imx_v2017.03_4.9.51_imx8m_ga release. But now U-Boot does not work anymore. SPL reports successful training, but hangs when jumping into the main U-Boot code. See the output below.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I updated ATF and imx-mkimage to the GA version. I am using the firmware files from the imx-firmware version 7.4 package.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Should I use an newer version of the DDR tool? If so, where can I get it?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;BLOCKQUOTE class="jive_macro_quote jive-quote jive_text_macro"&gt;&lt;P&gt;U-Boot SPL 2017.03-00838-g8ab673031c2d (Mar 22 2018 - 13:15:37)&lt;BR /&gt;PMIC: PFUZE100 ID=0x10&lt;BR /&gt;check ddr4_pmu_train_imem code&lt;BR /&gt;check ddr4_pmu_train_imem code pass&lt;BR /&gt;check ddr4_pmu_train_dmem code&lt;BR /&gt;check ddr4_pmu_train_dmem code pass&lt;BR /&gt;Training PASS&lt;BR /&gt;Training PASS&lt;BR /&gt;Training PASS&lt;BR /&gt;check ddr4_pmu_train_imem code&lt;BR /&gt;check ddr4_pmu_train_imem code pass&lt;BR /&gt;check ddr4_pmu_train_dmem code&lt;BR /&gt;check ddr4_pmu_train_dmem code pass&lt;BR /&gt;Training PASS&lt;BR /&gt;Normal Boot&lt;BR /&gt;Trying to boot from MMC2&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;baruch&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 22 Mar 2018 13:32:47 GMT</pubDate>
    <dc:creator>baruchsiach</dc:creator>
    <dc:date>2018-03-22T13:32:47Z</dc:date>
    <item>
      <title>Using MX8 DDR tool generated code with GA U-Boot</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Using-MX8-DDR-tool-generated-code-with-GA-U-Boot/m-p/728948#M113345</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I used the current MX8 DDR tool to generate DDR training code for U-Boot (ddr_init.c and ddrphy_train.c). The code runs successfully on my custom i.MX8 board with U-Boot from the imx_v2017.03_4.9.51_imx8m_beta branch.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I now updated U-Boot to the NXP imx_v2017.03_4.9.51_imx8m_ga release. But now U-Boot does not work anymore. SPL reports successful training, but hangs when jumping into the main U-Boot code. See the output below.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I updated ATF and imx-mkimage to the GA version. I am using the firmware files from the imx-firmware version 7.4 package.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Should I use an newer version of the DDR tool? If so, where can I get it?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;BLOCKQUOTE class="jive_macro_quote jive-quote jive_text_macro"&gt;&lt;P&gt;U-Boot SPL 2017.03-00838-g8ab673031c2d (Mar 22 2018 - 13:15:37)&lt;BR /&gt;PMIC: PFUZE100 ID=0x10&lt;BR /&gt;check ddr4_pmu_train_imem code&lt;BR /&gt;check ddr4_pmu_train_imem code pass&lt;BR /&gt;check ddr4_pmu_train_dmem code&lt;BR /&gt;check ddr4_pmu_train_dmem code pass&lt;BR /&gt;Training PASS&lt;BR /&gt;Training PASS&lt;BR /&gt;Training PASS&lt;BR /&gt;check ddr4_pmu_train_imem code&lt;BR /&gt;check ddr4_pmu_train_imem code pass&lt;BR /&gt;check ddr4_pmu_train_dmem code&lt;BR /&gt;check ddr4_pmu_train_dmem code pass&lt;BR /&gt;Training PASS&lt;BR /&gt;Normal Boot&lt;BR /&gt;Trying to boot from MMC2&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;baruch&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 22 Mar 2018 13:32:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Using-MX8-DDR-tool-generated-code-with-GA-U-Boot/m-p/728948#M113345</guid>
      <dc:creator>baruchsiach</dc:creator>
      <dc:date>2018-03-22T13:32:47Z</dc:date>
    </item>
    <item>
      <title>Re: Using MX8 DDR tool generated code with GA U-Boot</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Using-MX8-DDR-tool-generated-code-with-GA-U-Boot/m-p/728949#M113346</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I apologize for the delay.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Which is the revision of your i.MX8M?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Diego.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 10 Apr 2018 15:50:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Using-MX8-DDR-tool-generated-code-with-GA-U-Boot/m-p/728949#M113346</guid>
      <dc:creator>diegoadrian</dc:creator>
      <dc:date>2018-04-10T15:50:46Z</dc:date>
    </item>
    <item>
      <title>Re: Using MX8 DDR tool generated code with GA U-Boot</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Using-MX8-DDR-tool-generated-code-with-GA-U-Boot/m-p/728950#M113347</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Diego,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks for your reply.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The updated DDR script (&lt;SPAN&gt;mx8m_micron_lpddr4_3gb_2d_1600m_334m_32bit.ds&lt;/SPAN&gt;) fixed the issue for me.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/docs/DOC-340179"&gt;https://community.nxp.com/docs/DOC-340179&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;baruch&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 11 Apr 2018 10:50:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Using-MX8-DDR-tool-generated-code-with-GA-U-Boot/m-p/728950#M113347</guid>
      <dc:creator>baruchsiach</dc:creator>
      <dc:date>2018-04-11T10:50:56Z</dc:date>
    </item>
  </channel>
</rss>