<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 Auto-negotiation not complete in 1 Gigabit Ethernet in KSZ9031</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Auto-negotiation-not-complete-in-1-Gigabit-Ethernet-in-KSZ9031/m-p/728071#M113244</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi All,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; I am facing an weird problem in Ethernet when the speed is 1000 Mbps. When I connect my i.MX6 solo board to the&amp;nbsp; LAN port which supports 1 Gbps , the LED on the Ethernet port never blinks or glows.&amp;nbsp; As far as I investigated on this issue the link is not established so the LEDs are off. Software side wen we had a debug we were able to find out that the based on a status variable&amp;nbsp; the link is made up and down. In working case (10/100 Mbps) , the status variable is updated with the value 796D after reading the register MII_BMSR and non-working case the status value is 7949. After decoding the value we could understand that the auto-negotiation is not getting completed in 1000 Mbps.&amp;nbsp; I am not getting any clue to debug this issue forward.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Any one has faced such issue ?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 27 Oct 2017 12:23:05 GMT</pubDate>
    <dc:creator>anjalikkrishna</dc:creator>
    <dc:date>2017-10-27T12:23:05Z</dc:date>
    <item>
      <title>Auto-negotiation not complete in 1 Gigabit Ethernet in KSZ9031</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Auto-negotiation-not-complete-in-1-Gigabit-Ethernet-in-KSZ9031/m-p/728071#M113244</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi All,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; I am facing an weird problem in Ethernet when the speed is 1000 Mbps. When I connect my i.MX6 solo board to the&amp;nbsp; LAN port which supports 1 Gbps , the LED on the Ethernet port never blinks or glows.&amp;nbsp; As far as I investigated on this issue the link is not established so the LEDs are off. Software side wen we had a debug we were able to find out that the based on a status variable&amp;nbsp; the link is made up and down. In working case (10/100 Mbps) , the status variable is updated with the value 796D after reading the register MII_BMSR and non-working case the status value is 7949. After decoding the value we could understand that the auto-negotiation is not getting completed in 1000 Mbps.&amp;nbsp; I am not getting any clue to debug this issue forward.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Any one has faced such issue ?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 27 Oct 2017 12:23:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Auto-negotiation-not-complete-in-1-Gigabit-Ethernet-in-KSZ9031/m-p/728071#M113244</guid>
      <dc:creator>anjalikkrishna</dc:creator>
      <dc:date>2017-10-27T12:23:05Z</dc:date>
    </item>
    <item>
      <title>Re: Auto-negotiation not complete in 1 Gigabit Ethernet in KSZ9031</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Auto-negotiation-not-complete-in-1-Gigabit-Ethernet-in-KSZ9031/m-p/728072#M113245</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Anjalik&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;one can check if KSZ9031 correctly programmed, check for example&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="http://lists.infradead.org/pipermail/linux-arm-kernel/2013-June/178629.html" title="http://lists.infradead.org/pipermail/linux-arm-kernel/2013-June/178629.html"&gt;[PATCH 3/3] ARM: i.MX6: add ethernet phy fixup for KSZ9031&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="http://lists.infradead.org/pipermail/barebox/2016-March/026498.html" title="http://lists.infradead.org/pipermail/barebox/2016-March/026498.html"&gt;Ethernet PHY KSZ9031 is not working [SOLVED]&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;It has RGMII Pad Skew registers which may be used for adjusted RGMII timings&lt;/P&gt;&lt;P&gt;provided in i.MX6 Datasheet. &lt;A class="link-titled" href="https://www.nxp.com/docs/en/data-sheet/IMX6SDLCEC.pdf" title="https://www.nxp.com/docs/en/data-sheet/IMX6SDLCEC.pdf"&gt;https://www.nxp.com/docs/en/data-sheet/IMX6SDLCEC.pdf&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 27 Oct 2017 23:28:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Auto-negotiation-not-complete-in-1-Gigabit-Ethernet-in-KSZ9031/m-p/728072#M113245</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2017-10-27T23:28:14Z</dc:date>
    </item>
    <item>
      <title>Re: Auto-negotiation not complete in 1 Gigabit Ethernet in KSZ9031</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Auto-negotiation-not-complete-in-1-Gigabit-Ethernet-in-KSZ9031/m-p/728073#M113246</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Igor, &lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; Thanks for the reply.&lt;/P&gt;&lt;P&gt;&amp;nbsp; Our hardware team debugged the issue. and confirmed that no provision is provided for 1 Gbps support in hardware.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 12 Jan 2018 07:35:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Auto-negotiation-not-complete-in-1-Gigabit-Ethernet-in-KSZ9031/m-p/728073#M113246</guid>
      <dc:creator>anjalikkrishna</dc:creator>
      <dc:date>2018-01-12T07:35:34Z</dc:date>
    </item>
    <item>
      <title>Re: Auto-negotiation not complete in 1 Gigabit Ethernet in KSZ9031</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Auto-negotiation-not-complete-in-1-Gigabit-Ethernet-in-KSZ9031/m-p/2253346#M242578</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I have the same problem. when connecting to 1G, LED indicators turns off. and no link is stablished.&amp;nbsp;&lt;/P&gt;&lt;P&gt;it works fine with 10/100. Tried everything, No idea. ( reached out already to Microchio, no success)&lt;/P&gt;&lt;P&gt;I saw that you came out to a solution. Can you help me on that?&lt;/P&gt;</description>
      <pubDate>Tue, 02 Dec 2025 15:53:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Auto-negotiation-not-complete-in-1-Gigabit-Ethernet-in-KSZ9031/m-p/2253346#M242578</guid>
      <dc:creator>EngErfan</dc:creator>
      <dc:date>2025-12-02T15:53:14Z</dc:date>
    </item>
  </channel>
</rss>