<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: imx-lib</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/imx-lib/m-p/151112#M1132</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I've read these tests don't work, so i prefer directly go and use api from imx lib with doc on it.&lt;/P&gt;&lt;P&gt;Yes i'm also developing but i hope i could use imx53 without need of additional drivers, just api, in a first time.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 03 Apr 2012 09:15:58 GMT</pubDate>
    <dc:creator>christophe</dc:creator>
    <dc:date>2012-04-03T09:15:58Z</dc:date>
    <item>
      <title>imx-lib</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx-lib/m-p/151108#M1128</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi all,&lt;/P&gt;&lt;P&gt;I'm trying to use imx-lib-11.09.01 provided with imx packages and i want to use ipu features in particular.&lt;/P&gt;&lt;P&gt;Installation of package is ok, but problems rise with compilation attempts. If i can perfectly compile vpu part, ipu part refuses to do it (problem of struct definitions, ...)&lt;/P&gt;&lt;P&gt;So, is someone use this lib ? Is it really debugged ?&lt;/P&gt;&lt;P&gt;Is there an other way to use fastly ipu features ?&lt;/P&gt;&lt;P&gt;Thanks.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 02 Apr 2012 12:50:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx-lib/m-p/151108#M1128</guid>
      <dc:creator>christophe</dc:creator>
      <dc:date>2012-04-02T12:50:04Z</dc:date>
    </item>
    <item>
      <title>Re: imx-lib</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx-lib/m-p/151109#M1129</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Indeed. Your thread solves my problem. Thanks.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 02 Apr 2012 13:01:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx-lib/m-p/151109#M1129</guid>
      <dc:creator>christophe</dc:creator>
      <dc:date>2012-04-02T13:01:07Z</dc:date>
    </item>
    <item>
      <title>Re: imx-lib</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx-lib/m-p/151110#M1130</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Another point now i can go further. I suppose you use ipu functions, so did you integrate them easily and is it working as expected ? Seemingly, including .h file mxc_ipu_hl_lib.h doesn't go alone.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 02 Apr 2012 15:18:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx-lib/m-p/151110#M1130</guid>
      <dc:creator>christophe</dc:creator>
      <dc:date>2012-04-02T15:18:06Z</dc:date>
    </item>
    <item>
      <title>Re: imx-lib</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx-lib/m-p/151111#M1131</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I'm using linux. ltib is coming from freescale.&lt;/P&gt;&lt;P&gt;I manage to compile but with the min config profile. I've not tried another config.&lt;/P&gt;&lt;P&gt;Test profile is not so useful for me since i want to directly use ipu, vpu features. I hope it works at least... :-|&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 03 Apr 2012 08:43:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx-lib/m-p/151111#M1131</guid>
      <dc:creator>christophe</dc:creator>
      <dc:date>2012-04-03T08:43:52Z</dc:date>
    </item>
    <item>
      <title>Re: imx-lib</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx-lib/m-p/151112#M1132</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I've read these tests don't work, so i prefer directly go and use api from imx lib with doc on it.&lt;/P&gt;&lt;P&gt;Yes i'm also developing but i hope i could use imx53 without need of additional drivers, just api, in a first time.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 03 Apr 2012 09:15:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx-lib/m-p/151112#M1132</guid>
      <dc:creator>christophe</dc:creator>
      <dc:date>2012-04-03T09:15:58Z</dc:date>
    </item>
    <item>
      <title>Re: imx-lib</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx-lib/m-p/151113#M1133</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Yes, it seems Test profile don't work or/and prog tests don't work. But you can always read them and get programing info.&lt;/P&gt;&lt;P&gt;Let see this note from imx53_start_linux_bsp_userguide.pdf:&lt;/P&gt;&lt;P&gt;"Select platform to Freescale iMX reference boards and exit, saving the changes. At the&lt;BR /&gt;next menu, select platform type as imx5x and package profile. Exit and save&lt;BR /&gt;changes. Please note that only the profiles of Min profile, FSL gnome release&lt;BR /&gt;packages and mfg firmware profile pass build tests."&lt;/P&gt;&lt;P&gt;So...&lt;/P&gt;&lt;P&gt;It's possible i've to add new api or drivers for ipu, if needed. I've already added a specific camera driver for instance.&lt;/P&gt;&lt;P&gt;My project is a camera application. And you ?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 03 Apr 2012 09:42:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx-lib/m-p/151113#M1133</guid>
      <dc:creator>christophe</dc:creator>
      <dc:date>2012-04-03T09:42:34Z</dc:date>
    </item>
    <item>
      <title>Re: imx-lib</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx-lib/m-p/151114#M1134</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I'using macraigor usb2demon. Just received it, not really tested it yet.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 03 Apr 2012 10:19:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx-lib/m-p/151114#M1134</guid>
      <dc:creator>christophe</dc:creator>
      <dc:date>2012-04-03T10:19:59Z</dc:date>
    </item>
    <item>
      <title>Re: imx-lib</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx-lib/m-p/151115#M1135</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;No problem.&lt;/P&gt;&lt;P&gt;This probe can be used with eclipse too (not yet try). It costs about 750 $.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 03 Apr 2012 11:36:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx-lib/m-p/151115#M1135</guid>
      <dc:creator>christophe</dc:creator>
      <dc:date>2012-04-03T11:36:40Z</dc:date>
    </item>
  </channel>
</rss>