<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: High ethernet packet loss (iperf3) in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/High-ethernet-packet-loss-iperf3/m-p/727799#M113191</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello John,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We are using 1Gbps, I don't remember that the counters in ifconfig show any errors or drops.&lt;/P&gt;&lt;P&gt;But if iperf3 is a reliable tool (and I think it is), than we must understand why it show such high rate of lost packets.&lt;/P&gt;&lt;P&gt;The ethernet loss packets performance as seen with iperf3 explain the degraded performance with gstreamer rtp.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Ran&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 20 Dec 2017 08:31:24 GMT</pubDate>
    <dc:creator>rans</dc:creator>
    <dc:date>2017-12-20T08:31:24Z</dc:date>
    <item>
      <title>High ethernet packet loss (iperf3)</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/High-ethernet-packet-loss-iperf3/m-p/727795#M113187</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We are struglling for at least a week now, with performance issues related to Ethernet packets and gstreamer: we are sending video over rtp (udp) from PC to imx6 ( lec-imx6 from adlink) , and observed a very bad performance even with small resolutions and bandwidth: starting from ~50Mbits/sec there is a very bad video playback over the imx6 station.&lt;BR /&gt;We have been investigating this issue, for couple of days, and seems now that we found the root cause of this performance issue.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;It seems that there is high loss of packets between PC sender and the lec-imx6 receiver. we see this with a simple iperf3 test between this station. with 40Mbit/sec there is already over 85% packet loss !!&lt;/P&gt;&lt;P&gt;We see that the issue been discussed here:&lt;BR /&gt;&lt;A _jive_internal="true" href="https://community.nxp.com/thread/444707"&gt;https://community.nxp.com/thread/444707&lt;/A&gt;&lt;/P&gt;&lt;P&gt;But can't see it was resolved yet.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I would appreciate your assistance on this. This is a critical issue.&lt;BR /&gt;This is based on yocto build supplied by adlink from web site (jethro yocto)&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Best Regards,&lt;BR /&gt;Ran&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 17 Dec 2017 21:30:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/High-ethernet-packet-loss-iperf3/m-p/727795#M113187</guid>
      <dc:creator>rans</dc:creator>
      <dc:date>2017-12-17T21:30:42Z</dc:date>
    </item>
    <item>
      <title>Re: Ethernet packet loss (gstreamer rtp)</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/High-ethernet-packet-loss-iperf3/m-p/727796#M113188</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Possibly the issue is caused with bad connection, weak cable or something like this.&lt;BR /&gt;Please try to use another ethernet cable, to use or do not use ethernet swith between i.MX and PC, etc.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a great day,&lt;BR /&gt;Victor&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 19 Dec 2017 07:01:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/High-ethernet-packet-loss-iperf3/m-p/727796#M113188</guid>
      <dc:creator>b36401</dc:creator>
      <dc:date>2017-12-19T07:01:09Z</dc:date>
    </item>
    <item>
      <title>Re: Ethernet packet loss (gstreamer rtp)</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/High-ethernet-packet-loss-iperf3/m-p/727797#M113189</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Victor,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We're struglling with this issue for some 2 weeks now.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We first thought is it gpu issue, but doing same pipeline without streaming works fine.&lt;/P&gt;&lt;P&gt;The problem starts only with streaming.&lt;/P&gt;&lt;P&gt;So we made iperf tests.&lt;/P&gt;&lt;P&gt;iperf shows very low packet drop, but iperf3 shows very large.&lt;/P&gt;&lt;P&gt;It change from 30%-60% already in low bandwidth of 50Mbps.&lt;/P&gt;&lt;P&gt;Doing the exact same test, between PC to PC shows much lower packet loss in same bandwidth.&lt;/P&gt;&lt;P&gt;Changing cable, switch, etc - did not help.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I also see that this issue been discussed here before:&lt;/P&gt;&lt;P&gt;1.&lt;/P&gt;&lt;P&gt;&lt;A href="https://mail.comm-it.com/owa/redir.aspx?C=uXqcdwmJYs9gVbbzs9IcyeilFRtBlMBdPJnpPTjGG2bCCzqBt0bVCA..&amp;amp;URL=https%3a%2f%2fcommunity.nxp.com%2fthread%2f444707" style="font-size: 10pt;" target="_blank"&gt;https://community.nxp.com/thread/444707&lt;/A&gt;&lt;/P&gt;&lt;P&gt;2.&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/thread/340956"&gt;i.MX6Q Ethernet: Low RX performance&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;3.&lt;/P&gt;&lt;P&gt;Also see last comments in github:&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="https://github.com/esnet/iperf/issues/296" title="https://github.com/esnet/iperf/issues/296"&gt;Extremely high packet loss with UDP test · Issue #296 · esnet/iperf · GitHub&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;As you can see from clemens comments, it is a real problem with imx6.&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;I am not sure if it is related to imx, drivers, or board (adlink lec-imx6) , but it really made us stuck.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;I hope someone can test this issue with iperf3, and give us a good solution, because&amp;nbsp;currently we are considering that imx6 is too weak with its ethernet high packet drop.&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Ran&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 19 Dec 2017 08:12:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/High-ethernet-packet-loss-iperf3/m-p/727797#M113189</guid>
      <dc:creator>rans</dc:creator>
      <dc:date>2017-12-19T08:12:29Z</dc:date>
    </item>
    <item>
      <title>Re: High ethernet packet loss (iperf3)</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/High-ethernet-packet-loss-iperf3/m-p/727798#M113190</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;while sending video,does ifconfig gives any errors like RX&amp;nbsp; errors, dropped, overruns and frame. Also ethernet is in 100M or 1G ?&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 20 Dec 2017 08:07:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/High-ethernet-packet-loss-iperf3/m-p/727798#M113190</guid>
      <dc:creator>anjojohn</dc:creator>
      <dc:date>2017-12-20T08:07:13Z</dc:date>
    </item>
    <item>
      <title>Re: High ethernet packet loss (iperf3)</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/High-ethernet-packet-loss-iperf3/m-p/727799#M113191</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello John,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We are using 1Gbps, I don't remember that the counters in ifconfig show any errors or drops.&lt;/P&gt;&lt;P&gt;But if iperf3 is a reliable tool (and I think it is), than we must understand why it show such high rate of lost packets.&lt;/P&gt;&lt;P&gt;The ethernet loss packets performance as seen with iperf3 explain the degraded performance with gstreamer rtp.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Ran&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 20 Dec 2017 08:31:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/High-ethernet-packet-loss-iperf3/m-p/727799#M113191</guid>
      <dc:creator>rans</dc:creator>
      <dc:date>2017-12-20T08:31:24Z</dc:date>
    </item>
    <item>
      <title>Re: High ethernet packet loss (iperf3)</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/High-ethernet-packet-loss-iperf3/m-p/727800#M113192</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Could you check in 100M bandwidth. We had similar issue in 1G bandwidth, so we switched to 100M.&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 20 Dec 2017 09:13:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/High-ethernet-packet-loss-iperf3/m-p/727800#M113192</guid>
      <dc:creator>anjojohn</dc:creator>
      <dc:date>2017-12-20T09:13:39Z</dc:date>
    </item>
    <item>
      <title>Re: High ethernet packet loss (iperf3)</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/High-ethernet-packet-loss-iperf3/m-p/727801#M113193</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi John,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks a lot for the ideas.&lt;/P&gt;&lt;P&gt;I can check that, but it won't help me too much, becuase we must use 1Gbps.&lt;/P&gt;&lt;P&gt;We&amp;nbsp; need to stream video over ethernet in bandwidth ~450Mbits/sec), so we need to understand if imx6 can handle that, or maybe it is too weak, or buggy.&lt;/P&gt;&lt;P&gt;We made a lot of effort with gstreamer till now, not understanding why PC sender-PC reciever (pentium) with same gstreamer rtp pipeline works well, but PC sender-imx6 reciever performs very bad.&lt;/P&gt;&lt;P&gt;After investigation on this, which got strengthen when we used iperf3 for testing, we got to the conclusion that it is an ethernet issue which cause a lot of packet drops, starting from 50Mbit/sec (!!). Note that iperf tool shows much lower values. Seems that iperf3 catch much more problems than simple iperf (was discussed here too:&amp;nbsp;&lt;A class="link-titled" href="https://github.com/esnet/iperf/issues/296" title="https://github.com/esnet/iperf/issues/296"&gt;Extremely high packet loss with UDP test · Issue #296 · esnet/iperf · GitHub&lt;/A&gt;&amp;nbsp;&amp;nbsp;)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you for any ideas,&lt;/P&gt;&lt;P&gt;Ran&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 20 Dec 2017 09:22:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/High-ethernet-packet-loss-iperf3/m-p/727801#M113193</guid>
      <dc:creator>rans</dc:creator>
      <dc:date>2017-12-20T09:22:44Z</dc:date>
    </item>
    <item>
      <title>Re: High ethernet packet loss (iperf3)</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/High-ethernet-packet-loss-iperf3/m-p/727802#M113194</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Ranshalit,&lt;/P&gt;&lt;P&gt;We had similar video streaming requirement. How ever stable IMX6 bandwidth is around 200 to 300Mbps. Below is the quote from IMX6Dualite/Solo errata&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;"The theoretical maximum performance of 1 Gbps ENET is limited to 470 Mbps (total for Tx and Rx). The actual measured performance in an optimized environment is up to 400 Mbps"&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="https://www.nxp.com/docs/en/errata/IMX6SDLCE.pdf" title="https://www.nxp.com/docs/en/errata/IMX6SDLCE.pdf"&gt;https://www.nxp.com/docs/en/errata/IMX6SDLCE.pdf&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 20 Dec 2017 09:56:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/High-ethernet-packet-loss-iperf3/m-p/727802#M113194</guid>
      <dc:creator>anjojohn</dc:creator>
      <dc:date>2017-12-20T09:56:09Z</dc:date>
    </item>
    <item>
      <title>Re: High ethernet packet loss (iperf3)</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/High-ethernet-packet-loss-iperf3/m-p/727803#M113195</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;This can also help&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="https://boundarydevices.com/i-mx6-ethernet/" title="https://boundarydevices.com/i-mx6-ethernet/"&gt;i.MX6 Gigabit Ethernet - Boundary Devices&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 20 Dec 2017 09:59:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/High-ethernet-packet-loss-iperf3/m-p/727803#M113195</guid>
      <dc:creator>anjojohn</dc:creator>
      <dc:date>2017-12-20T09:59:23Z</dc:date>
    </item>
    <item>
      <title>Re: High ethernet packet loss (iperf3)</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/High-ethernet-packet-loss-iperf3/m-p/727804#M113196</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi John,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks a lot for the feedback.&lt;/P&gt;&lt;P&gt;Seems that the key here is "The actual measured performance in &lt;EM&gt;&lt;STRONG&gt;an optimized environment&lt;/STRONG&gt;&lt;/EM&gt; is up to 400 Mbps&lt;SPAN style="color: #51626f; background-color: #ffffff; border: 0px;"&gt;&lt;EM&gt;"&lt;/EM&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="background-color: #ffffff; border: 0px; color: #51626f;"&gt;For some reason, our performance in Ethernet&amp;nbsp;is very low, this is shown with iperf3.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff; border: 0px;"&gt;I am not sure if it is a driver version, board issue, or imx6 revision(?), but we are seeing bad performance even in 50Mbps.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff; border: 0px;"&gt;Not sure how we can continue from that. When you check with iperf3 (please try more than once):&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff; border: 0px;"&gt;in target:&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff; border: 0px;"&gt;iperf3 -s&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff; border: 0px;"&gt;in PC (for example the target has ip 192.168.0.1):&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff; border: 0px;"&gt;iperf -uZVc 192.168.0.1 -b100m&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff; border: 0px;"&gt;What is the loss rate you get on your board ?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;How can we make our configuration &lt;EM&gt;&lt;STRONG&gt;an optimized environment ?&lt;/STRONG&gt;&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff; border: 0px;"&gt;Regards,&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff; border: 0px;"&gt;Ran&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 20 Dec 2017 10:09:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/High-ethernet-packet-loss-iperf3/m-p/727804#M113196</guid>
      <dc:creator>rans</dc:creator>
      <dc:date>2017-12-20T10:09:34Z</dc:date>
    </item>
    <item>
      <title>Re: High ethernet packet loss (iperf3)</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/High-ethernet-packet-loss-iperf3/m-p/727805#M113197</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Global problem in Ethernet management ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;To have the correct performance in video we had to activate the jumbo frame on a Gigabit controller.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Continuing our investigation, we found very large differences between iperf3 and netcat.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;And that on the Gigabit Ethernet controller and on the &lt;STRONG&gt;local loop&lt;/STRONG&gt; !&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;This problem is detailed on this request :&amp;nbsp;&lt;A _jive_internal="true" href="https://community.nxp.com/thread/466054"&gt;https://community.nxp.com/thread/466054&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Pascal&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 22 Dec 2017 07:57:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/High-ethernet-packet-loss-iperf3/m-p/727805#M113197</guid>
      <dc:creator>chevereau</dc:creator>
      <dc:date>2017-12-22T07:57:58Z</dc:date>
    </item>
    <item>
      <title>Re: High ethernet packet loss (iperf3)</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/High-ethernet-packet-loss-iperf3/m-p/727806#M113198</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Chevereau,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you very much for the comment.&lt;/P&gt;&lt;P&gt;Wwe plan to get back with this issue, also with ethernet ( &lt;SPAN class=""&gt;SMARC 2.0 Carrier&lt;/SPAN&gt;&amp;nbsp; connect tech).&lt;/P&gt;&lt;P&gt;I have followed your link&amp;nbsp;&lt;A _jive_internal="true" data-containerid="2004" data-containertype="14" data-content-finding="Community" data-objectid="466054" data-objecttype="1" href="https://community.nxp.com/thread/466054" style="color: #5e89c1; background-color: #ffffff; border: 0px; padding: 1px 0px 1px calc(12px + 0.35ex);"&gt;https://community.nxp.com/thread/466054&lt;/A&gt;&lt;/P&gt;&lt;P&gt;I see that you used&amp;nbsp;Ixora (is it a PCIe adapter?),&lt;/P&gt;&lt;P&gt;yet your bandwidth was not good enough.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You wrote that you have used jumbo frames.&amp;nbsp;&lt;/P&gt;&lt;P&gt;What bandwidth did it give you finally ?&amp;nbsp; Is this issue resolved ? Which tool should we use for testing (iper3, iper2, netcat) ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you for the time,&lt;/P&gt;&lt;P&gt;ranran&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 06 Mar 2018 17:10:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/High-ethernet-packet-loss-iperf3/m-p/727806#M113198</guid>
      <dc:creator>rans</dc:creator>
      <dc:date>2018-03-06T17:10:25Z</dc:date>
    </item>
    <item>
      <title>Re: High ethernet packet loss (iperf3)</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/High-ethernet-packet-loss-iperf3/m-p/727807#M113199</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;One more...&lt;BR /&gt;If jumbo frame resolved the issue: &lt;BR /&gt;&lt;BR /&gt;Can you please add how you configured jumbo frame with imx6 ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you for your time,&lt;/P&gt;&lt;P&gt;ranran&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 06 Mar 2018 17:17:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/High-ethernet-packet-loss-iperf3/m-p/727807#M113199</guid>
      <dc:creator>rans</dc:creator>
      <dc:date>2018-03-06T17:17:31Z</dc:date>
    </item>
  </channel>
</rss>