<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 Re: imx6q</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/imx6q/m-p/726717#M113005</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;You need to add your application to startup for it ru run automatically when the OS starts up.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a great day,&lt;BR /&gt;Victor&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 27 Oct 2017 03:29:30 GMT</pubDate>
    <dc:creator>b36401</dc:creator>
    <dc:date>2017-10-27T03:29:30Z</dc:date>
    <item>
      <title>imx6q</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx6q/m-p/726716#M113004</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello!I created image,and the kernel version is 4.1.15.I use this command:DISTRO=fsl-imx-x11 MACHINE=imx6qsabresd source fsl-setup-release.sh -b build-x11 and&amp;nbsp;bitbake fsl-image-qt5;but after starting,i want to show my own desktop,For example, a simple QT program,what should i do?I am a novice ,I hope you can give me some advices.Thanks&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 26 Oct 2017 15:47:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx6q/m-p/726716#M113004</guid>
      <dc:creator>一个人的城市</dc:creator>
      <dc:date>2017-10-26T15:47:23Z</dc:date>
    </item>
    <item>
      <title>Re: imx6q</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx6q/m-p/726717#M113005</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;You need to add your application to startup for it ru run automatically when the OS starts up.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a great day,&lt;BR /&gt;Victor&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 27 Oct 2017 03:29:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx6q/m-p/726717#M113005</guid>
      <dc:creator>b36401</dc:creator>
      <dc:date>2017-10-27T03:29:30Z</dc:date>
    </item>
    <item>
      <title>Re: imx6q</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx6q/m-p/726718#M113006</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Where to add? And where is the desktop system started?Can you tell me in detail!Thanks&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 27 Oct 2017 07:24:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx6q/m-p/726718#M113006</guid>
      <dc:creator>一个人的城市</dc:creator>
      <dc:date>2017-10-27T07:24:31Z</dc:date>
    </item>
  </channel>
</rss>