<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Compiling kobs-ng_v5.5 Failed in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Compiling-kobs-ng-v5-5-Failed/m-p/726189#M112924</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I have got the source code of&amp;nbsp;imx-kobs version 5.5 from&amp;nbsp;&lt;A class="link-titled" href="https://github.com/codeauroraforum/imx-kobs" title="https://github.com/codeauroraforum/imx-kobs"&gt;GitHub - codeauroraforum/imx-kobs: Tool to create and write Freescale/NXP I.MX NAND boot related boot data structure to …&lt;/A&gt;&amp;nbsp;,and configured as this:&lt;/P&gt;&lt;P&gt;./configure CC=arm-none-linux-gnueabi-gcc --host=arm-none-linux-gnueabi-gcc. But when I compiled it, I got ERR like this&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/2581i114024F04CE6F487/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_3.png" alt="pastedImage_3.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;Who can help?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 08 Feb 2018 02:16:58 GMT</pubDate>
    <dc:creator>jasonshao</dc:creator>
    <dc:date>2018-02-08T02:16:58Z</dc:date>
    <item>
      <title>Compiling kobs-ng_v5.5 Failed</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Compiling-kobs-ng-v5-5-Failed/m-p/726189#M112924</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I have got the source code of&amp;nbsp;imx-kobs version 5.5 from&amp;nbsp;&lt;A class="link-titled" href="https://github.com/codeauroraforum/imx-kobs" title="https://github.com/codeauroraforum/imx-kobs"&gt;GitHub - codeauroraforum/imx-kobs: Tool to create and write Freescale/NXP I.MX NAND boot related boot data structure to …&lt;/A&gt;&amp;nbsp;,and configured as this:&lt;/P&gt;&lt;P&gt;./configure CC=arm-none-linux-gnueabi-gcc --host=arm-none-linux-gnueabi-gcc. But when I compiled it, I got ERR like this&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/2581i114024F04CE6F487/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_3.png" alt="pastedImage_3.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;Who can help?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 08 Feb 2018 02:16:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Compiling-kobs-ng-v5-5-Failed/m-p/726189#M112924</guid>
      <dc:creator>jasonshao</dc:creator>
      <dc:date>2018-02-08T02:16:58Z</dc:date>
    </item>
    <item>
      <title>Re: Compiling kobs-ng_v5.5 Failed</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Compiling-kobs-ng-v5-5-Failed/m-p/726190#M112925</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;It seems the is some mis-versioning in the sources you are compiling.&lt;BR /&gt;Please try to re-get the sources with an accuracy.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a great day,&lt;BR /&gt;Victor&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 07 Mar 2018 04:21:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Compiling-kobs-ng-v5-5-Failed/m-p/726190#M112925</guid>
      <dc:creator>b36401</dc:creator>
      <dc:date>2018-03-07T04:21:27Z</dc:date>
    </item>
  </channel>
</rss>