<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic android CTS Display Refresh Rate failing on IMX6 in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/android-CTS-Display-Refresh-Rate-failing-on-IMX6/m-p/725998#M112897</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I am working on nitrogen6x SOM version1. We have ported Android 7.1 on it and have interfaced a 7.0'' 800x480 LVDS panel. The display is up and running smoothly. We do not see any functionality issue . But when we run the&amp;nbsp; Android CTS we are facing two failures related to display. Following test cases are failing:&lt;/P&gt;&lt;P&gt;android.view.cts.DisplayRefreshRateTest#testRefreshRate: This is related to the refresh rate of the display. I am getting following log:&lt;/P&gt;&lt;P&gt;01-01 00:16:05.752&amp;nbsp; 3760&amp;nbsp; 3776 D DisplayRefreshRateTest: claimed 61.000004 fps, achieved 50.55673 fps&lt;BR /&gt;01-01 00:16:15.760&amp;nbsp; 3760&amp;nbsp; 3781 D DisplayRefreshRateTest: restarting&lt;BR /&gt;01-01 00:16:25.808&amp;nbsp; 3760&amp;nbsp; 3776 D DisplayRefreshRateTest: claimed 61.000004 fps, achieved 50.557114 fps&lt;BR /&gt;01-01 00:16:35.816&amp;nbsp; 3760&amp;nbsp; 3781 D DisplayRefreshRateTest: restarting&lt;BR /&gt;01-01 00:16:45.865&amp;nbsp; 3760&amp;nbsp; 3776 D DisplayRefreshRateTest: claimed 61.000004 fps, achieved 50.555187 fps&lt;BR /&gt;01-01 00:16:55.875&amp;nbsp; 3760&amp;nbsp; 3781 D DisplayRefreshRateTest: restarting&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The achieved fps is less than than the claimed fps due to which the testcase fails.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The second test case is:&lt;/P&gt;&lt;P&gt;android.view.cts.SurfaceViewSyncTests#testVideoSurfaceViewEdgeCoverage&lt;/P&gt;&lt;P&gt;In this test case it makes infinite objects on the screen and calculates the failed frames. the fail ratio of the frames is higher due to which the test case fails.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Can anyone please help to resolve these two issues?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank in advance.&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Divya&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 26 Oct 2017 15:02:41 GMT</pubDate>
    <dc:creator>divyasinghatwar</dc:creator>
    <dc:date>2017-10-26T15:02:41Z</dc:date>
    <item>
      <title>android CTS Display Refresh Rate failing on IMX6</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/android-CTS-Display-Refresh-Rate-failing-on-IMX6/m-p/725998#M112897</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I am working on nitrogen6x SOM version1. We have ported Android 7.1 on it and have interfaced a 7.0'' 800x480 LVDS panel. The display is up and running smoothly. We do not see any functionality issue . But when we run the&amp;nbsp; Android CTS we are facing two failures related to display. Following test cases are failing:&lt;/P&gt;&lt;P&gt;android.view.cts.DisplayRefreshRateTest#testRefreshRate: This is related to the refresh rate of the display. I am getting following log:&lt;/P&gt;&lt;P&gt;01-01 00:16:05.752&amp;nbsp; 3760&amp;nbsp; 3776 D DisplayRefreshRateTest: claimed 61.000004 fps, achieved 50.55673 fps&lt;BR /&gt;01-01 00:16:15.760&amp;nbsp; 3760&amp;nbsp; 3781 D DisplayRefreshRateTest: restarting&lt;BR /&gt;01-01 00:16:25.808&amp;nbsp; 3760&amp;nbsp; 3776 D DisplayRefreshRateTest: claimed 61.000004 fps, achieved 50.557114 fps&lt;BR /&gt;01-01 00:16:35.816&amp;nbsp; 3760&amp;nbsp; 3781 D DisplayRefreshRateTest: restarting&lt;BR /&gt;01-01 00:16:45.865&amp;nbsp; 3760&amp;nbsp; 3776 D DisplayRefreshRateTest: claimed 61.000004 fps, achieved 50.555187 fps&lt;BR /&gt;01-01 00:16:55.875&amp;nbsp; 3760&amp;nbsp; 3781 D DisplayRefreshRateTest: restarting&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The achieved fps is less than than the claimed fps due to which the testcase fails.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The second test case is:&lt;/P&gt;&lt;P&gt;android.view.cts.SurfaceViewSyncTests#testVideoSurfaceViewEdgeCoverage&lt;/P&gt;&lt;P&gt;In this test case it makes infinite objects on the screen and calculates the failed frames. the fail ratio of the frames is higher due to which the test case fails.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Can anyone please help to resolve these two issues?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank in advance.&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Divya&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 26 Oct 2017 15:02:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/android-CTS-Display-Refresh-Rate-failing-on-IMX6/m-p/725998#M112897</guid>
      <dc:creator>divyasinghatwar</dc:creator>
      <dc:date>2017-10-26T15:02:41Z</dc:date>
    </item>
  </channel>
</rss>