<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Programm SPI interface for imx6s android  in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Programm-SPI-interface-for-imx6s-android/m-p/725818#M112876</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;ECSPI driver implements a standard Linux driver interface (android is based on linux)&lt;/P&gt;&lt;P&gt;please refer to Chapter 36 Enhanced Configurable Serial Peripheral Interface (ECSPI) Driver&lt;/P&gt;&lt;P&gt;attached Linux Manual.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 05 Mar 2018 02:49:39 GMT</pubDate>
    <dc:creator>igorpadykov</dc:creator>
    <dc:date>2018-03-05T02:49:39Z</dc:date>
    <item>
      <title>Programm SPI interface for imx6s android</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Programm-SPI-interface-for-imx6s-android/m-p/725817#M112875</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;How to configure SPI interface for android. Shall we write application using c/cpp ?&lt;/P&gt;&lt;P&gt;Is there any inbuilt driver design for SPI which we can used to open SPI port and configure the SPI port?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 04 Mar 2018 07:56:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Programm-SPI-interface-for-imx6s-android/m-p/725817#M112875</guid>
      <dc:creator>androidimx6s</dc:creator>
      <dc:date>2018-03-04T07:56:04Z</dc:date>
    </item>
    <item>
      <title>Re: Programm SPI interface for imx6s android</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Programm-SPI-interface-for-imx6s-android/m-p/725818#M112876</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;ECSPI driver implements a standard Linux driver interface (android is based on linux)&lt;/P&gt;&lt;P&gt;please refer to Chapter 36 Enhanced Configurable Serial Peripheral Interface (ECSPI) Driver&lt;/P&gt;&lt;P&gt;attached Linux Manual.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 05 Mar 2018 02:49:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Programm-SPI-interface-for-imx6s-android/m-p/725818#M112876</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2018-03-05T02:49:39Z</dc:date>
    </item>
  </channel>
</rss>