<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic changing default root password in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/changing-default-root-password/m-p/725737#M112860</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I have imx6ul dev board&amp;nbsp; &lt;BR /&gt; &lt;BR /&gt; I tried to add a password for yocto login.&amp;nbsp; &lt;BR /&gt;steps I did:&lt;BR /&gt;create an MD5 password&lt;BR /&gt;Copied the generated hash output string and replace the MD5_ROOT_PASSWD with it.&lt;BR /&gt;in the local.conf file, removed debug-tweaks extra_image_features&lt;BR /&gt;rebuild the images.&lt;BR /&gt; &lt;BR /&gt; after installed the images, at prompt&lt;BR /&gt;&amp;nbsp; login:&lt;BR /&gt; type root, password: is not prompted&lt;BR /&gt; &lt;BR /&gt; Then I added&lt;BR /&gt; useradd - p 'password hash string' admin&lt;BR /&gt; after rebuild and install the images, at prompt&lt;BR /&gt; login: admin&lt;BR /&gt; Password:&lt;BR /&gt; &lt;BR /&gt; it shows the password, but returns login incorrect&lt;BR /&gt; &lt;BR /&gt; What did I miss?&lt;BR /&gt; &lt;BR /&gt; Thank you,&lt;BR /&gt; &lt;BR /&gt; David&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 11 Apr 2018 17:55:02 GMT</pubDate>
    <dc:creator>davidzhou</dc:creator>
    <dc:date>2018-04-11T17:55:02Z</dc:date>
    <item>
      <title>changing default root password</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/changing-default-root-password/m-p/725737#M112860</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I have imx6ul dev board&amp;nbsp; &lt;BR /&gt; &lt;BR /&gt; I tried to add a password for yocto login.&amp;nbsp; &lt;BR /&gt;steps I did:&lt;BR /&gt;create an MD5 password&lt;BR /&gt;Copied the generated hash output string and replace the MD5_ROOT_PASSWD with it.&lt;BR /&gt;in the local.conf file, removed debug-tweaks extra_image_features&lt;BR /&gt;rebuild the images.&lt;BR /&gt; &lt;BR /&gt; after installed the images, at prompt&lt;BR /&gt;&amp;nbsp; login:&lt;BR /&gt; type root, password: is not prompted&lt;BR /&gt; &lt;BR /&gt; Then I added&lt;BR /&gt; useradd - p 'password hash string' admin&lt;BR /&gt; after rebuild and install the images, at prompt&lt;BR /&gt; login: admin&lt;BR /&gt; Password:&lt;BR /&gt; &lt;BR /&gt; it shows the password, but returns login incorrect&lt;BR /&gt; &lt;BR /&gt; What did I miss?&lt;BR /&gt; &lt;BR /&gt; Thank you,&lt;BR /&gt; &lt;BR /&gt; David&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 11 Apr 2018 17:55:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/changing-default-root-password/m-p/725737#M112860</guid>
      <dc:creator>davidzhou</dc:creator>
      <dc:date>2018-04-11T17:55:02Z</dc:date>
    </item>
    <item>
      <title>Re: changing default root password</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/changing-default-root-password/m-p/725738#M112861</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;pls refer to the link as below, hope helpful for you&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="https://wiki.yoctoproject.org/wiki/FAQ:How_do_I_set_or_change_the_root_password" title="https://wiki.yoctoproject.org/wiki/FAQ:How_do_I_set_or_change_the_root_password"&gt;FAQ:How do I set or change the root password - Yocto Project&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 12 Apr 2018 07:59:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/changing-default-root-password/m-p/725738#M112861</guid>
      <dc:creator>joanxie</dc:creator>
      <dc:date>2018-04-12T07:59:49Z</dc:date>
    </item>
    <item>
      <title>Re: changing default root password</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/changing-default-root-password/m-p/725739#M112862</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Joan,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Also added into poky/meta/classes/extrausers.bbclass&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;David&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 13 Apr 2018 16:35:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/changing-default-root-password/m-p/725739#M112862</guid>
      <dc:creator>davidzhou</dc:creator>
      <dc:date>2018-04-13T16:35:08Z</dc:date>
    </item>
  </channel>
</rss>