<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Ethernet on ENET2 with imx6sx in u-boot  in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Ethernet-on-ENET2-with-imx6sx-in-u-boot/m-p/725672#M112856</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear Igor,&lt;/P&gt;&lt;P&gt;thanks for the answer, but i was not lucky!&lt;/P&gt;&lt;P&gt;here is the SCH of PHY and SOC:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/30111i1FA1D551EC1D2E5F/image-size/large?v=v2&amp;amp;px=999" title="sch.png" alt="sch.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;i&amp;nbsp; use y-boot imx: and modified the FEC pin mux: this is part of &lt;STRONG&gt;board/freescale/mx6sxsabresd/mx6sxsabresd.c&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;static iomux_v3_cfg_t const fec2_pads[] = {&lt;BR /&gt; MX6_PAD_ENET1_MDC__ENET2_MDC | MUX_PAD_CTRL(ENET_PAD_CTRL),&lt;BR /&gt; MX6_PAD_ENET1_MDIO__ENET2_MDIO | MUX_PAD_CTRL(ENET_PAD_CTRL),&lt;BR /&gt; MX6_PAD_RGMII2_RXC__ENET2_RX_ER | MUX_PAD_CTRL(ENET_PAD_CTRL),&lt;BR /&gt; MX6_PAD_RGMII2_RX_CTL__ENET2_RX_EN | MUX_PAD_CTRL(ENET_RX_PAD_CTRL),&lt;BR /&gt; MX6_PAD_RGMII2_RD0__GPIO5_IO_12 | MUX_PAD_CTRL(ENET_RX_PAD_CTRL),&lt;BR /&gt; MX6_PAD_RGMII2_RD1__GPIO5_IO_13 | MUX_PAD_CTRL(ENET_RX_PAD_CTRL),&lt;BR /&gt; MX6_PAD_RGMII2_TX_CTL__ENET2_TX_EN | MUX_PAD_CTRL(ENET_PAD_CTRL),&lt;BR /&gt; MX6_PAD_RGMII2_TD0__GPIO5_IO_18 | MUX_PAD_CTRL(ENET_PAD_CTRL),&lt;BR /&gt; MX6_PAD_RGMII2_TD1__GPIO5_IO_19 | MUX_PAD_CTRL(ENET_PAD_CTRL),&lt;BR /&gt;};&lt;BR /&gt;/*&lt;BR /&gt;static iomux_v3_cfg_t const fec2_pads[] = {&lt;BR /&gt; MX6_PAD_ENET1_MDC__ENET2_MDC | MUX_PAD_CTRL(ENET_PAD_CTRL),&lt;BR /&gt; MX6_PAD_ENET1_MDIO__ENET2_MDIO | MUX_PAD_CTRL(ENET_PAD_CTRL),&lt;BR /&gt; MX6_PAD_RGMII2_RX_CTL__ENET2_RX_EN | MUX_PAD_CTRL(ENET_RX_PAD_CTRL),&lt;BR /&gt; MX6_PAD_RGMII2_RD0__ENET2_RX_DATA_0 | MUX_PAD_CTRL(ENET_RX_PAD_CTRL),&lt;BR /&gt; MX6_PAD_RGMII2_RD1__ENET2_RX_DATA_1 | MUX_PAD_CTRL(ENET_RX_PAD_CTRL),&lt;BR /&gt; MX6_PAD_RGMII2_RD2__ENET2_RX_DATA_2 | MUX_PAD_CTRL(ENET_RX_PAD_CTRL),&lt;BR /&gt; MX6_PAD_RGMII2_RD3__ENET2_RX_DATA_3 | MUX_PAD_CTRL(ENET_RX_PAD_CTRL),&lt;BR /&gt; MX6_PAD_RGMII2_RXC__ENET2_RX_CLK | MUX_PAD_CTRL(ENET_RX_PAD_CTRL),&lt;BR /&gt; MX6_PAD_RGMII2_TX_CTL__ENET2_TX_EN | MUX_PAD_CTRL(ENET_PAD_CTRL),&lt;BR /&gt; MX6_PAD_RGMII2_TD0__ENET2_TX_DATA_0 | MUX_PAD_CTRL(ENET_PAD_CTRL),&lt;BR /&gt; MX6_PAD_RGMII2_TD1__ENET2_TX_DATA_1 | MUX_PAD_CTRL(ENET_PAD_CTRL),&lt;BR /&gt; MX6_PAD_RGMII2_TD2__ENET2_TX_DATA_2 | MUX_PAD_CTRL(ENET_PAD_CTRL),&lt;BR /&gt; MX6_PAD_RGMII2_TD3__ENET2_TX_DATA_3 | MUX_PAD_CTRL(ENET_PAD_CTRL),&lt;BR /&gt; MX6_PAD_RGMII2_TXC__ENET2_RGMII_TXC | MUX_PAD_CTRL(ENET_PAD_CTRL),&lt;BR /&gt;};&lt;BR /&gt;*/&lt;BR /&gt;static iomux_v3_cfg_t const phy_control_pads[] = {&lt;BR /&gt; /* 25MHz Ethernet PHY Clock */&lt;BR /&gt; /*MX6_PAD_ENET2_RX_CLK__ENET2_REF_CLK_25M | MUX_PAD_CTRL(ENET_CLK_PAD_CTRL),*/&lt;/P&gt;&lt;P&gt;/* 50M Ethernet clock*/&lt;BR /&gt; MX6_PAD_ENET2_TX_CLK__ENET2_REF_CLK2 | MUX_PAD_CTRL(ENET_CLK_PAD_CTRL),&lt;/P&gt;&lt;P&gt;/* ENET PHY Power */&lt;BR /&gt; /*MX6_PAD_ENET2_COL__GPIO2_IO_6 | MUX_PAD_CTRL(NO_PAD_CTRL),*/&lt;/P&gt;&lt;P&gt;/* AR8031 PHY Reset */&lt;BR /&gt; /*MX6_PAD_ENET2_CRS__GPIO2_IO_7 | MUX_PAD_CTRL(NO_PAD_CTRL),*/&lt;BR /&gt;};&lt;/P&gt;&lt;P&gt;static int setup_fec(int fec_id)&lt;BR /&gt;{&lt;BR /&gt; struct anatop_regs *anatop = (struct anatop_regs *)ANATOP_BASE_ADDR;&lt;BR /&gt; struct iomuxc_gpr_base_regs *const iomuxc_gpr_regs&lt;BR /&gt; = (struct iomuxc_gpr_base_regs *) IOMUXC_GPR_BASE_ADDR;&lt;BR /&gt; int reg;&lt;/P&gt;&lt;P&gt;if (0 == fec_id)&lt;BR /&gt; /* Use 125M anatop loopback REF_CLK1 for ENET1, clear gpr1[13], gpr1[17]*/&lt;BR /&gt; clrsetbits_le32(&amp;amp;iomuxc_gpr_regs-&amp;gt;gpr[1], IOMUX_GPR1_FEC1_MASK, 0);&lt;BR /&gt; else&lt;BR /&gt; /* Use 125M anatop loopback REF_CLK1 for ENET2, clear gpr1[14], gpr1[18]*/&lt;BR /&gt; clrsetbits_le32(&amp;amp;iomuxc_gpr_regs-&amp;gt;gpr[1], IOMUX_GPR1_FEC2_MASK, 0);&lt;/P&gt;&lt;P&gt;imx_iomux_v3_setup_multiple_pads(phy_control_pads,&lt;BR /&gt; ARRAY_SIZE(phy_control_pads));&lt;/P&gt;&lt;P&gt;/* Enable the ENET power, active low */&lt;BR /&gt; /*gpio_direction_output(IMX_GPIO_NR(2, 6) , 0);*/&lt;/P&gt;&lt;P&gt;/* Reset AR8031 PHY */&lt;BR /&gt; /*gpio_direction_output(IMX_GPIO_NR(2, 7) , 0);&lt;BR /&gt; udelay(500);&lt;BR /&gt; gpio_set_value(IMX_GPIO_NR(2, 7), 1);*/&lt;/P&gt;&lt;P&gt;/*&lt;BR /&gt; reg = readl(&amp;amp;anatop-&amp;gt;pll_enet);&lt;BR /&gt; reg |= BM_ANADIG_PLL_ENET_REF_25M_ENABLE;&lt;BR /&gt; writel(reg, &amp;amp;anatop-&amp;gt;pll_enet);&lt;/P&gt;&lt;P&gt;return enable_fec_anatop_clock(fec_id, ENET_125MHZ);*/&lt;BR /&gt; return 1;&lt;BR /&gt;}&lt;/P&gt;&lt;P&gt;int board_eth_init(bd_t *bis)&lt;BR /&gt;{&lt;BR /&gt; int retval;&lt;/P&gt;&lt;P&gt;if (0 == CONFIG_FEC_ENET_DEV)&lt;BR /&gt; imx_iomux_v3_setup_multiple_pads(fec1_pads, ARRAY_SIZE(fec1_pads));&lt;BR /&gt; else&lt;BR /&gt; imx_iomux_v3_setup_multiple_pads(fec2_pads, ARRAY_SIZE(fec2_pads));&lt;/P&gt;&lt;P&gt;setup_fec(CONFIG_FEC_ENET_DEV);&lt;BR /&gt; retval=cpu_eth_init(bis);&lt;BR /&gt; return retval;&lt;BR /&gt;}&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;would you please help.&lt;/P&gt;&lt;P&gt;thanks&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 19 Dec 2017 06:32:47 GMT</pubDate>
    <dc:creator>huihuang</dc:creator>
    <dc:date>2017-12-19T06:32:47Z</dc:date>
    <item>
      <title>Ethernet on ENET2 with imx6sx in u-boot</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Ethernet-on-ENET2-with-imx6sx-in-u-boot/m-p/725670#M112854</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi everybody,&lt;/P&gt;&lt;P&gt;I am using imx6sx on a costume board i connected ethernet to ENET2 with RMII and externel oscillator.&lt;/P&gt;&lt;P&gt;what modification i should do on u-boot to get it work?&lt;/P&gt;&lt;P&gt;already I set the &lt;STRONG&gt;CONFIG_FEC_ENET_DEV =&amp;nbsp;1&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;and &lt;STRONG&gt;CONFIG_FEC_XCV_TYPE = RMII&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;the result in u-boot-imx and in u-boot-fslc is: &lt;STRONG&gt;build and run but no network!&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;could anyone please help&lt;/P&gt;&lt;P&gt;thanks&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 17 Dec 2017 05:00:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Ethernet-on-ENET2-with-imx6sx-in-u-boot/m-p/725670#M112854</guid>
      <dc:creator>huihuang</dc:creator>
      <dc:date>2017-12-17T05:00:45Z</dc:date>
    </item>
    <item>
      <title>Re: Ethernet on ENET2 with imx6sx in u-boot</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Ethernet-on-ENET2-with-imx6sx-in-u-boot/m-p/725671#M112855</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Hui&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;one can check settings for external clock in IOMUXC_GPR_GPR1&lt;/P&gt;&lt;P&gt;which are defined in setup_fec() mx6sxsabresd.c&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="http://git.freescale.com/git/cgit.cgi/imx/uboot-imx.git/tree/board/freescale/mx6sxsabresd/mx6sxsabresd.c?h=imx_v2016.03_4.1.15_2.0.0_ga&amp;amp;id=rel_imx_4.1.15_2.1.0_ga" title="http://git.freescale.com/git/cgit.cgi/imx/uboot-imx.git/tree/board/freescale/mx6sxsabresd/mx6sxsabresd.c?h=imx_v2016.03_4.1.15_2.0.0_ga&amp;amp;id=rel_imx_4.1.15_2.1.0_ga"&gt;uboot-imx.git - Freescale i.MX u-boot Tree&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 18 Dec 2017 08:16:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Ethernet-on-ENET2-with-imx6sx-in-u-boot/m-p/725671#M112855</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2017-12-18T08:16:05Z</dc:date>
    </item>
    <item>
      <title>Re: Ethernet on ENET2 with imx6sx in u-boot</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Ethernet-on-ENET2-with-imx6sx-in-u-boot/m-p/725672#M112856</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear Igor,&lt;/P&gt;&lt;P&gt;thanks for the answer, but i was not lucky!&lt;/P&gt;&lt;P&gt;here is the SCH of PHY and SOC:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/30111i1FA1D551EC1D2E5F/image-size/large?v=v2&amp;amp;px=999" title="sch.png" alt="sch.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;i&amp;nbsp; use y-boot imx: and modified the FEC pin mux: this is part of &lt;STRONG&gt;board/freescale/mx6sxsabresd/mx6sxsabresd.c&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;static iomux_v3_cfg_t const fec2_pads[] = {&lt;BR /&gt; MX6_PAD_ENET1_MDC__ENET2_MDC | MUX_PAD_CTRL(ENET_PAD_CTRL),&lt;BR /&gt; MX6_PAD_ENET1_MDIO__ENET2_MDIO | MUX_PAD_CTRL(ENET_PAD_CTRL),&lt;BR /&gt; MX6_PAD_RGMII2_RXC__ENET2_RX_ER | MUX_PAD_CTRL(ENET_PAD_CTRL),&lt;BR /&gt; MX6_PAD_RGMII2_RX_CTL__ENET2_RX_EN | MUX_PAD_CTRL(ENET_RX_PAD_CTRL),&lt;BR /&gt; MX6_PAD_RGMII2_RD0__GPIO5_IO_12 | MUX_PAD_CTRL(ENET_RX_PAD_CTRL),&lt;BR /&gt; MX6_PAD_RGMII2_RD1__GPIO5_IO_13 | MUX_PAD_CTRL(ENET_RX_PAD_CTRL),&lt;BR /&gt; MX6_PAD_RGMII2_TX_CTL__ENET2_TX_EN | MUX_PAD_CTRL(ENET_PAD_CTRL),&lt;BR /&gt; MX6_PAD_RGMII2_TD0__GPIO5_IO_18 | MUX_PAD_CTRL(ENET_PAD_CTRL),&lt;BR /&gt; MX6_PAD_RGMII2_TD1__GPIO5_IO_19 | MUX_PAD_CTRL(ENET_PAD_CTRL),&lt;BR /&gt;};&lt;BR /&gt;/*&lt;BR /&gt;static iomux_v3_cfg_t const fec2_pads[] = {&lt;BR /&gt; MX6_PAD_ENET1_MDC__ENET2_MDC | MUX_PAD_CTRL(ENET_PAD_CTRL),&lt;BR /&gt; MX6_PAD_ENET1_MDIO__ENET2_MDIO | MUX_PAD_CTRL(ENET_PAD_CTRL),&lt;BR /&gt; MX6_PAD_RGMII2_RX_CTL__ENET2_RX_EN | MUX_PAD_CTRL(ENET_RX_PAD_CTRL),&lt;BR /&gt; MX6_PAD_RGMII2_RD0__ENET2_RX_DATA_0 | MUX_PAD_CTRL(ENET_RX_PAD_CTRL),&lt;BR /&gt; MX6_PAD_RGMII2_RD1__ENET2_RX_DATA_1 | MUX_PAD_CTRL(ENET_RX_PAD_CTRL),&lt;BR /&gt; MX6_PAD_RGMII2_RD2__ENET2_RX_DATA_2 | MUX_PAD_CTRL(ENET_RX_PAD_CTRL),&lt;BR /&gt; MX6_PAD_RGMII2_RD3__ENET2_RX_DATA_3 | MUX_PAD_CTRL(ENET_RX_PAD_CTRL),&lt;BR /&gt; MX6_PAD_RGMII2_RXC__ENET2_RX_CLK | MUX_PAD_CTRL(ENET_RX_PAD_CTRL),&lt;BR /&gt; MX6_PAD_RGMII2_TX_CTL__ENET2_TX_EN | MUX_PAD_CTRL(ENET_PAD_CTRL),&lt;BR /&gt; MX6_PAD_RGMII2_TD0__ENET2_TX_DATA_0 | MUX_PAD_CTRL(ENET_PAD_CTRL),&lt;BR /&gt; MX6_PAD_RGMII2_TD1__ENET2_TX_DATA_1 | MUX_PAD_CTRL(ENET_PAD_CTRL),&lt;BR /&gt; MX6_PAD_RGMII2_TD2__ENET2_TX_DATA_2 | MUX_PAD_CTRL(ENET_PAD_CTRL),&lt;BR /&gt; MX6_PAD_RGMII2_TD3__ENET2_TX_DATA_3 | MUX_PAD_CTRL(ENET_PAD_CTRL),&lt;BR /&gt; MX6_PAD_RGMII2_TXC__ENET2_RGMII_TXC | MUX_PAD_CTRL(ENET_PAD_CTRL),&lt;BR /&gt;};&lt;BR /&gt;*/&lt;BR /&gt;static iomux_v3_cfg_t const phy_control_pads[] = {&lt;BR /&gt; /* 25MHz Ethernet PHY Clock */&lt;BR /&gt; /*MX6_PAD_ENET2_RX_CLK__ENET2_REF_CLK_25M | MUX_PAD_CTRL(ENET_CLK_PAD_CTRL),*/&lt;/P&gt;&lt;P&gt;/* 50M Ethernet clock*/&lt;BR /&gt; MX6_PAD_ENET2_TX_CLK__ENET2_REF_CLK2 | MUX_PAD_CTRL(ENET_CLK_PAD_CTRL),&lt;/P&gt;&lt;P&gt;/* ENET PHY Power */&lt;BR /&gt; /*MX6_PAD_ENET2_COL__GPIO2_IO_6 | MUX_PAD_CTRL(NO_PAD_CTRL),*/&lt;/P&gt;&lt;P&gt;/* AR8031 PHY Reset */&lt;BR /&gt; /*MX6_PAD_ENET2_CRS__GPIO2_IO_7 | MUX_PAD_CTRL(NO_PAD_CTRL),*/&lt;BR /&gt;};&lt;/P&gt;&lt;P&gt;static int setup_fec(int fec_id)&lt;BR /&gt;{&lt;BR /&gt; struct anatop_regs *anatop = (struct anatop_regs *)ANATOP_BASE_ADDR;&lt;BR /&gt; struct iomuxc_gpr_base_regs *const iomuxc_gpr_regs&lt;BR /&gt; = (struct iomuxc_gpr_base_regs *) IOMUXC_GPR_BASE_ADDR;&lt;BR /&gt; int reg;&lt;/P&gt;&lt;P&gt;if (0 == fec_id)&lt;BR /&gt; /* Use 125M anatop loopback REF_CLK1 for ENET1, clear gpr1[13], gpr1[17]*/&lt;BR /&gt; clrsetbits_le32(&amp;amp;iomuxc_gpr_regs-&amp;gt;gpr[1], IOMUX_GPR1_FEC1_MASK, 0);&lt;BR /&gt; else&lt;BR /&gt; /* Use 125M anatop loopback REF_CLK1 for ENET2, clear gpr1[14], gpr1[18]*/&lt;BR /&gt; clrsetbits_le32(&amp;amp;iomuxc_gpr_regs-&amp;gt;gpr[1], IOMUX_GPR1_FEC2_MASK, 0);&lt;/P&gt;&lt;P&gt;imx_iomux_v3_setup_multiple_pads(phy_control_pads,&lt;BR /&gt; ARRAY_SIZE(phy_control_pads));&lt;/P&gt;&lt;P&gt;/* Enable the ENET power, active low */&lt;BR /&gt; /*gpio_direction_output(IMX_GPIO_NR(2, 6) , 0);*/&lt;/P&gt;&lt;P&gt;/* Reset AR8031 PHY */&lt;BR /&gt; /*gpio_direction_output(IMX_GPIO_NR(2, 7) , 0);&lt;BR /&gt; udelay(500);&lt;BR /&gt; gpio_set_value(IMX_GPIO_NR(2, 7), 1);*/&lt;/P&gt;&lt;P&gt;/*&lt;BR /&gt; reg = readl(&amp;amp;anatop-&amp;gt;pll_enet);&lt;BR /&gt; reg |= BM_ANADIG_PLL_ENET_REF_25M_ENABLE;&lt;BR /&gt; writel(reg, &amp;amp;anatop-&amp;gt;pll_enet);&lt;/P&gt;&lt;P&gt;return enable_fec_anatop_clock(fec_id, ENET_125MHZ);*/&lt;BR /&gt; return 1;&lt;BR /&gt;}&lt;/P&gt;&lt;P&gt;int board_eth_init(bd_t *bis)&lt;BR /&gt;{&lt;BR /&gt; int retval;&lt;/P&gt;&lt;P&gt;if (0 == CONFIG_FEC_ENET_DEV)&lt;BR /&gt; imx_iomux_v3_setup_multiple_pads(fec1_pads, ARRAY_SIZE(fec1_pads));&lt;BR /&gt; else&lt;BR /&gt; imx_iomux_v3_setup_multiple_pads(fec2_pads, ARRAY_SIZE(fec2_pads));&lt;/P&gt;&lt;P&gt;setup_fec(CONFIG_FEC_ENET_DEV);&lt;BR /&gt; retval=cpu_eth_init(bis);&lt;BR /&gt; return retval;&lt;BR /&gt;}&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;would you please help.&lt;/P&gt;&lt;P&gt;thanks&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 19 Dec 2017 06:32:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Ethernet-on-ENET2-with-imx6sx-in-u-boot/m-p/725672#M112856</guid>
      <dc:creator>huihuang</dc:creator>
      <dc:date>2017-12-19T06:32:47Z</dc:date>
    </item>
  </channel>
</rss>