<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 Off-Chip Trace i.MX6UL</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Off-Chip-Trace-i-MX6UL/m-p/725077#M112752</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm looking for information or documents that tell me how to use the trace feature on i.MX6UL.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I saw that there was an Embedded Trace Macrocell (ETM) and Embedded Trace Buffer (ETB). In this case, it is necessary to read with the JTAG the buffer (ETB).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I would like in my case to make code coverage. I think the best solution is to use the trace port unit. However, I can not find the port to use and the pins.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is it possible to recover the traces with for example the LAUTERBACH Off-Chip Trace Solution probe ?&lt;BR /&gt;Is the trace port available and if so where can I find the pins?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks for your help&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Cordially&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 11 Apr 2018 12:49:21 GMT</pubDate>
    <dc:creator>guillaume17</dc:creator>
    <dc:date>2018-04-11T12:49:21Z</dc:date>
    <item>
      <title>Off-Chip Trace i.MX6UL</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Off-Chip-Trace-i-MX6UL/m-p/725077#M112752</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm looking for information or documents that tell me how to use the trace feature on i.MX6UL.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I saw that there was an Embedded Trace Macrocell (ETM) and Embedded Trace Buffer (ETB). In this case, it is necessary to read with the JTAG the buffer (ETB).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I would like in my case to make code coverage. I think the best solution is to use the trace port unit. However, I can not find the port to use and the pins.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is it possible to recover the traces with for example the LAUTERBACH Off-Chip Trace Solution probe ?&lt;BR /&gt;Is the trace port available and if so where can I find the pins?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks for your help&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Cordially&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 11 Apr 2018 12:49:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Off-Chip-Trace-i-MX6UL/m-p/725077#M112752</guid>
      <dc:creator>guillaume17</dc:creator>
      <dc:date>2018-04-11T12:49:21Z</dc:date>
    </item>
    <item>
      <title>Re: Off-Chip Trace</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Off-Chip-Trace-i-MX6UL/m-p/725078#M112753</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;&amp;nbsp;Use section 4.1.1 (Muxing Options) of the i.MX 6UL Reference Manual (Rev. 1, &lt;BR /&gt;04/2016) for “ARM_PLATFORM” instance, signals EVENTx, TRACEx, mux-ed with &lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;LCD signals.&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;&lt;A class="link-titled" href="https://www.nxp.com/docs/en/reference-manual/IMX6ULRM.pdf" title="https://www.nxp.com/docs/en/reference-manual/IMX6ULRM.pdf"&gt;https://www.nxp.com/docs/en/reference-manual/IMX6ULRM.pdf&lt;/A&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Yuri&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 12 Apr 2018 07:39:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Off-Chip-Trace-i-MX6UL/m-p/725078#M112753</guid>
      <dc:creator>Yuri</dc:creator>
      <dc:date>2018-04-12T07:39:20Z</dc:date>
    </item>
    <item>
      <title>Re: Off-Chip Trace i.MX6UL</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Off-Chip-Trace-i-MX6UL/m-p/725079#M112754</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;Appears, the LCD IF can not be used as TRACE IF. The TRACE IF might be used by SoC&lt;/P&gt;&lt;P&gt;team for internal test only. Currently, it uses the JTAG IF to connect to Lauterbach Trace32&lt;/P&gt;&lt;P&gt;on our EVK board.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Yuri.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 09 Jul 2018 09:19:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Off-Chip-Trace-i-MX6UL/m-p/725079#M112754</guid>
      <dc:creator>Yuri</dc:creator>
      <dc:date>2018-07-09T09:19:39Z</dc:date>
    </item>
  </channel>
</rss>