<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processorsのトピックcore-image-minimal has bluetooth</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/core-image-minimal-has-bluetooth/m-p/723723#M112529</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am trying to build core-image-minimal receipe for iMx7 (Yocto project), the image gets successfully built but it has bluetooth, caam and lot of other stuff. How can I remove these from including in the minimal-image?&lt;/P&gt;&lt;P&gt;core-image-minimal should only have things required for just booting nothing else, somehow other packages are getting added.&amp;nbsp;&lt;/P&gt;&lt;P&gt;MACHINE = "imx7dsabresd"&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have tried to remove bluetooth by adding the following in my local.config but this could not remove bluetooth from the kernel image that is produced.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;DISTRO_FEATURES_remove = "bluetooth bluez5 bluez-hcidump" &lt;BR /&gt;DISTRO_FEATURES_BACKFILL_remove ="bluez5"&lt;BR /&gt;DISTRO_FEATURES_BACKFILL_CONSIDERED_remove ="bluez5"&lt;BR /&gt;DISTRO_FEATURES_DEFAULT_remove = " bluetooth bluez5" &amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 20 Nov 2017 18:55:32 GMT</pubDate>
    <dc:creator>saikirank</dc:creator>
    <dc:date>2017-11-20T18:55:32Z</dc:date>
    <item>
      <title>core-image-minimal has bluetooth</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/core-image-minimal-has-bluetooth/m-p/723723#M112529</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am trying to build core-image-minimal receipe for iMx7 (Yocto project), the image gets successfully built but it has bluetooth, caam and lot of other stuff. How can I remove these from including in the minimal-image?&lt;/P&gt;&lt;P&gt;core-image-minimal should only have things required for just booting nothing else, somehow other packages are getting added.&amp;nbsp;&lt;/P&gt;&lt;P&gt;MACHINE = "imx7dsabresd"&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have tried to remove bluetooth by adding the following in my local.config but this could not remove bluetooth from the kernel image that is produced.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;DISTRO_FEATURES_remove = "bluetooth bluez5 bluez-hcidump" &lt;BR /&gt;DISTRO_FEATURES_BACKFILL_remove ="bluez5"&lt;BR /&gt;DISTRO_FEATURES_BACKFILL_CONSIDERED_remove ="bluez5"&lt;BR /&gt;DISTRO_FEATURES_DEFAULT_remove = " bluetooth bluez5" &amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 20 Nov 2017 18:55:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/core-image-minimal-has-bluetooth/m-p/723723#M112529</guid>
      <dc:creator>saikirank</dc:creator>
      <dc:date>2017-11-20T18:55:32Z</dc:date>
    </item>
    <item>
      <title>Re: core-image-minimal has bluetooth</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/core-image-minimal-has-bluetooth/m-p/723724#M112530</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I think you can disable the features in kernel "menuconfig".&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 18 Dec 2017 01:03:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/core-image-minimal-has-bluetooth/m-p/723724#M112530</guid>
      <dc:creator>jimmychan</dc:creator>
      <dc:date>2017-12-18T01:03:36Z</dc:date>
    </item>
  </channel>
</rss>