<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: IMX6DL LINUX4.9 How to add fb2？</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/IMX6DL-LINUX4-9-How-to-add-fb2/m-p/723354#M112466</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks,I already solve the problem.&lt;/P&gt;&lt;P&gt;The problem is "mxc_sdc_fb &lt;A data-content-finding="Community" href="mailto:fb@2"&gt;&lt;SPAN style="color: #0066cc; text-decoration: underline;"&gt;fb@2&lt;/SPAN&gt;&lt;/A&gt;: ipu0-di0 already in use".&lt;/P&gt;&lt;P&gt;So,I change hdmi to ipu0-di1 in&amp;nbsp; dts file,and I can use fb2 to display HDMI.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 08 Mar 2018 00:46:33 GMT</pubDate>
    <dc:creator>sendong</dc:creator>
    <dc:date>2018-03-08T00:46:33Z</dc:date>
    <item>
      <title>IMX6DL LINUX4.9 How to add fb2？</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX6DL-LINUX4-9-How-to-add-fb2/m-p/723352#M112464</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I have a imx6dl board，and I use yocto project 2.2 to bitbake fsl-image-qt5,linux 4.9.0 and qt5.8,&lt;/P&gt;&lt;P&gt;but when I boot the board，and setenv mmcargs 'setenv bootargs console=${console},${baudrate} ${smp} root=${mmcroot} video=mxcfb0:dev=ldb,if=RGB24 ldb=sin0 video=mxcfb2:dev=hdmi,1280x800M@60,if=RGB24'.&lt;/P&gt;&lt;P&gt;In /dev/,there are only fb0 and fb1,I want to use fb2 to display hdmi.&lt;/P&gt;&lt;P&gt;Here is the error:&lt;/P&gt;&lt;P&gt;mxc_sdc_fb &lt;A href="mailto:fb@0"&gt;fb@0&lt;/A&gt;: registered mxc display driver ldb&lt;BR /&gt;imx-ipuv3 2400000.ipu: IPU DMFC DP HIGH RESOLUTION: 1(0,1), 5B(2~5), 5F(6,7)&lt;BR /&gt;Console: switching to colour frame buffer device 160x50&lt;BR /&gt;mxc_hdmi 20e0000.hdmi_video: Detected HDMI controller 0x13:0x1a:0xa0:0xc1&lt;BR /&gt;fbcvt: &lt;A href="mailto:1280x800@60"&gt;1280x800@60&lt;/A&gt;: CVT Name - 1.024MA&lt;BR /&gt;mxc_sdc_fb &lt;A href="mailto:fb@2"&gt;fb@2&lt;/A&gt;: registered mxc display driver hdmi&lt;BR /&gt;mxc_sdc_fb &lt;A href="mailto:fb@2"&gt;fb@2&lt;/A&gt;: ipu0-di0 already in use&lt;BR /&gt;mxc_sdc_fb: probe of &lt;A href="mailto:fb@2"&gt;fb@2&lt;/A&gt; failed with error -16&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please help me ,thank you !!!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 02 Mar 2018 07:53:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX6DL-LINUX4-9-How-to-add-fb2/m-p/723352#M112464</guid>
      <dc:creator>sendong</dc:creator>
      <dc:date>2018-03-02T07:53:59Z</dc:date>
    </item>
    <item>
      <title>Re: IMX6DL LINUX4.9 How to add fb2？</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX6DL-LINUX4-9-How-to-add-fb2/m-p/723353#M112465</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;if you need to use fb2, you need to set mxcfb1. fb2 is relevent to mxcfb1&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 06 Mar 2018 07:57:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX6DL-LINUX4-9-How-to-add-fb2/m-p/723353#M112465</guid>
      <dc:creator>joanxie</dc:creator>
      <dc:date>2018-03-06T07:57:16Z</dc:date>
    </item>
    <item>
      <title>Re: IMX6DL LINUX4.9 How to add fb2？</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX6DL-LINUX4-9-How-to-add-fb2/m-p/723354#M112466</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks,I already solve the problem.&lt;/P&gt;&lt;P&gt;The problem is "mxc_sdc_fb &lt;A data-content-finding="Community" href="mailto:fb@2"&gt;&lt;SPAN style="color: #0066cc; text-decoration: underline;"&gt;fb@2&lt;/SPAN&gt;&lt;/A&gt;: ipu0-di0 already in use".&lt;/P&gt;&lt;P&gt;So,I change hdmi to ipu0-di1 in&amp;nbsp; dts file,and I can use fb2 to display HDMI.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 08 Mar 2018 00:46:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX6DL-LINUX4-9-How-to-add-fb2/m-p/723354#M112466</guid>
      <dc:creator>sendong</dc:creator>
      <dc:date>2018-03-08T00:46:33Z</dc:date>
    </item>
    <item>
      <title>Re: IMX6DL LINUX4.9 How to add fb2？</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX6DL-LINUX4-9-How-to-add-fb2/m-p/723355#M112467</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;yes your issue is that IPU0-DI0 is used, you just change another channel, even IPU1-DI0 in source code, but let me correct,mxcfb2 doesn't equal to fb2. &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 16 Mar 2018 07:02:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX6DL-LINUX4-9-How-to-add-fb2/m-p/723355#M112467</guid>
      <dc:creator>joanxie</dc:creator>
      <dc:date>2018-03-16T07:02:43Z</dc:date>
    </item>
  </channel>
</rss>