<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 Re: I.MX6ULL Image Rotation Using PXP</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/I-MX6ULL-Image-Rotation-Using-PXP/m-p/723263#M112409</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi tk&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am not aware of documentation for usage pxp library, but&lt;/P&gt;&lt;P&gt;possible rotation shifting is described in sect.41.3.25 Rotation&lt;/P&gt;&lt;P&gt;i.MX6ULL Reference Manual in "NOTE" on p.2514&lt;BR /&gt;&lt;A href="http://www.nxp.com/docs/en/reference-manual/IMX6ULLRM.pdf"&gt;http://www.nxp.com/docs/en/reference-manual/IMX6ULLRM.pdf&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 02 Mar 2018 10:38:24 GMT</pubDate>
    <dc:creator>igorpadykov</dc:creator>
    <dc:date>2018-03-02T10:38:24Z</dc:date>
    <item>
      <title>I.MX6ULL Image Rotation Using PXP</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/I-MX6ULL-Image-Rotation-Using-PXP/m-p/723262#M112408</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I am using i.mx6ull chipset with release fsl-yocto-L4.9.11_1.0.0. I would like to implement framebuffer image rotation (90 degree) using PXP. I manage to run imx-test/Display/pxp_test.out demo on EVK. Below are the snapshot of image for no rotation, with command: .pxp_test.out -I "-o/dev/fb0 -r0"&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/27078iD48FB8B159FEBAE2/image-size/large?v=v2&amp;amp;px=999" title="rotation_00.jpeg" alt="rotation_00.jpeg" /&gt;&lt;/span&gt; Diagram 1&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;When I executed rotation of 90degree with command: ./pxp_test.out -I "-o/dev/fb0 -r90", I would expect the image is rotate 90 degree, with a section of the image fall outside of the LCD screen, as shown below.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/27153i2C10F9DB37DD6AEC/image-size/large?v=v2&amp;amp;px=999" title="simulate_rotate90_crop.png" alt="simulate_rotate90_crop.png" /&gt;&lt;/span&gt;Diagram 2&lt;/P&gt;&lt;P&gt;But in actual the output is shown as below.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/27326i4CB51E64129C772C/image-size/large?v=v2&amp;amp;px=999" title="rotation_90.jpeg" alt="rotation_90.jpeg" /&gt;&lt;/span&gt; Diagram 3&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We tried to modify the parameter in the pxp_test.c(especially on width, height of srect/drect/s0_param parameters) to try achieve of Diagram2 but it is unsuccessful.&lt;/P&gt;&lt;P&gt;Kindly advise what changes is require in code to get output as in Diagram 2.&lt;/P&gt;&lt;P&gt;It would be very helpful if I can have some documentations on usage of the pxp library&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 02 Mar 2018 02:59:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/I-MX6ULL-Image-Rotation-Using-PXP/m-p/723262#M112408</guid>
      <dc:creator>tkcheng01</dc:creator>
      <dc:date>2018-03-02T02:59:06Z</dc:date>
    </item>
    <item>
      <title>Re: I.MX6ULL Image Rotation Using PXP</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/I-MX6ULL-Image-Rotation-Using-PXP/m-p/723263#M112409</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi tk&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am not aware of documentation for usage pxp library, but&lt;/P&gt;&lt;P&gt;possible rotation shifting is described in sect.41.3.25 Rotation&lt;/P&gt;&lt;P&gt;i.MX6ULL Reference Manual in "NOTE" on p.2514&lt;BR /&gt;&lt;A href="http://www.nxp.com/docs/en/reference-manual/IMX6ULLRM.pdf"&gt;http://www.nxp.com/docs/en/reference-manual/IMX6ULLRM.pdf&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 02 Mar 2018 10:38:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/I-MX6ULL-Image-Rotation-Using-PXP/m-p/723263#M112409</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2018-03-02T10:38:24Z</dc:date>
    </item>
    <item>
      <title>Re: I.MX6ULL Image Rotation Using PXP</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/I-MX6ULL-Image-Rotation-Using-PXP/m-p/723264#M112410</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I found another pxp example(pxp_v4l2_test.out) in the imx-test, which is working. Command i use as below:&lt;BR /&gt;pxp_v4l2_test.out -sx 240 -sy 400 -res 400:80 -dst 0:0:240:400 -a 0 -w 2 -f 1 -r 270 daisy-400x240-565.rgb BLANK &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 21 Mar 2018 10:47:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/I-MX6ULL-Image-Rotation-Using-PXP/m-p/723264#M112410</guid>
      <dc:creator>tkcheng01</dc:creator>
      <dc:date>2018-03-21T10:47:42Z</dc:date>
    </item>
  </channel>
</rss>