<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: ov5642 30fps not working in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/ov5642-30fps-not-working/m-p/722435#M112329</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I got mxc_v4l2_capture.out generated by using Yocto Image and copied the binary into my root file system..&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Executed the following command:&lt;/P&gt;&lt;P&gt;./mxc_v4l2_capture.out -iw 640 -ih 480 -ow 640 -oh 480 -i1 -c&amp;nbsp; 50 -fr 30 test.yuv&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Many times i got the following errors:&lt;/P&gt;&lt;P&gt;./mxc_v4l2_capture.out -iw 640 -ih 480 -ow 640 -oh 480 -i&lt;BR /&gt; 1 -c 50power_down_callback: ipu0/csi0&lt;BR /&gt;0 -fr 30 test1.yuv&lt;BR /&gt;in_width = 640, in_height = 480&lt;BR /&gt;mxc_cam_select_input: input(1) CSI MEM&lt;BR /&gt;out_width = 640, out_height = 480&lt;BR /&gt;top = 0, left = 0&lt;BR /&gt;sensor chip is ov5642_camera&lt;BR /&gt;sensor supported frame size:&lt;BR /&gt; 640x480&lt;BR /&gt; 320x240&lt;BR /&gt; 720x480&lt;BR /&gt; 720x576&lt;BR /&gt; 1280x720&lt;BR /&gt; 1920x1080&lt;BR /&gt; 2592x1944&lt;BR /&gt; 176x144&lt;BR /&gt; 1024x768&lt;BR /&gt;sensor frame format: YUYV&lt;BR /&gt;ov5642_write_reg:write reg error:reg=3502,val=80 ret=-5&lt;BR /&gt;ov5642_apply_settings, write reg 0x3502 failed&lt;BR /&gt;mxc_v4l2_s_param: vidioc_int_s_parm returned an error -5&lt;BR /&gt;VIDIOC_S_PARM failed&lt;BR /&gt;get format failed&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Each time writing to a particular register fails.. Sometimes, it is getting successful.. Why is such behavior.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I tried to play the yuv file in windows, I am getting the pink color layer above the video sometimes, if we can remove that pink layer, my problem will be almost solved.. Can you help in understanding why is that layer coming above and how can I remove that..&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Attached screenshot for your reference..&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/24000iB56BC79080541572/image-size/large?v=v2&amp;amp;px=999" title="Pink Layer.jpg" alt="Pink Layer.jpg" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 29 May 2018 07:20:32 GMT</pubDate>
    <dc:creator>jamalmohiuddin</dc:creator>
    <dc:date>2018-05-29T07:20:32Z</dc:date>
    <item>
      <title>ov5642 30fps not working</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/ov5642-30fps-not-working/m-p/722430#M112324</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Guys,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We have a customized i.MX6Q Board based on sabrelite reference board.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We have the following configuration:&lt;/P&gt;&lt;P&gt;Linux : 3.10.53&lt;/P&gt;&lt;P&gt;Gstreamer 1.0 latest i.MX6 Plugins&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We connected OV5642 Camera over CSI Interface..Used the following command to display the camera output on the screen.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;gst-launch-1.0 imxv4l2videosrc device=/dev/video0 imx-capture-mode=4 fps-n=15&amp;nbsp;! imxipuvideosink&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;It works, but initially, it takes time to settle for few seconds,&amp;nbsp; there is genlock issue&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;But when I modify the fps to 30, I get distorted output.. What do you think is wrong here.. Any help is appreciated...&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/51153iA66F1067B1CCCB61/image-size/large?v=v2&amp;amp;px=999" title="Distorted_30fps.jpg" alt="Distorted_30fps.jpg" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The problem is not with OV5642, as it works well when I connect it to Boundary devices reference board at 30fps.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Jamal&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 25 May 2018 05:24:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/ov5642-30fps-not-working/m-p/722430#M112324</guid>
      <dc:creator>jamalmohiuddin</dc:creator>
      <dc:date>2018-05-25T05:24:09Z</dc:date>
    </item>
    <item>
      <title>Re: ov5642 30fps not working</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/ov5642-30fps-not-working/m-p/722431#M112325</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;1) could you test by unit test? do you have the same error by unit test?&lt;/P&gt;&lt;P&gt;2) try to use the command as user guide mentioned:&lt;/P&gt;&lt;P&gt;Camera preview example:&lt;BR /&gt;gst-launch-1.0 imxv4l2src device=/dev/video1 ! 'video/x-raw,&lt;BR /&gt;format=(string)UYVY,width=640,height=480,framerate=(fraction)30/1'&lt;BR /&gt;! imxv4l2sink&lt;/P&gt;&lt;P&gt;but I suggest that you use unit test first&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 25 May 2018 07:52:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/ov5642-30fps-not-working/m-p/722431#M112325</guid>
      <dc:creator>joanxie</dc:creator>
      <dc:date>2018-05-25T07:52:06Z</dc:date>
    </item>
    <item>
      <title>Re: ov5642 30fps not working</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/ov5642-30fps-not-working/m-p/722432#M112326</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Can you please provide more detail about unit test...Which unit test are you referring?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 25 May 2018 08:49:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/ov5642-30fps-not-working/m-p/722432#M112326</guid>
      <dc:creator>jamalmohiuddin</dc:creator>
      <dc:date>2018-05-25T08:49:43Z</dc:date>
    </item>
    <item>
      <title>Re: ov5642 30fps not working</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/ov5642-30fps-not-working/m-p/722433#M112327</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;one can use "mxc_v4l2_capture.out", for more detaile information, pls refer to the chapter 20.2.5 Unit Test of i.MX 6 Linux Reference Manual,&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 28 May 2018 08:22:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/ov5642-30fps-not-working/m-p/722433#M112327</guid>
      <dc:creator>joanxie</dc:creator>
      <dc:date>2018-05-28T08:22:18Z</dc:date>
    </item>
    <item>
      <title>Re: ov5642 30fps not working</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/ov5642-30fps-not-working/m-p/722434#M112328</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am using buildroot.. Do you have steps to compile mxc_v4l2_capture.out for buildroot. I know that this is present in Yocto. But we have our images running in Yocto..&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 28 May 2018 11:03:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/ov5642-30fps-not-working/m-p/722434#M112328</guid>
      <dc:creator>jamalmohiuddin</dc:creator>
      <dc:date>2018-05-28T11:03:12Z</dc:date>
    </item>
    <item>
      <title>Re: ov5642 30fps not working</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/ov5642-30fps-not-working/m-p/722435#M112329</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I got mxc_v4l2_capture.out generated by using Yocto Image and copied the binary into my root file system..&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Executed the following command:&lt;/P&gt;&lt;P&gt;./mxc_v4l2_capture.out -iw 640 -ih 480 -ow 640 -oh 480 -i1 -c&amp;nbsp; 50 -fr 30 test.yuv&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Many times i got the following errors:&lt;/P&gt;&lt;P&gt;./mxc_v4l2_capture.out -iw 640 -ih 480 -ow 640 -oh 480 -i&lt;BR /&gt; 1 -c 50power_down_callback: ipu0/csi0&lt;BR /&gt;0 -fr 30 test1.yuv&lt;BR /&gt;in_width = 640, in_height = 480&lt;BR /&gt;mxc_cam_select_input: input(1) CSI MEM&lt;BR /&gt;out_width = 640, out_height = 480&lt;BR /&gt;top = 0, left = 0&lt;BR /&gt;sensor chip is ov5642_camera&lt;BR /&gt;sensor supported frame size:&lt;BR /&gt; 640x480&lt;BR /&gt; 320x240&lt;BR /&gt; 720x480&lt;BR /&gt; 720x576&lt;BR /&gt; 1280x720&lt;BR /&gt; 1920x1080&lt;BR /&gt; 2592x1944&lt;BR /&gt; 176x144&lt;BR /&gt; 1024x768&lt;BR /&gt;sensor frame format: YUYV&lt;BR /&gt;ov5642_write_reg:write reg error:reg=3502,val=80 ret=-5&lt;BR /&gt;ov5642_apply_settings, write reg 0x3502 failed&lt;BR /&gt;mxc_v4l2_s_param: vidioc_int_s_parm returned an error -5&lt;BR /&gt;VIDIOC_S_PARM failed&lt;BR /&gt;get format failed&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Each time writing to a particular register fails.. Sometimes, it is getting successful.. Why is such behavior.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I tried to play the yuv file in windows, I am getting the pink color layer above the video sometimes, if we can remove that pink layer, my problem will be almost solved.. Can you help in understanding why is that layer coming above and how can I remove that..&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Attached screenshot for your reference..&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/24000iB56BC79080541572/image-size/large?v=v2&amp;amp;px=999" title="Pink Layer.jpg" alt="Pink Layer.jpg" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 29 May 2018 07:20:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/ov5642-30fps-not-working/m-p/722435#M112329</guid>
      <dc:creator>jamalmohiuddin</dc:creator>
      <dc:date>2018-05-29T07:20:32Z</dc:date>
    </item>
    <item>
      <title>Re: ov5642 30fps not working</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/ov5642-30fps-not-working/m-p/722436#M112330</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;how about try the "-i 0" in your command? any improvement?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 30 May 2018 02:52:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/ov5642-30fps-not-working/m-p/722436#M112330</guid>
      <dc:creator>joanxie</dc:creator>
      <dc:date>2018-05-30T02:52:02Z</dc:date>
    </item>
    <item>
      <title>Re: ov5642 30fps not working</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/ov5642-30fps-not-working/m-p/722437#M112331</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Same output.. That above layer is still present&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 30 May 2018 03:26:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/ov5642-30fps-not-working/m-p/722437#M112331</guid>
      <dc:creator>jamalmohiuddin</dc:creator>
      <dc:date>2018-05-30T03:26:32Z</dc:date>
    </item>
    <item>
      <title>Re: ov5642 30fps not working</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/ov5642-30fps-not-working/m-p/722438#M112332</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;the command you use means Capture the camera and store the 50 frames of YUV420 (VGA size) to the test.yuv file, try to use other capture format, if you don't know how to set the format, try to use mxc_v4l2_capture.out -help to find more detailed information.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 30 May 2018 06:21:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/ov5642-30fps-not-working/m-p/722438#M112332</guid>
      <dc:creator>joanxie</dc:creator>
      <dc:date>2018-05-30T06:21:20Z</dc:date>
    </item>
    <item>
      <title>Re: ov5642 30fps not working</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/ov5642-30fps-not-working/m-p/722439#M112333</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;As this issue is only happening in 30fps, and not in 15fps, the format should not be problem.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 30 May 2018 07:13:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/ov5642-30fps-not-working/m-p/722439#M112333</guid>
      <dc:creator>jamalmohiuddin</dc:creator>
      <dc:date>2018-05-30T07:13:36Z</dc:date>
    </item>
    <item>
      <title>Re: ov5642 30fps not working</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/ov5642-30fps-not-working/m-p/722440#M112334</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;when you use“./mxc_v4l2_capture.out -iw 640 -ih 480 -ow 640 -oh 480 -i1 -c&amp;nbsp; 50&lt;SPAN style="color: #ff0000;"&gt; -fr 15&lt;/SPAN&gt; test.yuv”， everything is ok?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 30 May 2018 07:26:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/ov5642-30fps-not-working/m-p/722440#M112334</guid>
      <dc:creator>joanxie</dc:creator>
      <dc:date>2018-05-30T07:26:41Z</dc:date>
    </item>
    <item>
      <title>Re: ov5642 30fps not working</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/ov5642-30fps-not-working/m-p/722441#M112335</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Playing test.yuv video in mplayer is same whether it is in 15fps or 30 fps.. The only difference comes when I run gstreamer pipeline.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/23809iABB8FD53340BC119/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 30 May 2018 08:14:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/ov5642-30fps-not-working/m-p/722441#M112335</guid>
      <dc:creator>jamalmohiuddin</dc:creator>
      <dc:date>2018-05-30T08:14:21Z</dc:date>
    </item>
    <item>
      <title>Re: ov5642 30fps not working</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/ov5642-30fps-not-working/m-p/722442#M112336</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;refer to the picture, it seems you set incorrect data format, try to check this first.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 30 May 2018 08:17:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/ov5642-30fps-not-working/m-p/722442#M112336</guid>
      <dc:creator>joanxie</dc:creator>
      <dc:date>2018-05-30T08:17:11Z</dc:date>
    </item>
    <item>
      <title>Re: ov5642 30fps not working</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/ov5642-30fps-not-working/m-p/722443#M112337</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Are you referring to windows yuv player or in &lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;mxc_v4l2_capture command..&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 30 May 2018 08:23:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/ov5642-30fps-not-working/m-p/722443#M112337</guid>
      <dc:creator>jamalmohiuddin</dc:creator>
      <dc:date>2018-05-30T08:23:09Z</dc:date>
    </item>
    <item>
      <title>Re: ov5642 30fps not working</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/ov5642-30fps-not-working/m-p/722444#M112338</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I mean mxc_v4l2_capture, you can use mxc_v4l2_capture -help&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 31 May 2018 07:15:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/ov5642-30fps-not-working/m-p/722444#M112338</guid>
      <dc:creator>joanxie</dc:creator>
      <dc:date>2018-05-31T07:15:06Z</dc:date>
    </item>
    <item>
      <title>Re: ov5642 30fps not working</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/ov5642-30fps-not-working/m-p/722445#M112339</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I have enabled all the logs in mxc ipu drivers. Can you look at the boot logs and gstreamer logs and tell if there is anything wrong.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Booting Linux on physical CPU 0x0&lt;BR /&gt;Linux version 3.10.53 (lloyd@ubuntu) (gcc version 4.8.3 20140320 (prerelease) (Sourcery CodeBench Lite 2014.05-29) ) #5 SMP PREEMPT Tue Jun 5 01:35:58 EDT 2018&lt;BR /&gt;CPU: ARMv7 Processor [412fc09a] revision 10 (ARMv7), cr=10c53c7d&lt;BR /&gt;CPU: PIPT / VIPT nonaliasing data cache, VIPT aliasing instruction cache&lt;BR /&gt;Machine: Freescale i.MX6 Quad/DualLite (Device Tree), model: Freescale i.MX6 Quad SABRE Smart Device Board&lt;BR /&gt;cma: CMA: reserved 320 MiB at 3c000000&lt;BR /&gt;Memory policy: ECC disabled, Data cache writealloc&lt;BR /&gt;PERCPU: Embedded 8 pages/cpu @815a1000 s8960 r8192 d15616 u32768&lt;BR /&gt;Built 1 zonelists in Zone order, mobility grouping on. Total pages: 260096&lt;BR /&gt;Kernel command line: console=ttymxc0,115200 video=mxcfb0:dev=ldb,LDB-XGA,if=RGB24 video=mxcfb1:dev=hdmi,1920x1080@60,if=RGB24 ldb=sin0 consoleblank=0 root=/dev/mmcblk3p2 rootwait rw&lt;BR /&gt;PID hash table entries: 4096 (order: 2, 16384 bytes)&lt;BR /&gt;Dentry cache hash table entries: 131072 (order: 7, 524288 bytes)&lt;BR /&gt;Inode-cache hash table entries: 65536 (order: 6, 262144 bytes)&lt;BR /&gt;Memory: 1024MB = 1024MB total&lt;BR /&gt;Memory: 697124k/697124k available, 351452k reserved, 0K highmem&lt;BR /&gt;Virtual kernel memory layout:&lt;BR /&gt; vector : 0xffff0000 - 0xffff1000 ( 4 kB)&lt;BR /&gt; fixmap : 0xfff00000 - 0xfffe0000 ( 896 kB)&lt;BR /&gt; vmalloc : 0xc0800000 - 0xff000000 (1000 MB)&lt;BR /&gt; lowmem : 0x80000000 - 0xc0000000 (1024 MB)&lt;BR /&gt; pkmap : 0x7fe00000 - 0x80000000 ( 2 MB)&lt;BR /&gt; modules : 0x7f000000 - 0x7fe00000 ( 14 MB)&lt;BR /&gt; .text : 0x80008000 - 0x80c79834 (12743 kB)&lt;BR /&gt; .init : 0x80c7a000 - 0x80cc6300 ( 305 kB)&lt;BR /&gt; .data : 0x80cc8000 - 0x80d1fe40 ( 352 kB)&lt;BR /&gt; .bss : 0x80d1fe40 - 0x80d8926c ( 422 kB)&lt;BR /&gt;SLUB: HWalign=64, Order=0-3, MinObjects=0, CPUs=4, Nodes=1&lt;BR /&gt;Preemptible hierarchical RCU implementation.&lt;BR /&gt;NR_IRQS:16 nr_irqs:16 16&lt;BR /&gt;L310 cache controller enabled&lt;BR /&gt;l2x0: 16 ways, CACHE_ID 0x410000c7, AUX_CTRL 0x32070000, Cache size: 1048576 B&lt;BR /&gt;sched_clock: 32 bits at 3000kHz, resolution 333ns, wraps every 1431655ms&lt;BR /&gt;CPU identified as i.MX6Q, silicon rev 1.5&lt;BR /&gt;Console: colour dummy device 80x30&lt;BR /&gt;Calibrating delay loop... 1581.05 BogoMIPS (lpj=7905280)&lt;BR /&gt;pid_max: default: 32768 minimum: 301&lt;BR /&gt;Mount-cache hash table entries: 512&lt;BR /&gt;CPU: Testing write buffer coherency: ok&lt;BR /&gt;CPU0: thread -1, cpu 0, socket 0, mpidr 80000000&lt;BR /&gt;Setting up static identity map for 0x8068b2b0 - 0x8068b308&lt;BR /&gt;CPU1: Booted secondary processor&lt;BR /&gt;CPU1: thread -1, cpu 1, socket 0, mpidr 80000001&lt;BR /&gt;CPU2: Booted secondary processor&lt;BR /&gt;CPU2: thread -1, cpu 2, socket 0, mpidr 80000002&lt;BR /&gt;CPU3: Booted secondary processor&lt;BR /&gt;CPU3: thread -1, cpu 3, socket 0, mpidr 80000003&lt;BR /&gt;Brought up 4 CPUs&lt;BR /&gt;SMP: Total of 4 processors activated (6324.22 BogoMIPS).&lt;BR /&gt;CPU: All CPU(s) started in SVC mode.&lt;BR /&gt;devtmpfs: initialized&lt;BR /&gt;pinctrl core: initialized pinctrl subsystem&lt;BR /&gt;regulator-dummy: no parameters&lt;BR /&gt;NET: Registered protocol family 16&lt;BR /&gt;DMA: preallocated 256 KiB pool for atomic coherent allocations&lt;BR /&gt;Use WDOG2 as reset source&lt;BR /&gt;syscon 20c8000.anatop: regmap [mem 0x020c8000-0x020c8fff] registered&lt;BR /&gt;vdd1p1: 800 &amp;lt;--&amp;gt; 1375 mV at 1100 mV &lt;BR /&gt;vdd3p0: 2625 &amp;lt;--&amp;gt; 3400 mV at 3000 mV &lt;BR /&gt;vdd2p5: 2000 &amp;lt;--&amp;gt; 2750 mV at 2400 mV &lt;BR /&gt;cpu: 725 &amp;lt;--&amp;gt; 1450 mV &lt;BR /&gt;vddpu: 725 &amp;lt;--&amp;gt; 1450 mV &lt;BR /&gt;vddsoc: 725 &amp;lt;--&amp;gt; 1450 mV &lt;BR /&gt;syscon 20e0000.iomuxc-gpr: regmap [mem 0x020e0000-0x020e0037] registered&lt;BR /&gt;syscon 21bc000.ocotp-ctrl: regmap [mem 0x021bc000-0x021bffff] registered&lt;BR /&gt;hw-breakpoint: found 5 (+1 reserved) breakpoint and 1 watchpoint registers.&lt;BR /&gt;hw-breakpoint: maximum watchpoint size is 4 bytes.&lt;BR /&gt;imx6q-pinctrl 20e0000.iomuxc: initialized IMX pinctrl driver&lt;BR /&gt;bio: create slab &amp;lt;bio-0&amp;gt; at 0&lt;BR /&gt;mxs-dma 110000.dma-apbh: initialized&lt;BR /&gt;usb_otg_vbus: 5000 mV &lt;BR /&gt;usb_h1_vbus: 5000 mV &lt;BR /&gt;wm8962-supply: no parameters&lt;BR /&gt;i2c-core: driver [max17135] using legacy suspend method&lt;BR /&gt;i2c-core: driver [max17135] using legacy resume method&lt;BR /&gt;SCSI subsystem initialized&lt;BR /&gt;usbcore: registered new interface driver usbfs&lt;BR /&gt;usbcore: registered new interface driver hub&lt;BR /&gt;usbcore: registered new device driver usb&lt;BR /&gt;i2c i2c-0: IMX I2C adapter registered&lt;BR /&gt;i2c i2c-1: IMX I2C adapter registered&lt;BR /&gt;i2c i2c-2: IMX I2C adapter registered&lt;BR /&gt;Linux video capture interface: v2.00&lt;BR /&gt;pps_core: LinuxPPS API ver. 1 registered&lt;BR /&gt;&lt;SPAN&gt;pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giometti &amp;lt;&lt;/SPAN&gt;&lt;A class="jive-link-email-small" href="mailto:giometti@linux.it"&gt;giometti@linux.it&lt;/A&gt;&lt;SPAN&gt;&amp;gt;&lt;/SPAN&gt;&lt;BR /&gt;PTP clock support registered&lt;BR /&gt;imx-ipuv3 2400000.ipu: &amp;lt;ipu_probe&amp;gt;&lt;BR /&gt;imx-ipuv3 2400000.ipu: IPU rev:4&lt;BR /&gt;imx-ipuv3 2400000.ipu: IPU CM Regs = c0816000&lt;BR /&gt;imx-ipuv3 2400000.ipu: IPU IC Regs = c081e000&lt;BR /&gt;imx-ipuv3 2400000.ipu: IPU IDMAC Regs = c0826000&lt;BR /&gt;imx-ipuv3 2400000.ipu: IPU DP Regs = c082e000&lt;BR /&gt;imx-ipuv3 2400000.ipu: IPU DC Regs = c0836000&lt;BR /&gt;imx-ipuv3 2400000.ipu: IPU DMFC Regs = c083e000&lt;BR /&gt;imx-ipuv3 2400000.ipu: IPU DI0 Regs = c0846000&lt;BR /&gt;imx-ipuv3 2400000.ipu: IPU DI1 Regs = c084e000&lt;BR /&gt;imx-ipuv3 2400000.ipu: IPU SMFC Regs = c0856000&lt;BR /&gt;imx-ipuv3 2400000.ipu: IPU CSI0 Regs = c085e000&lt;BR /&gt;imx-ipuv3 2400000.ipu: IPU CSI1 Regs = c0866000&lt;BR /&gt;imx-ipuv3 2400000.ipu: IPU CPMem = c0900000&lt;BR /&gt;imx-ipuv3 2400000.ipu: IPU TPMem = c08e0000&lt;BR /&gt;imx-ipuv3 2400000.ipu: IPU DC Template Mem = c0940000&lt;BR /&gt;imx-ipuv3 2400000.ipu: IPU Display Region 1 Mem = c086e000&lt;BR /&gt;imx-ipuv3 2400000.ipu: IPU VDI Regs = c086c000&lt;BR /&gt;imx-ipuv3 2400000.ipu: IPU DMFC NORMAL mode: 1(0~1), 5B(4,5), 5F(6,7)&lt;BR /&gt;imx-ipuv3 2400000.ipu: ipu_clk = 264000000&lt;BR /&gt;imx-ipuv3 2800000.ipu: &amp;lt;ipu_probe&amp;gt;&lt;BR /&gt;imx-ipuv3 2800000.ipu: IPU rev:4&lt;BR /&gt;imx-ipuv3 2800000.ipu: IPU CM Regs = c087a000&lt;BR /&gt;imx-ipuv3 2800000.ipu: IPU IC Regs = c087c000&lt;BR /&gt;imx-ipuv3 2800000.ipu: IPU IDMAC Regs = c087e000&lt;BR /&gt;imx-ipuv3 2800000.ipu: IPU DP Regs = c08bc000&lt;BR /&gt;imx-ipuv3 2800000.ipu: IPU DC Regs = c08be000&lt;BR /&gt;imx-ipuv3 2800000.ipu: IPU DMFC Regs = c08c6000&lt;BR /&gt;imx-ipuv3 2800000.ipu: IPU DI0 Regs = c08ce000&lt;BR /&gt;imx-ipuv3 2800000.ipu: IPU DI1 Regs = c08d6000&lt;BR /&gt;imx-ipuv3 2800000.ipu: IPU SMFC Regs = c08d8000&lt;BR /&gt;imx-ipuv3 2800000.ipu: IPU CSI0 Regs = c08da000&lt;BR /&gt;imx-ipuv3 2800000.ipu: IPU CSI1 Regs = c08dc000&lt;BR /&gt;imx-ipuv3 2800000.ipu: IPU CPMem = c0980000&lt;BR /&gt;imx-ipuv3 2800000.ipu: IPU TPMem = c09c0000&lt;BR /&gt;imx-ipuv3 2800000.ipu: IPU DC Template Mem = c0a00000&lt;BR /&gt;imx-ipuv3 2800000.ipu: IPU Display Region 1 Mem = c08f2000&lt;BR /&gt;imx-ipuv3 2800000.ipu: IPU VDI Regs = c08de000&lt;BR /&gt;imx-ipuv3 2800000.ipu: IPU DMFC NORMAL mode: 1(0~1), 5B(4,5), 5F(6,7)&lt;BR /&gt;imx-ipuv3 2800000.ipu: ipu_clk = 264000000&lt;BR /&gt;mxc_mipi_csi2 21dc000.mipi_csi: i.MX MIPI CSI2 driver probed&lt;BR /&gt;mxc_mipi_csi2 21dc000.mipi_csi: i.MX MIPI CSI2 dphy version is 0x3130302a&lt;BR /&gt;MIPI CSI2 driver module loaded&lt;BR /&gt;Advanced Linux Sound Architecture Driver Initialized.&lt;BR /&gt;Bluetooth: Core ver 2.16&lt;BR /&gt;NET: Registered protocol family 31&lt;BR /&gt;Bluetooth: HCI device and connection manager initialized&lt;BR /&gt;Bluetooth: HCI socket layer initialized&lt;BR /&gt;Bluetooth: L2CAP socket layer initialized&lt;BR /&gt;Bluetooth: SCO socket layer initialized&lt;BR /&gt;cfg80211: Calling CRDA to update world regulatory domain&lt;BR /&gt;pureg-dummy: no parameters&lt;BR /&gt;Switching to clocksource mxc_timer1&lt;BR /&gt;NET: Registered protocol family 2&lt;BR /&gt;TCP established hash table entries: 8192 (order: 4, 65536 bytes)&lt;BR /&gt;TCP bind hash table entries: 8192 (order: 4, 65536 bytes)&lt;BR /&gt;TCP: Hash tables configured (established 8192 bind 8192)&lt;BR /&gt;TCP: reno registered&lt;BR /&gt;UDP hash table entries: 512 (order: 2, 16384 bytes)&lt;BR /&gt;UDP-Lite hash table entries: 512 (order: 2, 16384 bytes)&lt;BR /&gt;NET: Registered protocol family 1&lt;BR /&gt;RPC: Registered named UNIX socket transport module.&lt;BR /&gt;RPC: Registered udp transport module.&lt;BR /&gt;RPC: Registered tcp transport module.&lt;BR /&gt;RPC: Registered tcp NFSv4.1 backchannel transport module.&lt;BR /&gt;hw perfevents: enabled with ARMv7 Cortex-A9 PMU driver, 7 counters available&lt;BR /&gt;imx6_busfreq busfreq.16: DDR medium rate not supported.&lt;BR /&gt;Bus freq driver module loaded&lt;BR /&gt;futex hash table entries: 1024 (order: 4, 65536 bytes)&lt;BR /&gt;VFS: Disk quotas dquot_6.5.2&lt;BR /&gt;Dquot-cache hash table entries: 1024 (order 0, 4096 bytes)&lt;BR /&gt;NFS: Registering the id_resolver key type&lt;BR /&gt;Key type id_resolver registered&lt;BR /&gt;Key type id_legacy registered&lt;BR /&gt;jffs2: version 2.2. (NAND) © 2001-2006 Red Hat, Inc.&lt;BR /&gt;fuse init (API version 7.22)&lt;BR /&gt;msgmni has been set to 2001&lt;BR /&gt;io scheduler noop registered&lt;BR /&gt;io scheduler deadline registered&lt;BR /&gt;io scheduler cfq registered (default)&lt;BR /&gt;imx-weim 21b8000.weim: WEIM driver registered.&lt;BR /&gt;imx6q-pinctrl 20e0000.iomuxc: pin MX6Q_PAD_SD1_DAT3 already requested by 20e0000.iomuxc; cannot claim for 2080000.pwm&lt;BR /&gt;imx6q-pinctrl 20e0000.iomuxc: pin-209 (2080000.pwm) status -22&lt;BR /&gt;imx6q-pinctrl 20e0000.iomuxc: could not request pin 209 on device 20e0000.iomuxc&lt;BR /&gt;imx-pwm 2080000.pwm: Error applying setting, reverse things back&lt;BR /&gt;MIPI DSI driver module loaded&lt;BR /&gt;mxc_sdc_fb fb.27: mxcfb_probe enter&lt;BR /&gt;mxc_sdc_fb fb.27: di_pixfmt:0x33424752, bpp:0x18, di:0, ipu:1&lt;BR /&gt;mxc_sdc_fb fb.27: registered mxc display driver ldb&lt;BR /&gt;mxc_sdc_fb fb.27: Reconfiguring framebuffer&lt;BR /&gt;imx-ipuv3 2800000.ipu: Channel already disabled 9&lt;BR /&gt;imx-ipuv3 2800000.ipu: Channel already uninitialized 9&lt;BR /&gt;mxc_sdc_fb fb.27: allocated fb @ paddr=0x3C100000, size=1572864.&lt;BR /&gt;imx-ipuv3 2800000.ipu: init channel = 9&lt;BR /&gt;imx-ipuv3 2800000.ipu: ipu busfreq high requst.&lt;BR /&gt;mxc_sdc_fb fb.27: pixclock = 65002000l Hz&lt;BR /&gt;mxc_sdc_fb fb.27: 1024x768 h_sync,r,l: 60,40,220 v_sync,l,u: 10,7,21 pixclock=65002000 Hz&lt;BR /&gt;imx-ipuv3 2800000.ipu: panel size = 1024 x 768&lt;BR /&gt;imx-ipuv3 2800000.ipu: pixel clk = 65002000&lt;BR /&gt;imx-ipuv3 2800000.ipu: use special clk parent&lt;BR /&gt;imx-ipuv3 2800000.ipu: round pixel clk:64653061&lt;BR /&gt;imx-ipuv3 2800000.ipu: disp=0, pixel_clk=65002000 64653061 parent=64653061 div=1&lt;BR /&gt;mxc_sdc_fb fb.27: Y wrap disabled&lt;BR /&gt;imx-ipuv3 2800000.ipu: initializing idma ch 23 @ c09805c0&lt;BR /&gt;imx-ipuv3 2800000.ipu: initializing idma ch 23 @ c0981140 sub cpmem&lt;BR /&gt;imx-ipuv3 2800000.ipu: IPU DMFC DP HIGH RESOLUTION: 1(0,1), 5B(2~5), 5F(6,7)&lt;BR /&gt;imx-ipuv3 2800000.ipu: ch 23 word 0 - 00000000 00000000 00000000 E0001800 000BFC7F&lt;BR /&gt;imx-ipuv3 2800000.ipu: ch 23 word 1 - 07820000 00F04000 00E7C000 F2C1FFC0 00082CA0&lt;BR /&gt;imx-ipuv3 2800000.ipu: PFS 0x7, &lt;BR /&gt;imx-ipuv3 2800000.ipu: BPP 0x3, &lt;BR /&gt;imx-ipuv3 2800000.ipu: NPB 0x1f&lt;BR /&gt;imx-ipuv3 2800000.ipu: FW 1023, &lt;BR /&gt;imx-ipuv3 2800000.ipu: FH 767, &lt;BR /&gt;imx-ipuv3 2800000.ipu: EBA0 0x3c100000&lt;BR /&gt;imx-ipuv3 2800000.ipu: EBA1 0x3c100000&lt;BR /&gt;imx-ipuv3 2800000.ipu: Stride 2047&lt;BR /&gt;imx-ipuv3 2800000.ipu: scan_order 0&lt;BR /&gt;imx-ipuv3 2800000.ipu: uv_stride 11424&lt;BR /&gt;imx-ipuv3 2800000.ipu: u_offset 0x0&lt;BR /&gt;imx-ipuv3 2800000.ipu: v_offset 0x0&lt;BR /&gt;imx-ipuv3 2800000.ipu: Width0 4+1, &lt;BR /&gt;imx-ipuv3 2800000.ipu: Width1 5+1, &lt;BR /&gt;imx-ipuv3 2800000.ipu: Width2 4+1, &lt;BR /&gt;imx-ipuv3 2800000.ipu: Width3 7+1, &lt;BR /&gt;imx-ipuv3 2800000.ipu: Offset0 0, &lt;BR /&gt;imx-ipuv3 2800000.ipu: Offset1 5, &lt;BR /&gt;imx-ipuv3 2800000.ipu: Offset2 11, &lt;BR /&gt;imx-ipuv3 2800000.ipu: Offset3 16&lt;BR /&gt;mxc_sdc_fb fb.27: Y wrap disabled&lt;BR /&gt;mxc_sdc_fb fb.27: Updating SDC DISP4 BG buf 0 address=0x3C100000&lt;BR /&gt;mxc_sdc_fb fb.27: Update complete&lt;BR /&gt;mxc_sdc_fb fb.27: blank = 0&lt;BR /&gt;mxc_sdc_fb fb.27: Reconfiguring framebuffer&lt;BR /&gt;imx-ipuv3 2800000.ipu: DC stop timeout - 3 * 10ms&lt;BR /&gt;imx-ipuv3 2800000.ipu: ipu busfreq high release.&lt;BR /&gt;imx-ipuv3 2800000.ipu: init channel = 9&lt;BR /&gt;imx-ipuv3 2800000.ipu: ipu busfreq high requst.&lt;BR /&gt;mxc_sdc_fb fb.27: pixclock = 65002000l Hz&lt;BR /&gt;mxc_sdc_fb fb.27: 1024x768 h_sync,r,l: 60,40,220 v_sync,l,u: 10,7,21 pixclock=65002000 Hz&lt;BR /&gt;imx-ipuv3 2800000.ipu: panel size = 1024 x 768&lt;BR /&gt;imx-ipuv3 2800000.ipu: pixel clk = 65002000&lt;BR /&gt;imx-ipuv3 2800000.ipu: use special clk parent&lt;BR /&gt;imx-ipuv3 2800000.ipu: round pixel clk:64653061&lt;BR /&gt;imx-ipuv3 2800000.ipu: disp=0, pixel_clk=65002000 64653061 parent=64653061 div=1&lt;BR /&gt;mxc_sdc_fb fb.27: Y wrap disabled&lt;BR /&gt;imx-ipuv3 2800000.ipu: initializing idma ch 23 @ c09805c0&lt;BR /&gt;imx-ipuv3 2800000.ipu: initializing idma ch 23 @ c0981140 sub cpmem&lt;BR /&gt;imx-ipuv3 2800000.ipu: DMFC high resolution has set, will not change&lt;BR /&gt;imx-ipuv3 2800000.ipu: ch 23 word 0 - 00000000 00000000 00000000 E0001800 000BFC7F&lt;BR /&gt;imx-ipuv3 2800000.ipu: ch 23 word 1 - 07820000 00F04000 00E7C000 F2C1FFC0 00082CA0&lt;BR /&gt;imx-ipuv3 2800000.ipu: PFS 0x7, &lt;BR /&gt;imx-ipuv3 2800000.ipu: BPP 0x3, &lt;BR /&gt;imx-ipuv3 2800000.ipu: NPB 0x1f&lt;BR /&gt;imx-ipuv3 2800000.ipu: FW 1023, &lt;BR /&gt;imx-ipuv3 2800000.ipu: FH 767, &lt;BR /&gt;imx-ipuv3 2800000.ipu: EBA0 0x3c100000&lt;BR /&gt;imx-ipuv3 2800000.ipu: EBA1 0x3c100000&lt;BR /&gt;imx-ipuv3 2800000.ipu: Stride 2047&lt;BR /&gt;imx-ipuv3 2800000.ipu: scan_order 0&lt;BR /&gt;imx-ipuv3 2800000.ipu: uv_stride 11424&lt;BR /&gt;imx-ipuv3 2800000.ipu: u_offset 0x0&lt;BR /&gt;imx-ipuv3 2800000.ipu: v_offset 0x0&lt;BR /&gt;imx-ipuv3 2800000.ipu: Width0 4+1, &lt;BR /&gt;imx-ipuv3 2800000.ipu: Width1 5+1, &lt;BR /&gt;imx-ipuv3 2800000.ipu: Width2 4+1, &lt;BR /&gt;imx-ipuv3 2800000.ipu: Width3 7+1, &lt;BR /&gt;imx-ipuv3 2800000.ipu: Offset0 0, &lt;BR /&gt;imx-ipuv3 2800000.ipu: Offset1 5, &lt;BR /&gt;imx-ipuv3 2800000.ipu: Offset2 11, &lt;BR /&gt;imx-ipuv3 2800000.ipu: Offset3 16&lt;BR /&gt;mxc_sdc_fb fb.27: Y wrap disabled&lt;BR /&gt;mxc_sdc_fb fb.27: Updating SDC DISP4 BG buf 0 address=0x3C100000&lt;BR /&gt;mxc_sdc_fb fb.27: Update complete&lt;BR /&gt;Console: switching to colour frame buffer device 128x48&lt;BR /&gt;mxc_sdc_fb fb.27: Y wrap disabled&lt;BR /&gt;mxc_sdc_fb fb.27: Updating SDC DISP4 BG buf 1 address=0x3C100000&lt;BR /&gt;mxc_sdc_fb fb.27: Update complete&lt;BR /&gt;mxc_sdc_fb fb.27: pixclock set for 60Hz refresh = 217013 ps&lt;BR /&gt;mxc_sdc_fb fb.27: Reconfiguring framebuffer&lt;BR /&gt;imx-ipuv3 2800000.ipu: Channel already disabled 10&lt;BR /&gt;imx-ipuv3 2800000.ipu: Channel already uninitialized 10&lt;BR /&gt;mxc_sdc_fb fb.27: allocated fb @ paddr=0x3C300000, size=691200.&lt;BR /&gt;mxc_sdc_fb fb.28: mxcfb_probe enter&lt;BR /&gt;mxc_hdmi 20e0000.hdmi_video: Detected HDMI controller 0x13:0xa:0xa0:0xc1&lt;BR /&gt;mxc_sdc_fb fb.28: di_pixfmt:0x33424752, bpp:0x18, di:0, ipu:0&lt;BR /&gt;mxc_sdc_fb fb.28: registered mxc display driver hdmi&lt;BR /&gt;mxc_sdc_fb fb.28: Reconfiguring framebuffer&lt;BR /&gt;imx-ipuv3 2400000.ipu: Channel already disabled 9&lt;BR /&gt;imx-ipuv3 2400000.ipu: Channel already uninitialized 9&lt;BR /&gt;mxc_sdc_fb fb.28: allocated fb @ paddr=0x3C400000, size=6220800.&lt;BR /&gt;imx-ipuv3 2400000.ipu: init channel = 9&lt;BR /&gt;imx-ipuv3 2400000.ipu: ipu busfreq high requst.&lt;BR /&gt;mxc_sdc_fb fb.28: pixclock = 148500000l Hz&lt;BR /&gt;mxc_sdc_fb fb.28: 1920x1080 h_sync,r,l: 44,88,148 v_sync,l,u: 5,4,36 pixclock=148500000 Hz&lt;BR /&gt;imx-ipuv3 2400000.ipu: panel size = 1920 x 1080&lt;BR /&gt;imx-ipuv3 2400000.ipu: pixel clk = 148500000&lt;BR /&gt;imx-ipuv3 2400000.ipu: try ipu internal clk&lt;BR /&gt;imx-ipuv3 2400000.ipu: rounded pix clk:176000000&lt;BR /&gt;imx-ipuv3 2400000.ipu: try ipu ext di clk&lt;BR /&gt;imx-ipuv3 2400000.ipu: di clk:148500000&lt;BR /&gt;imx-ipuv3 2400000.ipu: round pixel clk:148500000&lt;BR /&gt;imx-ipuv3 2400000.ipu: disp=0, pixel_clk=148500000 148500000 parent=148500000 div=1&lt;BR /&gt;mxc_sdc_fb fb.28: Y wrap disabled&lt;BR /&gt;imx-ipuv3 2400000.ipu: initializing idma ch 23 @ c09005c0&lt;BR /&gt;imx-ipuv3 2400000.ipu: initializing idma ch 23 @ c0901140 sub cpmem&lt;BR /&gt;imx-ipuv3 2400000.ipu: DMFC high resolution has set, will not change&lt;BR /&gt;imx-ipuv3 2400000.ipu: ch 23 word 0 - 00000000 00000000 00000000 E0000800 0010DCEF&lt;BR /&gt;imx-ipuv3 2400000.ipu: ch 23 word 1 - 07880000 00F10000 00E4C000 FFF59FC0 000C4100&lt;BR /&gt;imx-ipuv3 2400000.ipu: PFS 0x7, &lt;BR /&gt;imx-ipuv3 2400000.ipu: BPP 0x1, &lt;BR /&gt;imx-ipuv3 2400000.ipu: NPB 0x13&lt;BR /&gt;imx-ipuv3 2400000.ipu: FW 1919, &lt;BR /&gt;imx-ipuv3 2400000.ipu: FH 1079, &lt;BR /&gt;imx-ipuv3 2400000.ipu: EBA0 0x3c400000&lt;BR /&gt;imx-ipuv3 2400000.ipu: EBA1 0x3c400000&lt;BR /&gt;imx-ipuv3 2400000.ipu: Stride 5759&lt;BR /&gt;imx-ipuv3 2400000.ipu: scan_order 0&lt;BR /&gt;imx-ipuv3 2400000.ipu: uv_stride 256&lt;BR /&gt;imx-ipuv3 2400000.ipu: u_offset 0x0&lt;BR /&gt;imx-ipuv3 2400000.ipu: v_offset 0x0&lt;BR /&gt;imx-ipuv3 2400000.ipu: Width0 7+1, &lt;BR /&gt;imx-ipuv3 2400000.ipu: Width1 7+1, &lt;BR /&gt;imx-ipuv3 2400000.ipu: Width2 7+1, &lt;BR /&gt;imx-ipuv3 2400000.ipu: Width3 7+1, &lt;BR /&gt;imx-ipuv3 2400000.ipu: Offset0 0, &lt;BR /&gt;imx-ipuv3 2400000.ipu: Offset1 8, &lt;BR /&gt;imx-ipuv3 2400000.ipu: Offset2 16, &lt;BR /&gt;imx-ipuv3 2400000.ipu: Offset3 24&lt;BR /&gt;mxc_sdc_fb fb.28: Y wrap disabled&lt;BR /&gt;mxc_sdc_fb fb.28: Updating SDC DISP3 BG buf 0 address=0x3C400000&lt;BR /&gt;mxc_sdc_fb fb.28: Update complete&lt;BR /&gt;mxc_sdc_fb fb.28: blank = 0&lt;BR /&gt;mxc_sdc_fb fb.28: pixclock set for 60Hz refresh = 217013 ps&lt;BR /&gt;mxc_sdc_fb fb.28: Reconfiguring framebuffer&lt;BR /&gt;imx-ipuv3 2400000.ipu: Channel already disabled 10&lt;BR /&gt;imx-ipuv3 2400000.ipu: Channel already uninitialized 10&lt;BR /&gt;mxc_sdc_fb fb.28: allocated fb @ paddr=0x3CA00000, size=691200.&lt;BR /&gt;mxc_sdc_fb fb.29: mxcfb_probe enter&lt;BR /&gt;mxc_sdc_fb fb.29: NO mxc display driver found!&lt;BR /&gt;mxc_sdc_fb fb.30: mxcfb_probe enter&lt;BR /&gt;mxc_sdc_fb fb.30: get of property mode_str fail&lt;BR /&gt;mxc_sdc_fb fb.30: di_pixfmt:0x36424752, bpp:0x10, di:1, ipu:1&lt;BR /&gt;mxc_sdc_fb fb.30: registered mxc display driver ldb&lt;BR /&gt;mxc_sdc_fb fb.30: Reconfiguring framebuffer&lt;BR /&gt;imx-ipuv3 2800000.ipu: Channel already disabled 7&lt;BR /&gt;imx-ipuv3 2800000.ipu: Channel already uninitialized 7&lt;BR /&gt;mxc_sdc_fb fb.30: allocated fb @ paddr=0x3CB00000, size=1572864.&lt;BR /&gt;imx-ipuv3 2800000.ipu: init channel = 7&lt;BR /&gt;mxc_sdc_fb fb.30: pixclock = 65002000l Hz&lt;BR /&gt;mxc_sdc_fb fb.30: 1024x768 h_sync,r,l: 60,40,220 v_sync,l,u: 10,7,21 pixclock=65002000 Hz&lt;BR /&gt;imx-ipuv3 2800000.ipu: panel size = 1024 x 768&lt;BR /&gt;imx-ipuv3 2800000.ipu: pixel clk = 65002000&lt;BR /&gt;imx-ipuv3 2800000.ipu: use special clk parent&lt;BR /&gt;imx-ipuv3 2800000.ipu: round pixel clk:64653061&lt;BR /&gt;imx-ipuv3 2800000.ipu: disp=1, pixel_clk=65002000 64653061 parent=64653061 div=1&lt;BR /&gt;mxc_sdc_fb fb.30: Y wrap disabled&lt;BR /&gt;imx-ipuv3 2800000.ipu: initializing idma ch 28 @ c0980700&lt;BR /&gt;imx-ipuv3 2800000.ipu: initializing idma ch 28 @ c09811c0 sub cpmem&lt;BR /&gt;imx-ipuv3 2800000.ipu: DMFC high resolution has set, will not change&lt;BR /&gt;imx-ipuv3 2800000.ipu: ch 28 word 0 - 00000000 00000000 00000000 E0001800 000BFC7F&lt;BR /&gt;imx-ipuv3 2800000.ipu: ch 28 word 1 - 07960000 00F2C000 00E7C000 F2C1FFC0 00082CA0&lt;BR /&gt;imx-ipuv3 2800000.ipu: PFS 0x7, &lt;BR /&gt;imx-ipuv3 2800000.ipu: BPP 0x3, &lt;BR /&gt;imx-ipuv3 2800000.ipu: NPB 0x1f&lt;BR /&gt;imx-ipuv3 2800000.ipu: FW 1023, &lt;BR /&gt;imx-ipuv3 2800000.ipu: FH 767, &lt;BR /&gt;imx-ipuv3 2800000.ipu: EBA0 0x3cb00000&lt;BR /&gt;imx-ipuv3 2800000.ipu: EBA1 0x3cb00000&lt;BR /&gt;imx-ipuv3 2800000.ipu: Stride 2047&lt;BR /&gt;imx-ipuv3 2800000.ipu: scan_order 0&lt;BR /&gt;imx-ipuv3 2800000.ipu: uv_stride 11424&lt;BR /&gt;imx-ipuv3 2800000.ipu: u_offset 0x0&lt;BR /&gt;imx-ipuv3 2800000.ipu: v_offset 0x0&lt;BR /&gt;imx-ipuv3 2800000.ipu: Width0 4+1, &lt;BR /&gt;imx-ipuv3 2800000.ipu: Width1 5+1, &lt;BR /&gt;imx-ipuv3 2800000.ipu: Width2 4+1, &lt;BR /&gt;imx-ipuv3 2800000.ipu: Width3 7+1, &lt;BR /&gt;imx-ipuv3 2800000.ipu: Offset0 0, &lt;BR /&gt;imx-ipuv3 2800000.ipu: Offset1 5, &lt;BR /&gt;imx-ipuv3 2800000.ipu: Offset2 11, &lt;BR /&gt;imx-ipuv3 2800000.ipu: Offset3 16&lt;BR /&gt;mxc_sdc_fb fb.30: Y wrap disabled&lt;BR /&gt;mxc_sdc_fb fb.30: Updating SDC DISP4 BG - DI1 buf 0 address=0x3CB00000&lt;BR /&gt;mxc_sdc_fb fb.30: Update complete&lt;BR /&gt;mxc_sdc_fb fb.30: blank = 0&lt;BR /&gt;imx-sdma 20ec000.sdma: no iram assigned, using external mem&lt;BR /&gt;imx-sdma 20ec000.sdma: loaded firmware 1.1&lt;BR /&gt;imx-sdma 20ec000.sdma: initialized&lt;BR /&gt;mxc_sdc_fb fb.28: Reconfiguring framebuffer&lt;BR /&gt;pfuze100-regulator 1-0008: Full lay: 2, Metal lay: 1&lt;BR /&gt;pfuze100-regulator 1-0008: FAB: 0, FIN: 0&lt;BR /&gt;pfuze100-regulator 1-0008: pfuze100 found.&lt;BR /&gt;SW1AB: 300 &amp;lt;--&amp;gt; 1875 mV at 1150 mV &lt;BR /&gt;SW1C: 300 &amp;lt;--&amp;gt; 1875 mV at 1175 mV &lt;BR /&gt;SW2: 800 &amp;lt;--&amp;gt; 3300 mV at 3300 mV &lt;BR /&gt;SW3A: 400 &amp;lt;--&amp;gt; 1975 mV at 1500 mV &lt;BR /&gt;SW3B: 400 &amp;lt;--&amp;gt; 1975 mV at 1500 mV &lt;BR /&gt;SW4: 800 &amp;lt;--&amp;gt; 3300 mV at 3150 mV &lt;BR /&gt;SWBST: 5000 &amp;lt;--&amp;gt; 5150 mV at 5000 mV &lt;BR /&gt;VSNVS: 1000 &amp;lt;--&amp;gt; 3000 mV at 3000 mV &lt;BR /&gt;VREFDDR: 750 mV &lt;BR /&gt;imx-ipuv3 2400000.ipu: DC stop timeout - 1 * 10ms&lt;BR /&gt;imx-ipuv3 2400000.ipu: ipu busfreq high release.&lt;BR /&gt;imx-ipuv3 2400000.ipu: init channel = 9&lt;BR /&gt;imx-ipuv3 2400000.ipu: ipu busfreq high requst.&lt;BR /&gt;mxc_sdc_fb fb.28: pixclock = 25175000l Hz&lt;BR /&gt;mxc_sdc_fb fb.28: 640x480 h_sync,r,l: 96,16,48 v_sync,l,u: 2,10,33 pixclock=25175000 Hz&lt;BR /&gt;imx-ipuv3 2400000.ipu: panel size = 640 x 480&lt;BR /&gt;imx-ipuv3 2400000.ipu: pixel clk = 25175000&lt;BR /&gt;imx-ipuv3 2400000.ipu: try ipu internal clk&lt;BR /&gt;imx-ipuv3 2400000.ipu: rounded pix clk:25142857&lt;BR /&gt;imx-ipuv3 2400000.ipu: round pixel clk:25142857&lt;BR /&gt;VGEN1: 800 &amp;lt;--&amp;gt; 1550 mV at 1500 mV &lt;BR /&gt;VGEN2: 800 &amp;lt;--&amp;gt; 1550 mV at 1500 mV &lt;BR /&gt;VGEN3: 1800 &amp;lt;--&amp;gt; 3300 mV at 2800 mV &lt;BR /&gt;VGEN4: 1800 &amp;lt;--&amp;gt; 3300 mV at 1800 mV &lt;BR /&gt;VGEN5: 1800 &amp;lt;--&amp;gt; 3300 mV at 3000 mV &lt;BR /&gt;VGEN6: 1800 &amp;lt;--&amp;gt; 3300 mV at 3300 mV &lt;BR /&gt;Serial: IMX driver&lt;BR /&gt;2020000.serial: ttymxc0 at MMIO 0x2020000 (irq = 58) is a IMX&lt;BR /&gt;imx-ipuv3 2400000.ipu: disp=0, pixel_clk=25175000 25142857 parent=264000000 div=10&lt;BR /&gt;mxc_sdc_fb fb.28: Y wrap disabled&lt;BR /&gt;imx-ipuv3 2400000.ipu: initializing idma ch 23 @ c09005c0&lt;BR /&gt;imx-ipuv3 2400000.ipu: initializing idma ch 23 @ c0901140 sub cpmem&lt;BR /&gt;imx-ipuv3 2400000.ipu: ch 23 word 0 - 00000000 00000000 00000000 E0000800 00077C4F&lt;BR /&gt;imx-ipuv3 2400000.ipu: ch 23 word 1 - 07880000 00F10000 00E4C000 FFF1DFC0 000C4100&lt;BR /&gt;imx-ipuv3 2400000.ipu: PFS 0x7, &lt;BR /&gt;imx-ipuv3 2400000.ipu: BPP 0x1, &lt;BR /&gt;imx-ipuv3 2400000.ipu: NPB 0x13&lt;BR /&gt;imx-ipuv3 2400000.ipu: FW 639, &lt;BR /&gt;imx-ipuv3 2400000.ipu: FH 479, &lt;BR /&gt;imx-ipuv3 2400000.ipu: EBA0 0x3c400000&lt;BR /&gt;imx-ipuv3 2400000.ipu: EBA1 0x3c400000&lt;BR /&gt;imx-ipuv3 2400000.ipu: Stride 1919&lt;BR /&gt;imx-ipuv3 2400000.ipu: scan_order 0&lt;BR /&gt;imx-ipuv3 2400000.ipu: uv_stride 256&lt;BR /&gt;imx-ipuv3 2400000.ipu: u_offset 0x0&lt;BR /&gt;imx-ipuv3 2400000.ipu: v_offset 0x0&lt;BR /&gt;imx-ipuv3 2400000.ipu: Width0 7+1, &lt;BR /&gt;imx-ipuv3 2400000.ipu: Width1 7+1, &lt;BR /&gt;imx-ipuv3 2400000.ipu: Width2 7+1, &lt;BR /&gt;imx-ipuv3 2400000.ipu: Width3 7+1, &lt;BR /&gt;imx-ipuv3 2400000.ipu: Offset0 0, &lt;BR /&gt;imx-ipuv3 2400000.ipu: Offset1 8, &lt;BR /&gt;imx-ipuv3 2400000.ipu: Offset2 16, &lt;BR /&gt;imx-ipuv3 2400000.ipu: Offset3 24&lt;BR /&gt;mxc_sdc_fb fb.28: Y wrap disabled&lt;BR /&gt;mxc_sdc_fb fb.28: Updating SDC DISP3 BG buf 0 address=0x3C400000&lt;BR /&gt;mxc_sdc_fb fb.28: Update complete&lt;BR /&gt;mxc_sdc_fb fb.28: Reconfiguring framebuffer&lt;BR /&gt;console [ttymxc0] enabled&lt;BR /&gt;21e8000.serial: ttymxc1 at MMIO 0x21e8000 (irq = 59) is a IMX&lt;BR /&gt;21ec000.serial: ttymxc2 at MMIO 0x21ec000 (irq = 60) is a IMX&lt;BR /&gt;serial: Freescale lpuart driver&lt;BR /&gt;imx sema4 driver is registered.&lt;BR /&gt;[drm] Initialized drm 1.1.0 20060810&lt;BR /&gt;[drm] Initialized vivante 1.0.0 20120216 on minor 0&lt;BR /&gt;brd: module loaded&lt;BR /&gt;loop: module loaded&lt;BR /&gt;imx-ipuv3 2400000.ipu: DC stop timeout - 2 * 10ms&lt;BR /&gt;imx-ipuv3 2400000.ipu: ipu busfreq high release.&lt;BR /&gt;imx-ipuv3 2400000.ipu: init channel = 9&lt;BR /&gt;imx-ipuv3 2400000.ipu: ipu busfreq high requst.&lt;BR /&gt;mxc_sdc_fb fb.28: pixclock = 148500000l Hz&lt;BR /&gt;mxc_sdc_fb fb.28: 1920x1080 h_sync,r,l: 44,88,148 v_sync,l,u: 5,4,36 pixclock=148500000 Hz&lt;BR /&gt;imx-ipuv3 2400000.ipu: panel size = 1920 x 1080&lt;BR /&gt;imx-ipuv3 2400000.ipu: pixel clk = 148500000&lt;BR /&gt;imx-ipuv3 2400000.ipu: try ipu internal clk&lt;BR /&gt;imx-ipuv3 2400000.ipu: rounded pix clk:176000000&lt;BR /&gt;imx-ipuv3 2400000.ipu: try ipu ext di clk&lt;BR /&gt;imx-ipuv3 2400000.ipu: di clk:148500000&lt;BR /&gt;imx-ipuv3 2400000.ipu: round pixel clk:148500000&lt;BR /&gt;m25p80 spi32766.0: s25fl128s (16384 Kbytes)&lt;BR /&gt;spi_imx 200c000.ecspi: probed&lt;BR /&gt;CAN device driver interface&lt;BR /&gt;/soc/aips-bus@02100000/ethernet@02188000: could not find phy node&lt;BR /&gt;fec 2188000.ethernet (unregistered net_device): Invalid MAC address: 00:00:00:00:00:00&lt;BR /&gt;fec 2188000.ethernet (unregistered net_device): Using random MAC address: 62:cc:8f:ff:a8:03&lt;BR /&gt;libphy: fec_enet_mii_bus: probed&lt;BR /&gt;ehci_hcd: USB 2.0 'Enhanced' Host Controller (EHCI) Driver&lt;BR /&gt;usbcore: registered new interface driver usb-storage&lt;BR /&gt;setup_reset_gpios:-2, flags 0&lt;BR /&gt;setup_reset_gpios:-2, flags 0&lt;BR /&gt;imx-ipuv3 2400000.ipu: disp=0, pixel_clk=148500000 148500000 parent=148500000 div=1&lt;BR /&gt;mxc_sdc_fb fb.28: Y wrap disabled&lt;BR /&gt;imx-ipuv3 2400000.ipu: initializing idma ch 23 @ c09005c0&lt;BR /&gt;imx-ipuv3 2400000.ipu: initializing idma ch 23 @ c0901140 sub cpmem&lt;BR /&gt;imx-ipuv3 2400000.ipu: DMFC high resolution has set, will not change&lt;BR /&gt;imx-ipuv3 2400000.ipu: ch 23 word 0 - 00000000 00000000 00000000 E0000800 0010DCEF&lt;BR /&gt;imx-ipuv3 2400000.ipu: ch 23 word 1 - 07880000 00F10000 00E4C000 FFF59FC0 000C4100&lt;BR /&gt;imx-ipuv3 2400000.ipu: PFS 0x7, &lt;BR /&gt;imx-ipuv3 2400000.ipu: BPP 0x1, &lt;BR /&gt;imx-ipuv3 2400000.ipu: NPB 0x13&lt;BR /&gt;imx-ipuv3 2400000.ipu: FW 1919, &lt;BR /&gt;imx-ipuv3 2400000.ipu: FH 1079, &lt;BR /&gt;imx-ipuv3 2400000.ipu: EBA0 0x3c400000&lt;BR /&gt;imx-ipuv3 2400000.ipu: EBA1 0x3c400000&lt;BR /&gt;imx-ipuv3 2400000.ipu: Stride 5759&lt;BR /&gt;imx-ipuv3 2400000.ipu: scan_order 0&lt;BR /&gt;imx-ipuv3 2400000.ipu: uv_stride 256&lt;BR /&gt;imx-ipuv3 2400000.ipu: u_offset 0x0&lt;BR /&gt;imx-ipuv3 2400000.ipu: v_offset 0x0&lt;BR /&gt;imx-ipuv3 2400000.ipu: Width0 7+1, &lt;BR /&gt;imx-ipuv3 2400000.ipu: Width1 7+1, &lt;BR /&gt;imx-ipuv3 2400000.ipu: Width2 7+1, &lt;BR /&gt;imx-ipuv3 2400000.ipu: Width3 7+1, &lt;BR /&gt;imx-ipuv3 2400000.ipu: Offset0 0, &lt;BR /&gt;imx-ipuv3 2400000.ipu: Offset1 8, &lt;BR /&gt;imx-ipuv3 2400000.ipu: Offset2 16, &lt;BR /&gt;imx-ipuv3 2400000.ipu: Offset3 24&lt;BR /&gt;ci_hdrc ci_hdrc.1: doesn't support gadget&lt;BR /&gt;ci_hdrc ci_hdrc.1: EHCI Host Controller&lt;BR /&gt;ci_hdrc ci_hdrc.1: new USB bus registered, assigned bus number 1&lt;BR /&gt;mxc_sdc_fb fb.28: Y wrap disabled&lt;BR /&gt;mxc_sdc_fb fb.28: Updating SDC DISP3 BG buf 0 address=0x3C400000&lt;BR /&gt;mxc_sdc_fb fb.28: Update complete&lt;BR /&gt;ci_hdrc ci_hdrc.1: USB 2.0 started, EHCI 1.00&lt;BR /&gt;hub 1-0:1.0: USB hub found&lt;BR /&gt;hub 1-0:1.0: 1 port detected&lt;BR /&gt;mousedev: PS/2 mouse device common for all mice&lt;BR /&gt;i2c-core: driver [isl29023] using legacy suspend method&lt;BR /&gt;i2c-core: driver [isl29023] using legacy resume method&lt;BR /&gt;check_alarm_past: alarm in the past&lt;BR /&gt;snvs_rtc 20cc034.snvs-rtc-lp: rtc core: registered 20cc034.snvs-rtc-lp as rtc0&lt;BR /&gt;i2c /dev entries driver&lt;BR /&gt;mxc_v4l2_output v4l2_out.32: V4L2 device registered as video16&lt;BR /&gt;mxc_v4l2_output v4l2_out.32: V4L2 device registered as video17&lt;BR /&gt;mxc_v4l2_output v4l2_out.32: V4L2 device registered as video18&lt;BR /&gt;mxc_v4l2_output v4l2_out.32: V4L2 device registered as video19&lt;BR /&gt;mxc_v4l2_output v4l2_out.32: V4L2 device registered as video20&lt;BR /&gt;i2c-core: driver [mag3110] using legacy suspend method&lt;BR /&gt;i2c-core: driver [mag3110] using legacy resume method&lt;BR /&gt;imx2-wdt 20c0000.wdog: IMX2+ Watchdog Timer enabled. timeout=60s (nowayout=0)&lt;BR /&gt;Bluetooth: HCI UART driver ver 2.2&lt;BR /&gt;Bluetooth: HCI H4 protocol initialized&lt;BR /&gt;Bluetooth: HCI BCSP protocol initialized&lt;BR /&gt;Bluetooth: HCIATH3K protocol initialized&lt;BR /&gt;usbcore: registered new interface driver bcm203x&lt;BR /&gt;usbcore: registered new interface driver btusb&lt;BR /&gt;Bluetooth: Generic Bluetooth SDIO driver ver 0.1&lt;BR /&gt;usbcore: registered new interface driver ath3k&lt;BR /&gt;cpuidle: using governor ladder&lt;BR /&gt;cpuidle: using governor menu&lt;BR /&gt;sdhci: Secure Digital Host Controller Interface driver&lt;BR /&gt;sdhci: Copyright(c) Pierre Ossman&lt;BR /&gt;sdhci-pltfm: SDHCI platform and OF driver helper&lt;BR /&gt;sdhci-esdhc-imx 2198000.usdhc: sdhci_esdhc_imx_probe_dt: power-gpio -2&lt;BR /&gt;mmc2: no vqmmc regulator found&lt;BR /&gt;mmc2: no vmmc regulator found&lt;BR /&gt;mmc2: SDHCI controller on 2198000.usdhc [2198000.usdhc] using ADMA&lt;BR /&gt;sdhci-esdhc-imx 219c000.usdhc: sdhci_esdhc_imx_probe_dt: power-gpio -2&lt;BR /&gt;mmc3: no vqmmc regulator found&lt;BR /&gt;mmc3: no vmmc regulator found&lt;BR /&gt;mmc3: SDHCI controller on 219c000.usdhc [219c000.usdhc] using ADMA&lt;BR /&gt;Galcore version 5.0.11.25762&lt;BR /&gt;mmc3: BKOPS_EN bit is not set&lt;BR /&gt;mmc3: new high speed DDR MMC card at address 0001&lt;BR /&gt;mmcblk3: mmc3:0001 MMC08G 7.26 GiB &lt;BR /&gt;mmcblk3boot0: mmc3:0001 MMC08G partition 1 16.0 MiB&lt;BR /&gt;mmcblk3boot1: mmc3:0001 MMC08G partition 2 16.0 MiB&lt;BR /&gt;mmcblk3rpmb: mmc3:0001 MMC08G partition 3 128 KiB&lt;BR /&gt; mmcblk3: p1 p2&lt;BR /&gt; mmcblk3boot1: unknown partition table&lt;BR /&gt; mmcblk3boot0: unknown partition table&lt;BR /&gt;mxc_vdoa 21e4000.vdoa: i.MX Video Data Order Adapter(VDOA) driver probed&lt;BR /&gt;mxc_asrc 2034000.asrc: mxc_asrc registered&lt;BR /&gt;mxc_vpu 2040000.vpu: VPU initialized&lt;BR /&gt;leds-gpio leds.19: pins are not configured from the driver&lt;BR /&gt;caam 2100000.caam: Instantiated RNG4 SH0&lt;BR /&gt;ci_hdrc ci_hdrc.0: role 1 to 0&lt;BR /&gt;ci_hdrc ci_hdrc.0: EHCI Host Controller&lt;BR /&gt;ci_hdrc ci_hdrc.0: new USB bus registered, assigned bus number 2&lt;BR /&gt;ci_hdrc ci_hdrc.0: USB 2.0 started, EHCI 1.00&lt;BR /&gt;hub 2-0:1.0: USB hub found&lt;BR /&gt;hub 2-0:1.0: 1 port detected&lt;BR /&gt;caam 2100000.caam: Instantiated RNG4 SH1&lt;BR /&gt;caam 2100000.caam: device ID = 0x0a160100 (Era 4)&lt;BR /&gt;caam 2100000.caam: job rings = 2, qi = 0&lt;BR /&gt;caam algorithms registered in /proc/crypto&lt;BR /&gt;caam_jr 2101000.jr0: registering rng-caam&lt;BR /&gt;platform caam_sm: blkkey_ex: 4 keystore units available&lt;BR /&gt;platform caam_sm: 64-bit clear key:&lt;BR /&gt;platform caam_sm: [0000] 00 01 02 03 04 0f 06 07&lt;BR /&gt;platform caam_sm: 64-bit black key:&lt;BR /&gt;platform caam_sm: [0000] fd ac ec 48 a1 36 f9 01&lt;BR /&gt;platform caam_sm: [0008] 57 36 7d d4 9f 2d 1d 95&lt;BR /&gt;platform caam_sm: 128-bit clear key:&lt;BR /&gt;platform caam_sm: [0000] 00 01 02 03 04 0f 06 07&lt;BR /&gt;platform caam_sm: [0008] 08 09 0a 0b 0c 0d 0e 0f&lt;BR /&gt;platform caam_sm: 128-bit black key:&lt;BR /&gt;platform caam_sm: [0000] a1 03 32 2c 21 5d 6a b1&lt;BR /&gt;platform caam_sm: [0008] 16 a6 c1 bf 39 86 55 66&lt;BR /&gt;platform caam_sm: 192-bit clear key:&lt;BR /&gt;platform caam_sm: [0000] 00 01 02 03 04 0f 06 07&lt;BR /&gt;platform caam_sm: [0008] 08 09 0a 0b 0c 0d 0e 0f&lt;BR /&gt;platform caam_sm: [0016] 10 11 12 13 14 15 16 17&lt;BR /&gt;platform caam_sm: 192-bit black key:&lt;BR /&gt;platform caam_sm: [0000] 34 8f a5 1e 09 41 49 7e&lt;BR /&gt;platform caam_sm: [0008] e0 2c 1a 95 ea 0d 1f 96&lt;BR /&gt;platform caam_sm: [0016] c1 f0 5a 81 c7 02 d3 5a&lt;BR /&gt;platform caam_sm: [0024] 85 3b 97 25 5c 9d 1d a7&lt;BR /&gt;platform caam_sm: 256-bit clear key:&lt;BR /&gt;platform caam_sm: [0000] 00 01 02 03 04 0f 06 07&lt;BR /&gt;platform caam_sm: [0008] 08 09 0a 0b 0c 0d 0e 0f&lt;BR /&gt;platform caam_sm: [0016] 10 11 12 13 14 15 16 17&lt;BR /&gt;platform caam_sm: [0024] 18 19 1a 1b 1c 1d 1e 1f&lt;BR /&gt;platform caam_sm: 256-bit black key:&lt;BR /&gt;platform caam_sm: [0000] 39 a6 ae 03 62 ad 61 80&lt;BR /&gt;platform caam_sm: [0008] d3 55 21 29 4d fe 63 ec&lt;BR /&gt;platform caam_sm: [0016] 28 97 e0 46 fa 08 a4 74&lt;BR /&gt;platform caam_sm: [0024] 6f ce c5 1a ae 6c 89 88&lt;BR /&gt;platform caam_sm: 64-bit unwritten blob:&lt;BR /&gt;platform caam_sm: [0000] 00 00 00 00 00 00 00 00&lt;BR /&gt;platform caam_sm: [0008] 00 00 00 00 00 00 00 00&lt;BR /&gt;platform caam_sm: [0016] 00 00 00 00 00 00 00 00&lt;BR /&gt;platform caam_sm: [0024] 00 00 00 00 00 00 00 00&lt;BR /&gt;platform caam_sm: [0032] 00 00 00 00 00 00 00 00&lt;BR /&gt;platform caam_sm: [0040] 00 00 00 00 00 00 00 00&lt;BR /&gt;platform caam_sm: [0048] 00 00 00 00 00 00 00 00&lt;BR /&gt;platform caam_sm: [0056] 00 00 00 00 00 00 00 00&lt;BR /&gt;platform caam_sm: [0064] 00 00 00 00 00 00 00 00&lt;BR /&gt;platform caam_sm: [0072] 00 00 00 00 00 00 00 00&lt;BR /&gt;platform caam_sm: [0080] 00 00 00 00 00 00 00 00&lt;BR /&gt;platform caam_sm: [0088] 00 00 00 00 00 00 00 00&lt;BR /&gt;platform caam_sm: 128-bit unwritten blob:&lt;BR /&gt;platform caam_sm: [0000] 00 00 00 00 00 00 00 00&lt;BR /&gt;platform caam_sm: [0008] 00 00 00 00 00 00 00 00&lt;BR /&gt;platform caam_sm: [0016] 00 00 00 00 00 00 00 00&lt;BR /&gt;platform caam_sm: [0024] 00 00 00 00 00 00 00 00&lt;BR /&gt;platform caam_sm: [0032] 00 00 00 00 00 00 00 00&lt;BR /&gt;platform caam_sm: [0040] 00 00 00 00 00 00 00 00&lt;BR /&gt;platform caam_sm: [0048] 00 00 00 00 00 00 00 00&lt;BR /&gt;platform caam_sm: [0056] 00 00 00 00 00 00 00 00&lt;BR /&gt;platform caam_sm: [0064] 00 00 00 00 00 00 00 00&lt;BR /&gt;platform caam_sm: [0072] 00 00 00 00 00 00 00 00&lt;BR /&gt;platform caam_sm: [0080] 00 00 00 00 00 00 00 00&lt;BR /&gt;platform caam_sm: [0088] 00 00 00 00 00 00 00 00&lt;BR /&gt;platform caam_sm: 196-bit unwritten blob:&lt;BR /&gt;platform caam_sm: [0000] 00 00 00 00 00 00 00 00&lt;BR /&gt;platform caam_sm: [0008] 00 00 00 00 00 00 00 00&lt;BR /&gt;platform caam_sm: [0016] 00 00 00 00 00 00 00 00&lt;BR /&gt;platform caam_sm: [0024] 00 00 00 00 00 00 00 00&lt;BR /&gt;platform caam_sm: [0032] 00 00 00 00 00 00 00 00&lt;BR /&gt;platform caam_sm: [0040] 00 00 00 00 00 00 00 00&lt;BR /&gt;platform caam_sm: [0048] 00 00 00 00 00 00 00 00&lt;BR /&gt;platform caam_sm: [0056] 00 00 00 00 00 00 00 00&lt;BR /&gt;platform caam_sm: [0064] 00 00 00 00 00 00 00 00&lt;BR /&gt;platform caam_sm: [0072] 00 00 00 00 00 00 00 00&lt;BR /&gt;platform caam_sm: [0080] 00 00 00 00 00 00 00 00&lt;BR /&gt;platform caam_sm: [0088] 00 00 00 00 00 00 00 00&lt;BR /&gt;platform caam_sm: 256-bit unwritten blob:&lt;BR /&gt;platform caam_sm: [0000] 00 00 00 00 00 00 00 00&lt;BR /&gt;platform caam_sm: [0008] 00 00 00 00 00 00 00 00&lt;BR /&gt;platform caam_sm: [0016] 00 00 00 00 00 00 00 00&lt;BR /&gt;platform caam_sm: [0024] 00 00 00 00 00 00 00 00&lt;BR /&gt;platform caam_sm: [0032] 00 00 00 00 00 00 00 00&lt;BR /&gt;platform caam_sm: [0040] 00 00 00 00 00 00 00 00&lt;BR /&gt;platform caam_sm: [0048] 00 00 00 00 00 00 00 00&lt;BR /&gt;platform caam_sm: [0056] 00 00 00 00 00 00 00 00&lt;BR /&gt;platform caam_sm: [0064] 00 00 00 00 00 00 00 00&lt;BR /&gt;platform caam_sm: [0072] 00 00 00 00 00 00 00 00&lt;BR /&gt;platform caam_sm: [0080] 00 00 00 00 00 00 00 00&lt;BR /&gt;platform caam_sm: [0088] 00 00 00 00 00 00 00 00&lt;BR /&gt;platform caam_sm: 64-bit black key in blob:&lt;BR /&gt;platform caam_sm: [0000] ee 7c 21 0d 3a 1a cf fa&lt;BR /&gt;platform caam_sm: [0008] 1c 9f 3b 8b ee 89 0c c0&lt;BR /&gt;platform caam_sm: [0016] bd f5 15 9f 53 73 17 53&lt;BR /&gt;platform caam_sm: [0024] 9a b2 2b 53 df 5e ed 98&lt;BR /&gt;platform caam_sm: [0032] 10 94 92 2d 8d 2a 39 cd&lt;BR /&gt;platform caam_sm: [0040] 69 59 d0 25 58 6f 82 79&lt;BR /&gt;platform caam_sm: [0048] bb a9 21 60 c3 21 a9 f2&lt;BR /&gt;platform caam_sm: [0056] 00 00 00 00 00 00 00 00&lt;BR /&gt;platform caam_sm: [0064] 00 00 00 00 00 00 00 00&lt;BR /&gt;platform caam_sm: [0072] 00 00 00 00 00 00 00 00&lt;BR /&gt;platform caam_sm: [0080] 00 00 00 00 00 00 00 00&lt;BR /&gt;platform caam_sm: [0088] 00 00 00 00 00 00 00 00&lt;BR /&gt;platform caam_sm: 128-bit black key in blob:&lt;BR /&gt;platform caam_sm: [0000] 9b f8 9b 02 60 1d 04 fa&lt;BR /&gt;platform caam_sm: [0008] ae 99 fd 11 f5 4f 1a 22&lt;BR /&gt;platform caam_sm: [0016] 15 9d 75 f5 17 c9 8d 28&lt;BR /&gt;platform caam_sm: [0024] be dd d7 4e b6 66 91 98&lt;BR /&gt;platform caam_sm: [0032] c0 29 10 c3 8a 48 95 48&lt;BR /&gt;platform caam_sm: [0040] 76 31 5d 2e e6 c4 52 70&lt;BR /&gt;platform caam_sm: [0048] 3a b3 32 24 76 23 14 5e&lt;BR /&gt;platform caam_sm: [0056] 6c 29 6a 98 86 66 0a a8&lt;BR /&gt;platform caam_sm: [0064] 00 00 00 00 00 00 00 00&lt;BR /&gt;platform caam_sm: [0072] 00 00 00 00 00 00 00 00&lt;BR /&gt;platform caam_sm: [0080] 00 00 00 00 00 00 00 00&lt;BR /&gt;platform caam_sm: [0088] 00 00 00 00 00 00 00 00&lt;BR /&gt;platform caam_sm: 192-bit black key in blob:&lt;BR /&gt;platform caam_sm: [0000] 38 ab ca 5b 32 62 cc 60&lt;BR /&gt;platform caam_sm: [0008] f1 95 0c ac 5f 33 25 e6&lt;BR /&gt;platform caam_sm: [0016] 93 e9 66 c7 dc 24 fa 03&lt;BR /&gt;platform caam_sm: [0024] 7f 8b a7 68 a9 ae b8 05&lt;BR /&gt;platform caam_sm: [0032] 9f 93 79 35 32 46 cc 37&lt;BR /&gt;platform caam_sm: [0040] 1e fe 85 b6 f8 4e 74 cb&lt;BR /&gt;platform caam_sm: [0048] f5 5e e1 0f 6f 69 cd 4d&lt;BR /&gt;platform caam_sm: [0056] 9a 7d e7 34 72 15 a9 23&lt;BR /&gt;platform caam_sm: [0064] fb 5b 3e ca 8b e5 7c 13&lt;BR /&gt;platform caam_sm: [0072] 00 00 00 00 00 00 00 00&lt;BR /&gt;platform caam_sm: [0080] 00 00 00 00 00 00 00 00&lt;BR /&gt;platform caam_sm: [0088] 00 00 00 00 00 00 00 00&lt;BR /&gt;platform caam_sm: 256-bit black key in blob:&lt;BR /&gt;platform caam_sm: [0000] e0 79 06 a9 80 98 47 1c&lt;BR /&gt;platform caam_sm: [0008] 6f 10 19 35 40 74 30 f4&lt;BR /&gt;platform caam_sm: [0016] d3 04 59 b7 2d da 5f 86&lt;BR /&gt;platform caam_sm: [0024] 5a e3 90 a6 0a 99 27 50&lt;BR /&gt;platform caam_sm: [0032] d6 70 60 8a ec b6 d6 c0&lt;BR /&gt;platform caam_sm: [0040] 39 11 f2 81 60 6b 44 35&lt;BR /&gt;platform caam_sm: [0048] 7a 15 86 b5 14 3e 91 01&lt;BR /&gt;platform caam_sm: [0056] 5e 9a 2e a1 65 d0 ce 8a&lt;BR /&gt;platform caam_sm: [0064] 70 0c 5a 4f ee 89 74 f7&lt;BR /&gt;platform caam_sm: [0072] 28 65 37 76 c3 28 23 f1&lt;BR /&gt;platform caam_sm: [0080] 00 00 00 00 00 00 00 00&lt;BR /&gt;platform caam_sm: [0088] 00 00 00 00 00 00 00 00&lt;BR /&gt;platform caam_sm: restored 64-bit black key:&lt;BR /&gt;platform caam_sm: [0000] ed 33 8d 86 07 b6 ed 56&lt;BR /&gt;platform caam_sm: [0008] 5c b0 b6 a1 4e 3d 20 f9&lt;BR /&gt;platform caam_sm: restored 128-bit black key:&lt;BR /&gt;platform caam_sm: [0000] a1 03 32 2c 21 5d 6a b1&lt;BR /&gt;platform caam_sm: [0008] 16 a6 c1 bf 39 86 55 66&lt;BR /&gt;platform caam_sm: restored 192-bit black key:&lt;BR /&gt;platform caam_sm: [0000] 34 8f a5 1e 09 41 49 7e&lt;BR /&gt;platform caam_sm: [0008] e0 2c 1a 95 ea 0d 1f 96&lt;BR /&gt;platform caam_sm: [0016] 74 e6 21 9e 6c 48 a0 3d&lt;BR /&gt;platform caam_sm: [0024] e3 67 7b 99 8a e5 13 06&lt;BR /&gt;platform caam_sm: restored 256-bit black key:&lt;BR /&gt;platform caam_sm: [0000] 39 a6 ae 03 62 ad 61 80&lt;BR /&gt;platform caam_sm: [0008] d3 55 21 29 4d fe 63 ec&lt;BR /&gt;platform caam_sm: [0016] 28 97 e0 46 fa 08 a4 74&lt;BR /&gt;platform caam_sm: [0024] 6f ce c5 1a ae 6c 89 88&lt;BR /&gt;snvs-secvio 20cc000.caam-snvs: violation handlers armed - non-secure state&lt;BR /&gt;usbcore: registered new interface driver usbhid&lt;BR /&gt;usbhid: USB HID core driver&lt;BR /&gt;wm8962 0-001a: Failed to read ID register&lt;BR /&gt;wm8962: probe of 0-001a failed with error -5&lt;BR /&gt;imx-wm8962 sound.25: failed to find codec platform device&lt;BR /&gt;imx-wm8962: probe of sound.25 failed with error -22&lt;BR /&gt;imx-audio-hdmi sound-hdmi.26: hdmi-hifi &amp;lt;-&amp;gt; hdmi_audio.17 mapping ok&lt;BR /&gt;NET: Registered protocol family 26&lt;BR /&gt;TCP: cubic registered&lt;BR /&gt;NET: Registered protocol family 10&lt;BR /&gt;sit: IPv6 over IPv4 tunneling driver&lt;BR /&gt;NET: Registered protocol family 17&lt;BR /&gt;can: controller area network core (rev 20120528 abi 9)&lt;BR /&gt;NET: Registered protocol family 29&lt;BR /&gt;can: raw protocol (rev 20120528)&lt;BR /&gt;can: broadcast manager protocol (rev 20120528 t)&lt;BR /&gt;can: netlink gateway (rev 20130117) max_hops=1&lt;BR /&gt;Bluetooth: RFCOMM TTY layer initialized&lt;BR /&gt;Bluetooth: RFCOMM socket layer initialized&lt;BR /&gt;Bluetooth: RFCOMM ver 1.11&lt;BR /&gt;Bluetooth: BNEP (Ethernet Emulation) ver 1.3&lt;BR /&gt;Bluetooth: BNEP filters: protocol multicast&lt;BR /&gt;Bluetooth: BNEP socket layer initialized&lt;BR /&gt;Bluetooth: HIDP (Human Interface Emulation) ver 1.2&lt;BR /&gt;Bluetooth: HIDP socket layer initialized&lt;BR /&gt;8021q: 802.1Q VLAN Support v1.8&lt;BR /&gt;Key type dns_resolver registered&lt;BR /&gt;VFP support v0.3: implementor 41 architecture 3 part 30 variant 9 rev 4&lt;BR /&gt;VGEN3: disabling&lt;BR /&gt;VGEN2: disabling&lt;BR /&gt;VGEN1: disabling&lt;BR /&gt;SWBST: disabling&lt;BR /&gt;SW4: disabling&lt;BR /&gt;wm8962-supply: disabling&lt;BR /&gt;regulator-dummy: disabling&lt;BR /&gt;imx mcc test is registered.&lt;BR /&gt;input: gpio-keys.24 as /devices/soc0/gpio-keys.24/input/input0&lt;BR /&gt;snvs_rtc 20cc034.snvs-rtc-lp: setting system clock to 1970-01-01 00:03:57 UTC (237)&lt;BR /&gt;ALSA device list:&lt;BR /&gt; #0: imx-hdmi-soc&lt;BR /&gt;kjournald starting. Commit interval 5 seconds&lt;BR /&gt;EXT3-fs (mmcblk3p2): using internal journal&lt;BR /&gt;EXT3-fs (mmcblk3p2): mounted filesystem with ordered data mode&lt;BR /&gt;VFS: Mounted root (ext3 filesystem) on device 179:2.&lt;BR /&gt;devtmpfs: mounted&lt;BR /&gt;Freeing unused kernel memory: 304K (80c7a000 - 80cc6000)&lt;BR /&gt;Starting logging: OK&lt;BR /&gt;Initializing random number generator... done.&lt;BR /&gt;Starting network...&lt;BR /&gt; &lt;BR /&gt;Welcome to Buildroot&lt;BR /&gt; buildroot login: root&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 05 Jun 2018 11:22:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/ov5642-30fps-not-working/m-p/722445#M112339</guid>
      <dc:creator>jamalmohiuddin</dc:creator>
      <dc:date>2018-06-05T11:22:57Z</dc:date>
    </item>
  </channel>
</rss>