<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic TJA1043 state after power-on in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/TJA1043-state-after-power-on/m-p/722425#M112319</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi all,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am using TJA1043 in my project, and the issue I am experiencing is the following:&lt;/P&gt;&lt;P&gt;On power-on, only Vbat is present, despite that, in the first moment, INH signal is set high and only after about 200ms it is set floating.&lt;/P&gt;&lt;P&gt;My question is why TJA1043 does not immediately go to sleep-mode after power-on when only Vbat is present? How can I force it to do that?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Our setup is pretty simple, and the circuit is identical to the one provided in the application note.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 15 Jan 2018 15:10:19 GMT</pubDate>
    <dc:creator>nexy_sm</dc:creator>
    <dc:date>2018-01-15T15:10:19Z</dc:date>
    <item>
      <title>TJA1043 state after power-on</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/TJA1043-state-after-power-on/m-p/722425#M112319</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi all,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am using TJA1043 in my project, and the issue I am experiencing is the following:&lt;/P&gt;&lt;P&gt;On power-on, only Vbat is present, despite that, in the first moment, INH signal is set high and only after about 200ms it is set floating.&lt;/P&gt;&lt;P&gt;My question is why TJA1043 does not immediately go to sleep-mode after power-on when only Vbat is present? How can I force it to do that?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Our setup is pretty simple, and the circuit is identical to the one provided in the application note.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 15 Jan 2018 15:10:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/TJA1043-state-after-power-on/m-p/722425#M112319</guid>
      <dc:creator>nexy_sm</dc:creator>
      <dc:date>2018-01-15T15:10:19Z</dc:date>
    </item>
    <item>
      <title>Re: TJA1043 state after power-on</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/TJA1043-state-after-power-on/m-p/722426#M112320</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;The only way to put the TJA1043 into Sleep Mode is via Go-to-Sleep mode, and with an under-voltage detection on either VCC or VIO:&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;OL&gt;&lt;LI&gt;&lt;SPAN&gt; Using the Go-to-Sleep Mode (STBN to LOW, EN to HIGH). &lt;/SPAN&gt;&lt;/LI&gt;&lt;/OL&gt;&lt;P&gt;&lt;SPAN&gt;If it is selected for longer than the minimum hold time of go-to-sleep command th(min) (20 us), the transceiver is automatically forced into Sleep Mode switching the pin INH to floating. &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;OL start="2"&gt;&lt;LI&gt;&lt;SPAN&gt; By an under-voltage detection on VIO or VCC. &lt;/SPAN&gt;&lt;/LI&gt;&lt;/OL&gt;&lt;P&gt;&lt;SPAN&gt;When the under-voltage detection time (350ms) on either VCC (Vuvd(VCC) = 3.5V) or VIO (Vuvd(VIO) = 1.8V) elapses before the relevant voltage level has recovered.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Jose&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 16 Jan 2018 20:53:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/TJA1043-state-after-power-on/m-p/722426#M112320</guid>
      <dc:creator>reyes</dc:creator>
      <dc:date>2018-01-16T20:53:05Z</dc:date>
    </item>
    <item>
      <title>Re: TJA1043 state after power-on</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/TJA1043-state-after-power-on/m-p/722427#M112321</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;in my use case, when I switch the board on, only Vbat is present. What I measure is that INH is active for 200ms after which it goes floating, and I assumed that TJA1043 is in one of the states, and in parallel it measures the absence of the supply voltage.&lt;/P&gt;&lt;P&gt;Is there any chance to send it directly to the sleep-mode, before it actually starts with measuring 350ms until UVnom flag is set? Since this can be done only by STB_N and EN pins, I wonder which condition has priority, undervoltag or pins?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanx&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 17 Jan 2018 09:36:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/TJA1043-state-after-power-on/m-p/722427#M112321</guid>
      <dc:creator>nexy_sm</dc:creator>
      <dc:date>2018-01-17T09:36:17Z</dc:date>
    </item>
    <item>
      <title>Re: TJA1043 state after power-on</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/TJA1043-state-after-power-on/m-p/722428#M112322</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;No, if you are using under voltage to go to sleep mode, the 350ms time window with undervoltage condition should pass before going to sleep mode. &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Using the Go-to-Sleep Mode (STBN to LOW, EN to HIGH pins), first, the device should be in functional mode. &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Jose&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 17 Jan 2018 19:43:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/TJA1043-state-after-power-on/m-p/722428#M112322</guid>
      <dc:creator>reyes</dc:creator>
      <dc:date>2018-01-17T19:43:44Z</dc:date>
    </item>
    <item>
      <title>Re: TJA1043 state after power-on</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/TJA1043-state-after-power-on/m-p/722429#M112323</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thank you very much&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 18 Jan 2018 10:37:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/TJA1043-state-after-power-on/m-p/722429#M112323</guid>
      <dc:creator>nexy_sm</dc:creator>
      <dc:date>2018-01-18T10:37:28Z</dc:date>
    </item>
  </channel>
</rss>