<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックGetting an HDMI output on IMX8QMLPDDR4ARM2</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Getting-an-HDMI-output-on-IMX8QMLPDDR4ARM2/m-p/722313#M112302</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I just received my i.MX8 QM (LPD4CPU according to the packing list).&lt;/P&gt;&lt;P&gt;I set up my yocto environment as mentionned in the user guide with the repo command :&lt;/P&gt;&lt;P&gt;repo init -u &lt;A href="https://source.codeaurora.org/external/imx/imx-manifest"&gt;https://source.codeaurora.org/external/imx/imx-manifest&lt;/A&gt; -b imx-linux-morty -m imx-4.9.51-8qm_beta2.xml&lt;/P&gt;&lt;P&gt;I built an image with yocto setting the correct machine, and wayland as a distro :&lt;/P&gt;&lt;P&gt;DISTRO=fsl-imx-wayland MACHINE=imx8qmlpddr4arm2 source fsl-setup-release.sh -b build&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Then I ran a "bitbake fsl-image-qt5-validation-imx" and flash my SD card to boot on.&lt;/P&gt;&lt;P&gt;I connected my computer to the serial port and uses minicomto comunicate.&lt;/P&gt;&lt;P&gt;I also connected a screen (iiyama prolite b2280hs) through HDMI to the imx8 and expected to see the boot screen and then the GUI.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;But when I boot the card, I have all the information about the boot that are displayed on the console (with the serial port) but nothing on the HDMI. When the boot end, I am connected to the console through the serial port, but still nothing on the HDMI.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I tried to setup the uboot environment for a 1080p60FPS screen, like it was mentionned here : &lt;A href="https://community.nxp.com/thread/470325"&gt;Getting a 4K HDMI output on MCIMX8M-EVK&lt;/A&gt; , but it does not work either.&lt;/P&gt;&lt;P&gt;setenv mmcargs 'setenv bootargs console=${console} root=${mmcroot} video=HDMI-A-1:1920x1080-32@60'&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm not sure if the problem comes from the monitor I use, or from the board itself. I tried to change several times the uboot environment to enable the HDMI and set up the display but without any success.&lt;/P&gt;&lt;P&gt;If anyone as encountered this problem, it would be great to discuss about it.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Mathias&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;CODE&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;/CODE&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 01 Mar 2018 15:56:29 GMT</pubDate>
    <dc:creator>mathias_faro</dc:creator>
    <dc:date>2018-03-01T15:56:29Z</dc:date>
    <item>
      <title>Getting an HDMI output on IMX8QMLPDDR4ARM2</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Getting-an-HDMI-output-on-IMX8QMLPDDR4ARM2/m-p/722313#M112302</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I just received my i.MX8 QM (LPD4CPU according to the packing list).&lt;/P&gt;&lt;P&gt;I set up my yocto environment as mentionned in the user guide with the repo command :&lt;/P&gt;&lt;P&gt;repo init -u &lt;A href="https://source.codeaurora.org/external/imx/imx-manifest"&gt;https://source.codeaurora.org/external/imx/imx-manifest&lt;/A&gt; -b imx-linux-morty -m imx-4.9.51-8qm_beta2.xml&lt;/P&gt;&lt;P&gt;I built an image with yocto setting the correct machine, and wayland as a distro :&lt;/P&gt;&lt;P&gt;DISTRO=fsl-imx-wayland MACHINE=imx8qmlpddr4arm2 source fsl-setup-release.sh -b build&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Then I ran a "bitbake fsl-image-qt5-validation-imx" and flash my SD card to boot on.&lt;/P&gt;&lt;P&gt;I connected my computer to the serial port and uses minicomto comunicate.&lt;/P&gt;&lt;P&gt;I also connected a screen (iiyama prolite b2280hs) through HDMI to the imx8 and expected to see the boot screen and then the GUI.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;But when I boot the card, I have all the information about the boot that are displayed on the console (with the serial port) but nothing on the HDMI. When the boot end, I am connected to the console through the serial port, but still nothing on the HDMI.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I tried to setup the uboot environment for a 1080p60FPS screen, like it was mentionned here : &lt;A href="https://community.nxp.com/thread/470325"&gt;Getting a 4K HDMI output on MCIMX8M-EVK&lt;/A&gt; , but it does not work either.&lt;/P&gt;&lt;P&gt;setenv mmcargs 'setenv bootargs console=${console} root=${mmcroot} video=HDMI-A-1:1920x1080-32@60'&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm not sure if the problem comes from the monitor I use, or from the board itself. I tried to change several times the uboot environment to enable the HDMI and set up the display but without any success.&lt;/P&gt;&lt;P&gt;If anyone as encountered this problem, it would be great to discuss about it.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Mathias&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;CODE&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;/CODE&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 01 Mar 2018 15:56:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Getting-an-HDMI-output-on-IMX8QMLPDDR4ARM2/m-p/722313#M112302</guid>
      <dc:creator>mathias_faro</dc:creator>
      <dc:date>2018-03-01T15:56:29Z</dc:date>
    </item>
    <item>
      <title>Re: Getting an HDMI output on IMX8QMLPDDR4ARM2</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Getting-an-HDMI-output-on-IMX8QMLPDDR4ARM2/m-p/722314#M112303</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Can you please try with xwayland as Distro?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;DISTRO=fsl-imx-xwayland MACHINE=imx8qmlpddr4arm2 source fsl-setup-release.sh -b build&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We recommend use xwayland as Distro.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I hope this can solve your problem.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Diego.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 01 Mar 2018 17:45:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Getting-an-HDMI-output-on-IMX8QMLPDDR4ARM2/m-p/722314#M112303</guid>
      <dc:creator>diegoadrian</dc:creator>
      <dc:date>2018-03-01T17:45:44Z</dc:date>
    </item>
    <item>
      <title>Re: Getting an HDMI output on IMX8QMLPDDR4ARM2</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Getting-an-HDMI-output-on-IMX8QMLPDDR4ARM2/m-p/722315#M112304</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks for your response, I try to change the distro and I keep you updated.&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Mathias&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 02 Mar 2018 08:05:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Getting-an-HDMI-output-on-IMX8QMLPDDR4ARM2/m-p/722315#M112304</guid>
      <dc:creator>mathias_faro</dc:creator>
      <dc:date>2018-03-02T08:05:31Z</dc:date>
    </item>
    <item>
      <title>Re: Getting an HDMI output on IMX8QMLPDDR4ARM2</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Getting-an-HDMI-output-on-IMX8QMLPDDR4ARM2/m-p/722316#M112305</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;After a pretty long build I tried the new distro (xwayland). But the result is the same. Nothing pops on the HDMI and my screen keep displaying "no signal". I tried both configuration of switch 8 (ON/OFF even if I guess the good one is ON) because it defines the screen that will be used between HDMI and DP.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I attach yout my default uboot environment, no display (HDMI) or panel are present.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;printenv&lt;BR /&gt;baudrate=115200&lt;BR /&gt;board_name=ARM2&lt;BR /&gt;board_rev=iMX8QM&lt;BR /&gt;boot_fdt=try&lt;BR /&gt;bootcmd=mmc dev ${mmcdev}; if mmc rescan; then if run loadbootscript; then run bootscript; else if run loadimage; then run mmcboot; else run netboot; fi; fi; else booti ${loadaddr} - ${fdt_addr}; fi&lt;BR /&gt;bootcmd_mfg=run mfgtool_args;booti ${loadaddr} ${initrd_addr} ${fdt_addr};&lt;BR /&gt;bootdelay=3&lt;BR /&gt;bootscript=echo Running bootscript from mmc ...; source&lt;BR /&gt;commit_mkimage=4352f717&lt;BR /&gt;commit_scfw=c873dc14&lt;BR /&gt;console=ttyLP0,115200 earlycon=lpuart32,0x5a060000,115200&lt;BR /&gt;eth1addr=00:04:9f:05:1f:da&lt;BR /&gt;ethact=ethernet@5b040000&lt;BR /&gt;ethaddr=00:04:9f:05:1f:d9&lt;BR /&gt;ethprime=eth0&lt;BR /&gt;fdt_addr=0x83000000&lt;BR /&gt;fdt_file="fsl-imx8qm-lpddr4-arm2".dtb&lt;BR /&gt;fdt_high=0xffffffffffffffff&lt;BR /&gt;fdtcontroladdr=fda7f6b8&lt;BR /&gt;hdp_addr=0x84000000&lt;BR /&gt;hdp_file=dpfw.bin&lt;BR /&gt;image=Image&lt;BR /&gt;initrd_addr=0x83800000&lt;BR /&gt;initrd_high=0xffffffffffffffff&lt;BR /&gt;loadaddr=0x80280000&lt;BR /&gt;loadfdt=fatload mmc ${mmcdev}:${mmcpart} ${fdt_addr} ${fdt_file}&lt;BR /&gt;loadhdp=fatload mmc ${mmcdev}:${mmcpart} ${hdp_addr} ${hdp_file}&lt;BR /&gt;loadimage=fatload mmc ${mmcdev}:${mmcpart} ${loadaddr} ${image}&lt;BR /&gt;loadm4image_0=fatload mmc ${mmcdev}:${mmcpart} ${loadaddr} ${m4_0_image}&lt;BR /&gt;loadm4image_1=fatload mmc ${mmcdev}:${mmcpart} ${loadaddr} ${m4_1_image}&lt;BR /&gt;m4_0_image=m4_0.bin&lt;BR /&gt;m4_1_image=m4_1.bin&lt;BR /&gt;m4boot_0=run loadm4image_0; dcache flush; bootaux ${loadaddr} 0&lt;BR /&gt;m4boot_1=run loadm4image_1; dcache flush; bootaux ${loadaddr} 1&lt;BR /&gt;mfgtool_args=setenv bootargs console=${console},${baudrate} rdinit=/linuxrc g_mass_storage.stall=0 g_mass_storage.removable=1 g_mass_storage.idVendor=0x066F g_mass_storage.idProduct=0x37FF g_mass_storage.iSerialNumber="" video=imxdpufb5: &lt;BR /&gt;mmcargs=setenv bootargs console=${console},${baudrate} root=${mmcroot} loadbootscript=fatload mmc ${mmcdev}:${mmcpart} ${loadaddr} ${script};&lt;BR /&gt;mmcautodetect=yes&lt;BR /&gt;mmcboot=echo Booting from mmc ...; run loadhdp; hdp load ${hdp_addr}; run mmcargs; if test ${boot_fdt} = yes || test ${boot_fdt} = try; then if run loadfdt; then booti ${loadaddr} - ${fdt_addr}; else echo WARN: Cannot load the DT; fi; el;&lt;BR /&gt;mmcdev=1&lt;BR /&gt;mmcpart=1&lt;BR /&gt;mmcroot=/dev/mmcblk1p2 rootwait rw&lt;BR /&gt;netargs=setenv bootargs console=${console} root=/dev/nfs ip=dhcp nfsroot=${serverip}:${nfsroot},v3,tcp video=imxdpufb5:off video=imxdpufb6:off video=imxdpufb7:off&lt;BR /&gt;netboot=echo Booting from net ...; run netargs;&amp;nbsp; if test ${ip_dyn} = yes; then setenv get_cmd dhcp; else setenv get_cmd tftp; fi; ${get_cmd} ${hdp_addr} ${hdp_file}; hdp load ${hdp_addr}; ${get_cmd} ${loadaddr} ${image}; if test ${boot_f;&lt;BR /&gt;panel=NULL&lt;BR /&gt;script=boot.scr&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Environment size: 2812/4092 bytes&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If you want to check others log (dmesg or boot log) let me know. And if you have any other suggestions it would be really appreciated.&lt;/P&gt;&lt;P&gt;Thank you in advance.&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Mathias&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 02 Mar 2018 15:13:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Getting-an-HDMI-output-on-IMX8QMLPDDR4ARM2/m-p/722316#M112305</guid>
      <dc:creator>mathias_faro</dc:creator>
      <dc:date>2018-03-02T15:13:25Z</dc:date>
    </item>
    <item>
      <title>Re: Getting an HDMI output on IMX8QMLPDDR4ARM2</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Getting-an-HDMI-output-on-IMX8QMLPDDR4ARM2/m-p/722317#M112306</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello, &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Can you please try setting the below bootarg and see if it works?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;u-boot -&amp;gt; setenv mmcargs 'setenv bootargs console=${console} root=${mmcroot} video=HDMI-A-1:3840x2160-32@30'&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Diego.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 07 Mar 2018 18:53:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Getting-an-HDMI-output-on-IMX8QMLPDDR4ARM2/m-p/722317#M112306</guid>
      <dc:creator>diegoadrian</dc:creator>
      <dc:date>2018-03-07T18:53:15Z</dc:date>
    </item>
    <item>
      <title>Re: Getting an HDMI output on IMX8QMLPDDR4ARM2</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Getting-an-HDMI-output-on-IMX8QMLPDDR4ARM2/m-p/722318#M112307</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;hi&amp;nbsp;&lt;A class="jx-jive-macro-user" href="https://community.nxp.com/people/mathias_faro"&gt;mathias_faro&lt;/A&gt;,&lt;/P&gt;&lt;P&gt;‌ have you solved your problem?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;i'm facing exactly the same problem, and none of the solutions worked.&lt;/P&gt;&lt;P&gt;trying X11 only distro or xwayland have the same phenomenon.&lt;/P&gt;&lt;P&gt;also trying different monitors doesn't help.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;on X11 distro, the Xorg log complains about "no screen found".&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Arnaud Tonda&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 26 Apr 2018 07:59:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Getting-an-HDMI-output-on-IMX8QMLPDDR4ARM2/m-p/722318#M112307</guid>
      <dc:creator>arnaudtonda</dc:creator>
      <dc:date>2018-04-26T07:59:11Z</dc:date>
    </item>
    <item>
      <title>Re: Getting an HDMI output on IMX8QMLPDDR4ARM2</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Getting-an-HDMI-output-on-IMX8QMLPDDR4ARM2/m-p/722319#M112308</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;concerning this problem, I may have found why the native HDMI does not work.&lt;/P&gt;&lt;P&gt;In fact, you can read in one of the the documentation provided by nxp (based on fsl-yocto-L4.9.51-mx8_beta2) :&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_1.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/9108i25ABE25FACF85D5C/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;I guess the board we use have this device tree, because it is pretty similar. For now the HDMI firmware is not loaded.&lt;/P&gt;&lt;P&gt;If you try to load it manually the kernel does not boot.. Need a fix about this.&lt;/P&gt;&lt;P&gt;A workaround may be to use the LVDS port (I guess there is one on the board, i does not have it anymore) and use an LVDS/HDMI connector and then plug your screen in HDMI.&lt;/P&gt;&lt;P&gt;Check with your nxp contact if they can provide you the LVDS/HDMI adaptor, i'm pretty sure this is the right way to have HDMI that properly works.&lt;/P&gt;&lt;P&gt;Tell me your results if you try.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Mathias Faro&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 26 Apr 2018 14:28:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Getting-an-HDMI-output-on-IMX8QMLPDDR4ARM2/m-p/722319#M112308</guid>
      <dc:creator>mathias_faro</dc:creator>
      <dc:date>2018-04-26T14:28:48Z</dc:date>
    </item>
    <item>
      <title>Re: Getting an HDMI output on IMX8QMLPDDR4ARM2</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Getting-an-HDMI-output-on-IMX8QMLPDDR4ARM2/m-p/722320#M112309</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Mathias Faro&amp;nbsp;&lt;/P&gt;&lt;P&gt;May I know what IMX8QMLPDDR4ARM2 is? Is it one EVK board? If yes could you send me one link for it?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I see 2 board from NXP web,&amp;nbsp;they are:&amp;nbsp;&lt;A class="link-titled" href="https://www.nxp.com/support/developer-resources/run-time-software/i.mx-developer-resources/i.mx-8quadxplus-multisensory-enablement-kit-mek:MCIMX8QXP-CPU" title="https://www.nxp.com/support/developer-resources/run-time-software/i.mx-developer-resources/i.mx-8quadxplus-multisensory-enablement-kit-mek:MCIMX8QXP-CPU"&gt;i.MX 8QuadXPlus Multisensory Enablement Kit|NXP&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;and&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="https://www.nxp.com/support/developer-resources/run-time-software/i.mx-developer-resources/evaluation-kit-for-the-i.mx-8m-applications-processor:MCIMX8M-EVK" title="https://www.nxp.com/support/developer-resources/run-time-software/i.mx-developer-resources/evaluation-kit-for-the-i.mx-8m-applications-processor:MCIMX8M-EVK"&gt;i.MX 8M Evaluation Kit|NXP&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;but I am not sure which one it is, or &lt;SPAN&gt;IMX8QMLPDDR4ARM2&amp;nbsp;&lt;/SPAN&gt;is pointing to some board else?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 28 Jan 2019 08:49:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Getting-an-HDMI-output-on-IMX8QMLPDDR4ARM2/m-p/722320#M112309</guid>
      <dc:creator>zhenyongliu</dc:creator>
      <dc:date>2019-01-28T08:49:18Z</dc:date>
    </item>
  </channel>
</rss>