<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic I.MX RT Flash debug in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/I-MX-RT-Flash-debug/m-p/722129#M112275</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; All I.MX RT examples are for debug in the external SDRAM.&amp;nbsp;How to change the examples to load, run and debug the code&amp;nbsp;in the the external QSPI flash and the external Hyper Flash?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp; One I.MX RT Microcontroller connected to an external quad-spi flash is enough to work as normal microcontroller? Allowing to load and debug the code into the quad-spi flash using the jtag, just like a microcontroller with internal flash.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;Ari.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 20 Nov 2017 14:56:14 GMT</pubDate>
    <dc:creator>arimendes</dc:creator>
    <dc:date>2017-11-20T14:56:14Z</dc:date>
    <item>
      <title>I.MX RT Flash debug</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/I-MX-RT-Flash-debug/m-p/722129#M112275</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; All I.MX RT examples are for debug in the external SDRAM.&amp;nbsp;How to change the examples to load, run and debug the code&amp;nbsp;in the the external QSPI flash and the external Hyper Flash?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp; One I.MX RT Microcontroller connected to an external quad-spi flash is enough to work as normal microcontroller? Allowing to load and debug the code into the quad-spi flash using the jtag, just like a microcontroller with internal flash.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;Ari.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 20 Nov 2017 14:56:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/I-MX-RT-Flash-debug/m-p/722129#M112275</guid>
      <dc:creator>arimendes</dc:creator>
      <dc:date>2017-11-20T14:56:14Z</dc:date>
    </item>
    <item>
      <title>Re: I.MX RT Flash debug</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/I-MX-RT-Flash-debug/m-p/722130#M112276</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Ari,&lt;/P&gt;&lt;P&gt;Now for the I.MX RT we default use the Hyper Flash. The QSPI flash can work on&amp;nbsp;the I.MX RT. If you want use the QSPI flash, here need the open SDA firmware for QSPI, change the default firmware in K20, and use the J-link to download. But the firmware for QSPI is not released by now, you can wait.&amp;nbsp;&amp;nbsp; &lt;/P&gt;&lt;P&gt;Have a nice day&lt;/P&gt;&lt;P&gt;Rita&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 26 Dec 2017 09:20:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/I-MX-RT-Flash-debug/m-p/722130#M112276</guid>
      <dc:creator>Rita_Wang</dc:creator>
      <dc:date>2017-12-26T09:20:38Z</dc:date>
    </item>
  </channel>
</rss>