<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックATDTW bit of USB Command Register</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/ATDTW-bit-of-USB-Command-Register/m-p/201870#M11225</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;At USB OTG HOST1 Contoller (Device Mode) of Reference Manual 56.6.18 describes ATDTW (Add dTD TripWire - Read/Write) bit of USB Command Register (USB_USBCMD) is bit-12, at Page 3304. But the source code of linux arcotg and RM of i.MX53 describes it as bit-14.&lt;/P&gt;&lt;P&gt;Which is correct?&lt;/P&gt;&lt;P&gt;&lt;SPAN class="mce_paste_marker"&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Sun, 09 Dec 2012 23:22:40 GMT</pubDate>
    <dc:creator>AtomuHidaka</dc:creator>
    <dc:date>2012-12-09T23:22:40Z</dc:date>
    <item>
      <title>ATDTW bit of USB Command Register</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/ATDTW-bit-of-USB-Command-Register/m-p/201870#M11225</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;At USB OTG HOST1 Contoller (Device Mode) of Reference Manual 56.6.18 describes ATDTW (Add dTD TripWire - Read/Write) bit of USB Command Register (USB_USBCMD) is bit-12, at Page 3304. But the source code of linux arcotg and RM of i.MX53 describes it as bit-14.&lt;/P&gt;&lt;P&gt;Which is correct?&lt;/P&gt;&lt;P&gt;&lt;SPAN class="mce_paste_marker"&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 09 Dec 2012 23:22:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/ATDTW-bit-of-USB-Command-Register/m-p/201870#M11225</guid>
      <dc:creator>AtomuHidaka</dc:creator>
      <dc:date>2012-12-09T23:22:40Z</dc:date>
    </item>
    <item>
      <title>Re: ATDTW bit of USB Command Register</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/ATDTW-bit-of-USB-Command-Register/m-p/201871#M11226</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Taking into account that USB modules for devices of i.MX series are very similar and are based on the same IP,&lt;BR /&gt;it is reasonable to guess that there are misprints in the i.MX50 RM regarding USB Command Register (USB_USBCMD)&lt;BR /&gt;in section 56.6.18. Correct description may be found in i.MX53 / 28 / 6 RM(s). I will report about misprints to the doc&lt;BR /&gt;team.&amp;nbsp;&amp;nbsp; Thank for this information !&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 12 Dec 2012 03:13:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/ATDTW-bit-of-USB-Command-Register/m-p/201871#M11226</guid>
      <dc:creator>Yuri</dc:creator>
      <dc:date>2012-12-12T03:13:36Z</dc:date>
    </item>
    <item>
      <title>Re: ATDTW bit of USB Command Register</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/ATDTW-bit-of-USB-Command-Register/m-p/201872#M11227</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Yuri,&lt;BR /&gt;Thank you for your response. It was very helpful advice. I will refer i.MX53 RM.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regarding misprints of i.MX50 RM, I have found another following misprints at 56.6.30 Port Status and Control (USB_PORTSC), page 3323.&lt;BR /&gt;- The bit map chart is incorrect.&lt;BR /&gt;- Bit 28, PTW bit assignment should be 0 and 1. Those are not 1 and 2.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Please send these informations to the doc team, too.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="mce_paste_marker"&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 12 Dec 2012 08:13:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/ATDTW-bit-of-USB-Command-Register/m-p/201872#M11227</guid>
      <dc:creator>AtomuHidaka</dc:creator>
      <dc:date>2012-12-12T08:13:47Z</dc:date>
    </item>
    <item>
      <title>Re: ATDTW bit of USB Command Register</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/ATDTW-bit-of-USB-Command-Register/m-p/201873#M11228</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I've already reported about the USB_PORTSC to the doc team earlier.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;1.&lt;/P&gt;&lt;P&gt;The table “USB_PORTSC field descriptions” is correct, but on the figure the bits &lt;/P&gt;&lt;P&gt;on right side from PFSC in the illustration should be shifted right (1 bit).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;2.&lt;/P&gt;&lt;P&gt;Writing PTW bit as 0 selects the&amp;nbsp;&amp;nbsp; 8-bit [60MHz] UTMI interface.&amp;nbsp; &lt;/P&gt;&lt;P&gt;Writing PTW bit as 1 selects the 16-bit [30MHz] UTMI interface.&lt;/P&gt;&lt;P&gt;&lt;SPAN class="mce_paste_marker"&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 12 Dec 2012 08:31:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/ATDTW-bit-of-USB-Command-Register/m-p/201873#M11228</guid>
      <dc:creator>Yuri</dc:creator>
      <dc:date>2012-12-12T08:31:58Z</dc:date>
    </item>
    <item>
      <title>Re: ATDTW bit of USB Command Register</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/ATDTW-bit-of-USB-Command-Register/m-p/201874#M11229</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Yuri,&lt;/P&gt;&lt;P&gt;OK, Thank you for your notice.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="mce_paste_marker"&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 12 Dec 2012 09:07:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/ATDTW-bit-of-USB-Command-Register/m-p/201874#M11229</guid>
      <dc:creator>AtomuHidaka</dc:creator>
      <dc:date>2012-12-12T09:07:48Z</dc:date>
    </item>
  </channel>
</rss>