<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: eMMC not visible in u-boot in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/eMMC-not-visible-in-u-boot/m-p/721460#M112200</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Igor,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;That is the exact u-boot version that I am using, I downloaded it from the NXP git repo. And I am using the defconfig from the evk.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;BLOCKQUOTE class="jive_macro_quote jive-quote jive_text_macro"&gt;U-Boot 2017.03 (Feb 23 2018 - 17:02:39 +0000)&lt;BR /&gt;&lt;BR /&gt;CPU:&amp;nbsp;&amp;nbsp; Freescale i.MX6UL rev1.1 528 MHz (running at 396 MHz)&lt;BR /&gt;CPU:&amp;nbsp;&amp;nbsp; Commercial temperature grade (0C to 95C) at 61C&lt;BR /&gt;Reset cause: WDOG&lt;BR /&gt;Model: Freescale i.MX6 UltraLite 14x14 EVK Board&lt;BR /&gt;Board: MX6UL 14x14 EVK&lt;BR /&gt;DRAM:&amp;nbsp; 512 MiB&lt;BR /&gt;MMC:&amp;nbsp;&amp;nbsp; FSL_SDHC: 0, FSL_SDHC: 1&lt;/BLOCKQUOTE&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks, I will try something else.&lt;/P&gt;&lt;P&gt;Antonio&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 22 Mar 2018 10:36:28 GMT</pubDate>
    <dc:creator>antonioramos</dc:creator>
    <dc:date>2018-03-22T10:36:28Z</dc:date>
    <item>
      <title>eMMC not visible in u-boot</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/eMMC-not-visible-in-u-boot/m-p/721458#M112198</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Please see the listing below.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;BLOCKQUOTE class="jive_macro_quote jive-quote jive_text_macro"&gt;&lt;P&gt;=&amp;gt;&amp;nbsp; mmc list&lt;/P&gt;&lt;P&gt;FSL_SDHC: 0 (SD)&lt;/P&gt;&lt;P&gt;FSL_SDHC: 1&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;=&amp;gt; ls mmc 1:1&lt;/P&gt;&lt;P&gt;&amp;nbsp; 1000000&amp;nbsp;&amp;nbsp; random_data1&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;1 file(s), 0 dir(s)&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;=&amp;gt;&amp;nbsp; mmc list&lt;/P&gt;&lt;P&gt;FSL_SDHC: 0 (SD)&lt;/P&gt;&lt;P&gt;FSL_SDHC: 1 (eMMC)&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Why is it that “mmc list” shows the eMMC after listing the directory but not before? Is this a bug or a feature?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I am using a board designed by ourselves based on the iMX6UL EVK. I am using my own image created with Buildroot using the Linux kernel and U-Boot from the 4.9 release by NXP. We have a MicroSD cage from which I am currently booting connected to port 1 and connected to port 2 we have Kingston EMMC04G-M627-Y02U eMMC (eMMC v5.1 compatible with v4.5). Once Linux boots I can (on eMMC) create partitions, format them and copy data, so everything seems fine in Linux so far.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 21 Mar 2018 15:11:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/eMMC-not-visible-in-u-boot/m-p/721458#M112198</guid>
      <dc:creator>antonioramos</dc:creator>
      <dc:date>2018-03-21T15:11:49Z</dc:date>
    </item>
    <item>
      <title>Re: eMMC not visible in u-boot</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/eMMC-not-visible-in-u-boot/m-p/721459#M112199</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi antonioramos&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;one can try with nxp uboot imx_v2017.03 :&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="https://source.codeaurora.org/external/imx/uboot-imx/?h=imx_v2017.03_4.9.11_1.0.0_ga" title="https://source.codeaurora.org/external/imx/uboot-imx/?h=imx_v2017.03_4.9.11_1.0.0_ga"&gt;uboot-imx - i.MX U-Boot&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;and use yocto for build, Yocto Guide guidelines from&lt;/P&gt;&lt;P&gt;Documentation package&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="https://www.nxp.com/webapp/Download?colCode=L4.9.11_1.0.0_LINUX_DOCS" title="https://www.nxp.com/webapp/Download?colCode=L4.9.11_1.0.0_LINUX_DOCS"&gt;https://www.nxp.com/webapp/Download?colCode=L4.9.11_1.0.0_LINUX_DOCS&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Also may be recommended to post issue on uboot mail list&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="https://lists.denx.de/listinfo/u-boot" title="https://lists.denx.de/listinfo/u-boot"&gt;U-Boot Info Page&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 21 Mar 2018 23:18:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/eMMC-not-visible-in-u-boot/m-p/721459#M112199</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2018-03-21T23:18:24Z</dc:date>
    </item>
    <item>
      <title>Re: eMMC not visible in u-boot</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/eMMC-not-visible-in-u-boot/m-p/721460#M112200</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Igor,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;That is the exact u-boot version that I am using, I downloaded it from the NXP git repo. And I am using the defconfig from the evk.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;BLOCKQUOTE class="jive_macro_quote jive-quote jive_text_macro"&gt;U-Boot 2017.03 (Feb 23 2018 - 17:02:39 +0000)&lt;BR /&gt;&lt;BR /&gt;CPU:&amp;nbsp;&amp;nbsp; Freescale i.MX6UL rev1.1 528 MHz (running at 396 MHz)&lt;BR /&gt;CPU:&amp;nbsp;&amp;nbsp; Commercial temperature grade (0C to 95C) at 61C&lt;BR /&gt;Reset cause: WDOG&lt;BR /&gt;Model: Freescale i.MX6 UltraLite 14x14 EVK Board&lt;BR /&gt;Board: MX6UL 14x14 EVK&lt;BR /&gt;DRAM:&amp;nbsp; 512 MiB&lt;BR /&gt;MMC:&amp;nbsp;&amp;nbsp; FSL_SDHC: 0, FSL_SDHC: 1&lt;/BLOCKQUOTE&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks, I will try something else.&lt;/P&gt;&lt;P&gt;Antonio&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 22 Mar 2018 10:36:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/eMMC-not-visible-in-u-boot/m-p/721460#M112200</guid>
      <dc:creator>antonioramos</dc:creator>
      <dc:date>2018-03-22T10:36:28Z</dc:date>
    </item>
  </channel>
</rss>