<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 The example code for lpuart_polling_seven_bits under driver examples -&amp;gt; lpuart doesn't work?</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/The-example-code-for-lpuart-polling-seven-bits-under-driver/m-p/721354#M112166</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The example code for lpuart_polling_seven_bits under driver examples -&amp;gt; lpuart doesn't work. Even the prints are not coming. When the data bits are changed to 8 bits in the same code it works.&lt;/P&gt;&lt;P&gt;The serial terminal was configured for 7 data bits. Execution is XIP mode in hyperflash&lt;/P&gt;&lt;P&gt;SDKs tried are SDK_2.3.0_MIMXRT1051xxxxx.zip&amp;nbsp; and SDK_2.3.1_EVKB-IMXRT1050.zip.&lt;/P&gt;&lt;P&gt;Could some one explain me on what i would be missing here?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;P&gt;Fayiz&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 03 May 2018 12:30:24 GMT</pubDate>
    <dc:creator>fayizonline</dc:creator>
    <dc:date>2018-05-03T12:30:24Z</dc:date>
    <item>
      <title>The example code for lpuart_polling_seven_bits under driver examples -&gt; lpuart doesn't work?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/The-example-code-for-lpuart-polling-seven-bits-under-driver/m-p/721354#M112166</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The example code for lpuart_polling_seven_bits under driver examples -&amp;gt; lpuart doesn't work. Even the prints are not coming. When the data bits are changed to 8 bits in the same code it works.&lt;/P&gt;&lt;P&gt;The serial terminal was configured for 7 data bits. Execution is XIP mode in hyperflash&lt;/P&gt;&lt;P&gt;SDKs tried are SDK_2.3.0_MIMXRT1051xxxxx.zip&amp;nbsp; and SDK_2.3.1_EVKB-IMXRT1050.zip.&lt;/P&gt;&lt;P&gt;Could some one explain me on what i would be missing here?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;P&gt;Fayiz&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 03 May 2018 12:30:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/The-example-code-for-lpuart-polling-seven-bits-under-driver/m-p/721354#M112166</guid>
      <dc:creator>fayizonline</dc:creator>
      <dc:date>2018-05-03T12:30:24Z</dc:date>
    </item>
    <item>
      <title>Re: The example code for lpuart_polling_seven_bits under driver examples -&gt; lpuart doesn't work?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/The-example-code-for-lpuart-polling-seven-bits-under-driver/m-p/721355#M112167</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Fayiz,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You need to ensure you are running SDK_2.3.0 examples on a EVK-IMXRT1050 and SDK_2.3.1 examples on EVKB-IMXRT1050 board, as the hardware changes between revisions affects the functionality.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Then, you should refer to the “readme.txt” file included on the “evkbimxrt1050_driver_examples_lpuart_lpuart_polling_seven_bits” example, where it is mentioned that UART TX and RX used for this example are RX:J22-2 and TX: J22-1 of the Arduino expansion headers of the board. I just tested such example, and it is working properly.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Hope this will be useful for you.&lt;BR /&gt;Best regards!&lt;BR /&gt;/Carlos&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 08 May 2018 01:36:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/The-example-code-for-lpuart-polling-seven-bits-under-driver/m-p/721355#M112167</guid>
      <dc:creator>CarlosCasillas</dc:creator>
      <dc:date>2018-05-08T01:36:18Z</dc:date>
    </item>
  </channel>
</rss>