<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックHow to change tty behavior on bluetooth socket</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/How-to-change-tty-behavior-on-bluetooth-socket/m-p/721341#M112162</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I'm running Linux on the iMX6Q. I have code that accepts a Bluetooth connection on a socket. When I did this on the command line, I could have used stty (stty -F /dev/rfcomm0 raw) to change the default TTY behavior from converting all my LFs to CRLFs. However, now I'm running from code, and /dev/rfcomm0 does not exist. The closest "device" I can find is /dev/bus/usb/001/002, but I cannot run stty on that device. When I send a line-feed in the data stream, the tty interface seems to change it to \r\n. The result is that my length field is incorrect. The protocol does not include \r, so it is not sufficient for me to just bump the length.&amp;nbsp;&lt;/P&gt;&lt;P&gt;I've looked at the supported ioctl controls and found nothing. Open to any and all suggestions.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 01 Mar 2018 20:40:37 GMT</pubDate>
    <dc:creator>patsandt</dc:creator>
    <dc:date>2018-03-01T20:40:37Z</dc:date>
    <item>
      <title>How to change tty behavior on bluetooth socket</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/How-to-change-tty-behavior-on-bluetooth-socket/m-p/721341#M112162</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I'm running Linux on the iMX6Q. I have code that accepts a Bluetooth connection on a socket. When I did this on the command line, I could have used stty (stty -F /dev/rfcomm0 raw) to change the default TTY behavior from converting all my LFs to CRLFs. However, now I'm running from code, and /dev/rfcomm0 does not exist. The closest "device" I can find is /dev/bus/usb/001/002, but I cannot run stty on that device. When I send a line-feed in the data stream, the tty interface seems to change it to \r\n. The result is that my length field is incorrect. The protocol does not include \r, so it is not sufficient for me to just bump the length.&amp;nbsp;&lt;/P&gt;&lt;P&gt;I've looked at the supported ioctl controls and found nothing. Open to any and all suggestions.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 01 Mar 2018 20:40:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/How-to-change-tty-behavior-on-bluetooth-socket/m-p/721341#M112162</guid>
      <dc:creator>patsandt</dc:creator>
      <dc:date>2018-03-01T20:40:37Z</dc:date>
    </item>
    <item>
      <title>Re: How to change tty behavior on bluetooth socket</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/How-to-change-tty-behavior-on-bluetooth-socket/m-p/721342#M112163</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Pat&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;one can try with tty interface raw mode&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="https://acassis.wordpress.com/2016/01/22/configuring-linuxs-serial-port-to-raw-mode/" title="https://acassis.wordpress.com/2016/01/22/configuring-linuxs-serial-port-to-raw-mode/"&gt;Configuring Linux’s serial port to raw mode – Alan C. Assis&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 02 Mar 2018 02:45:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/How-to-change-tty-behavior-on-bluetooth-socket/m-p/721342#M112163</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2018-03-02T02:45:54Z</dc:date>
    </item>
    <item>
      <title>Re: How to change tty behavior on bluetooth socket</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/How-to-change-tty-behavior-on-bluetooth-socket/m-p/721343#M112164</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Unfortunately, I have a socket, but not a dev. That is, "/dev/rfcomm0" does not appear as a device. "/dev/ttyUSB0" does not appear as a device. There are 100 other /dev/tty? devices, but I've not been able to determine which a am (if any). &lt;/P&gt;&lt;P&gt;Still open to suggestions.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 06 Mar 2018 17:13:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/How-to-change-tty-behavior-on-bluetooth-socket/m-p/721343#M112164</guid>
      <dc:creator>patsandt</dc:creator>
      <dc:date>2018-03-06T17:13:26Z</dc:date>
    </item>
    <item>
      <title>Re: How to change tty behavior on bluetooth socket</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/How-to-change-tty-behavior-on-bluetooth-socket/m-p/721344#M112165</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I've added the following code after the accept call:&lt;/P&gt;&lt;P&gt;struct rfcomm_dev_req req;&lt;/P&gt;&lt;P&gt;memset(&amp;amp;req,0,sizeof(req));&lt;/P&gt;&lt;P&gt;req.dev_id = 0; //?? might depend on other connections, but I have none at this time&lt;/P&gt;&lt;P&gt;req.flags = (1 &amp;lt;&amp;lt; RFCOMM_REUSE_DLC) | (1 &amp;lt;&amp;lt; RFCOMM_RELEASE_ONHUP);&lt;/P&gt;&lt;P&gt;bacpy(&amp;amp;req.src, &amp;amp;loc_addr.rc_bdaddr);&lt;/P&gt;&lt;P&gt;bacpy(&amp;amp;req.dst, &amp;amp;rem_addr.rc_bdaddr);&lt;/P&gt;&lt;P&gt;req.channel = rem_addr.rc_channel;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;int dev = ioctl(clientSock, RFCOMMCREATEDEV, &amp;amp;req);&lt;/P&gt;&lt;P&gt;std::string devname = "/dev/rfcomm";&lt;/P&gt;&lt;P&gt;devname += std::to_string(dev);&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm assuming I'm on the right track because it DID create a /dev/rfcomm entry.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 06 Mar 2018 19:44:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/How-to-change-tty-behavior-on-bluetooth-socket/m-p/721344#M112165</guid>
      <dc:creator>patsandt</dc:creator>
      <dc:date>2018-03-06T19:44:54Z</dc:date>
    </item>
  </channel>
</rss>