<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: Linux.bin (Boot Linux without U-boot)</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Linux-bin-Boot-Linux-without-U-boot/m-p/721087#M112106</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Ailton,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You need uboot, but these are link that other third party has made it.&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/docs/DOC-94513"&gt;Boot The i.mx6 dual With Linux+uC/OS-II AMP&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="http://www.dave.eu/sites/default/files/an-xelk-001-amp-linux-freertos.pdf" title="http://www.dave.eu/sites/default/files/an-xelk-001-amp-linux-freertos.pdf"&gt;http://www.dave.eu/sites/default/files/an-xelk-001-amp-linux-freertos.pdf&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;A _jive_internal="true" class="link-titled" href="https://community.nxp.com/thread/324831#408721" title="https://community.nxp.com/thread/324831#408721"&gt;https://community.nxp.com/thread/324831&lt;/A&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 06 Jun 2018 14:15:14 GMT</pubDate>
    <dc:creator>Bio_TICFSL</dc:creator>
    <dc:date>2018-06-06T14:15:14Z</dc:date>
    <item>
      <title>Linux.bin (Boot Linux without U-boot)</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Linux-bin-Boot-Linux-without-U-boot/m-p/721086#M112105</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&amp;nbsp;&lt;/P&gt;&lt;P&gt;Im trying to create a .bin file for linux including the zImage and the Device tree and filesystem for the Imx6QSD following a tutorial made fo the Zedboard and i used the zImage and .dtb created using buildroot, my question is what are the pre-boot steps necessary to boot linux on the imx6QSD board.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;At the moment im passing to the kernel when calling it the address of the .dtb and the Machine ID.&amp;nbsp;&lt;/P&gt;&lt;P&gt;btw the .bin is necessary to use it as the non-secure guest of an trustzone assisted hypervisor.&lt;/P&gt;&lt;P&gt;Kind Regards,&amp;nbsp;&lt;/P&gt;&lt;P&gt;Ailton Lopes&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 24 May 2018 19:11:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Linux-bin-Boot-Linux-without-U-boot/m-p/721086#M112105</guid>
      <dc:creator>ailtonlopes</dc:creator>
      <dc:date>2018-05-24T19:11:13Z</dc:date>
    </item>
    <item>
      <title>Re: Linux.bin (Boot Linux without U-boot)</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Linux-bin-Boot-Linux-without-U-boot/m-p/721087#M112106</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Ailton,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You need uboot, but these are link that other third party has made it.&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/docs/DOC-94513"&gt;Boot The i.mx6 dual With Linux+uC/OS-II AMP&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="http://www.dave.eu/sites/default/files/an-xelk-001-amp-linux-freertos.pdf" title="http://www.dave.eu/sites/default/files/an-xelk-001-amp-linux-freertos.pdf"&gt;http://www.dave.eu/sites/default/files/an-xelk-001-amp-linux-freertos.pdf&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;A _jive_internal="true" class="link-titled" href="https://community.nxp.com/thread/324831#408721" title="https://community.nxp.com/thread/324831#408721"&gt;https://community.nxp.com/thread/324831&lt;/A&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 06 Jun 2018 14:15:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Linux-bin-Boot-Linux-without-U-boot/m-p/721087#M112106</guid>
      <dc:creator>Bio_TICFSL</dc:creator>
      <dc:date>2018-06-06T14:15:14Z</dc:date>
    </item>
  </channel>
</rss>